OV5640 camera inconstant issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV5640 camera inconstant issue

794 Views
mohammedazlum
Contributor IV

Hi,
 
We are facing below issue in OV5640 camera sensor module. When we continuously run the overlay, some of the time overlay is not working. I would like to say, we are facing inconstant issue in OV5640 camera sensor. The OV5640 camera module run with Embedded sync format. Do you have any idea why this inconsistent issue occurring in OV5640 ?

Any timing parameter to be changed ?
 
Please help us.
 
Regards,
Mohammed Azlum

Tags (1)
0 Kudos
1 Reply

607 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mohammed

one can check Release Notes of used BSP, for example

in attached sect.6.3 Known issues and limitations for multimedia.

Other options to narrow down issue may be descreasing processor bus

loading or increasing cma size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos