OV5640 MIPI V3 Camera Orientation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OV5640 MIPI V3 Camera Orientation

1,393件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I am using the OV5640 MIPI V3 camera with IMX8 Board in Android 9 Automotive. I need to change the camera orientation. 

Format : 1080P

Resolution : 1920x1080

Frame Rate: 30FPS

But video quality is very low. 

Please find the attachment and let me know the configuration for increasing the video quality and camera rotation.

pastedImage_1.png

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
4 返答(返信)

1,098件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I did the following ,

{0x3820, 0x47, 0, 0}, {0x3821, 0x01, 0, 0}, {0x3814, 0x31, 0, 0},

But, It dose not work as per this datasheet,

OV5640-MIRROR.png

Thanks & Regards,

Vinoths,

Regards,
Vinothkumar Sekar
0 件の賞賛

1,098件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the i.MX8QM is still under development. Many of the software is still under development and could be subject to change. We cannot guarantee if the software will work until the i.MX8QM is completely released.

Best regards,

Diego.

0 件の賞賛

1,098件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Diego,

 

Thank you for your reply.

 

What is the pixel clock for LVDS in IMX8QM?

 

Will you give please your input for the following thread?

 

https://community.nxp.com/thread/525298 

 

 

 

Thank You,

Vinoth S,

Regards,
Vinothkumar Sekar
0 件の賞賛

1,098件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, this is a completely different question. I suggest you submit another community thread with the new question. 

Best regards,

Diego.

0 件の賞賛