Hello NXP community,
Could you please let me know whether OV5640 porting via ISP on imx8mp-lppddr4-evk is supported or not.
If yes, please let me know what are the dependencies or supported packages need to be add/create .
In AN13713 document there are some steps related to ISP porting but i see that is with respect to other sensor not ov5640, If you confirm that if i follow the steps mentioned in AN13713 i could port ov5640 via isp to imx8mp then i'll follow that.
Also please provide any document specifically for ov5640 porting via ISP to imx8mp lpddr4 evk.
If no document please provide detailed steps possible.
Thanks in Advance,
Regards,
Gowrish.
Please refer the following link:
https://community.nxp.com/t5/i-MX-Processors/ov5640-isp-porting-on-imx8mp-evk/m-p/1893338
Hi @pengyong_zhang ,
Thanks for the reply.
Through ISI it is working fine I want to know how to enable the ISP porting to OV5640 camera only in .dts any supported packages are there ?
Thanks & Regards,
Gowrish.
HI @gowrish
Could you please let me know whether OV5640 porting via ISP on imx8mp-lppddr4-evk is supported or not.
A : It supports.
boot with imx8mp-evk-ov2775-ov5640.dtb file. set status of &isi_0 or &isi_1 to “Okay” in the dts file