OV420 driver for i.MX535 QSB and linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OV420 driver for i.MX535 QSB and linux

1,699 次查看
aksispd
Contributor II

​I'm fairly new to i.MX and trying to connect an OV420 A/D with CMOS sensor to the I.MX535 QSB, anyone has experience with driver development? the supplied OV3640 seems to be a good start, is this the right way to get going? modify the existing Driver or start from scratch. Also did anyone make the test pattern work? Thanks!

0 项奖励
回复
6 回复数

1,332 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the drvier souce code of mx53 in the bsp, I don't have ov420 data sheet, if you use tvin as input, I can send the tvin demo source code to you for reference.

0 项奖励
回复

1,332 次查看
aksispd
Contributor II

Can you please send the TVin demo? By any chance did you have the csi test mode working from the system dev guide 19th section.

0 项奖励
回复

1,332 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls find the demo code, hope helpful for you.

1,332 次查看
aksispd
Contributor II

I have one more question, per the documentation the i.MX53 QSB-R does not support camera, I guess this only means there is no connector installed. If you build a daughterboard it should all work fine. Is that right?

0 项奖励
回复

1,332 次查看
aksispd
Contributor II

I plan using the CSI0 and trying to see if the example snippets shown in the i.MX53 System Development Guide 19th section. 

0 项奖励
回复

1,332 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you use linux os, you can refer to the enclosed file to get the driver of bsp for other camera.

0 项奖励
回复