OTG1/2 on i.MXQXP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTG1/2 on i.MXQXP

1,092件の閲覧回数
ahyuo79
Contributor I

I am interested in USB2-OTG1/2  and USB3-OTG3 on i.MXQXP

because I reviewed USB in  i.MXQXP EVM , here use OTG2/OTG3 for USB Type-C

but I want to use only OTG1 and OTG2 (USB2)  not USB3 

I reviewed it below in Datasheet 

      14.1.1 Overview  (attached otg.png)

      14.10.3.1.1 Configuration, Control and Status Register Set

       UOG1/UOG2/UH   

      14.10.4 USB Non-Core Memory Map/Register Definition

       USBNC_OTG1_CTRL1/USBNC_OTG2_CTRL1/USBNC_UH_CTRL1

      14.12.6.33 USB2 Port Status and Control (PORTSC1USB2)

 

is it possible to use only OTG1 and OTG2 without USB3 well ?

Could you please explain it well if OTG1 and OTG2 have limited functions?

 

I think OTG1 share too many registers with OTG2 in Same Controller

I have a plan to set only OTG1 in device tree and I fix USB ID Pin for device or host  so want use both 

 

I hope to hear your advice 

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

1,080件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,077件の閲覧回数
jianwei_lan
Contributor III

Dear friend

 

The link you provide have expired.

 

pls push update one.

 

 

----

BR

0 件の賞賛
返信

1,072件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,070件の閲覧回数
jianwei_lan
Contributor III

Dear friend

 

What does the change meaning?

 

--

BR

0 件の賞賛
返信

1,047件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can use otg1 which is independent from otg2, in current B0 board, otg1 is used for baseboard, and otg2 is  part of the SS3 interface, you can remove type C and use otg1 to downloading

 

0 件の賞賛
返信