Hello Everyone,
we are trying to use the im8m mini usb otg2 with usb hub(usb4604) for mouse and other devices. It is found that it is not working and log file of our board not detecting the usb hub and mouse.
Any help is appreciated. Thank you
Regards,
Anusha
I use a similar USB hub on a custom board. Depending on the values of the strapping pins, the hub either connects automatically to the i.MX, it reads configuration data from an I2C eeprom, or acts as an I2C slave and waits for configuration.
In my design, the HUB waits for configuration via I2C/SMBUS. I use a custom Linux driver to configure the HUB. After configuration is finished, the HUB appears on the i.MX USB interface.
Best regards
Christian
Hi Anusha
first one can check if usb4604 configured properly: check power supplies,
clocks and strap pins using datasheet below, note it can work also in hsic mode.
http://ww1.microchip.com/downloads/en/DeviceDoc/00001716B.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Anusha,
a "Strap pin" is a kind of configuration pin (often found on ethernet PHYs). At normal operation, a strap pin has output functionality (e.g. link/activity LED). But at power on/reset time, the strap pin acts as a configuration input. Depending on external pullup/pulldown resistors, a particular configuration option (device depended) is selected.
I hope this answers your question.
regerds
Christian