Noise in OV5640 camera with IMX6 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Noise in OV5640 camera with IMX6 custom board

2,101 Views
jaiminthakkar
Contributor II

Hi,

I am getting noise/lines in ov5640 camera output on IMX6 based custom board (based on nitrogen6_max board).

I have attached the camera output pic. : Spiky - Free Image Hosting 

I am using Android 4.4.3_2.0.0-ga (Boundry Devices) which is based on Freescale BSP.

Please help me to debug this issue.

Labels (1)
0 Kudos
Reply
5 Replies

1,575 Views
v_khludenkov
Contributor I

Dear Jamin,

hosting spiky is blocking

did you manage to solve this problem?
please send your photo to the address

v.khludenkov@zenit-kmz.ru

best regards

0 Kudos
Reply

1,575 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaimin

if software is the same noise can be from hardware,

please check analog supplies and its noise, sensor cables.

Attach sensor from good board to custom and check if that helps.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,575 Views
jaiminthakkar
Contributor II

Hi,

We have already added filters on Analog and digital supply rails as well as added parallel termination on MIPI signals . But lines are observed on capture.  Total length of MIPI CSI is 5" Inch on flex-rigid PCB.

Thanks,

Jaimin Thakkar

0 Kudos
Reply

1,575 Views
igorpadykov
NXP Employee
NXP Employee

one can try to test with imx-test (folder mxc_v4l2_test) in

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

also one can check signals with oscilloscope and using app note

http://www.analog.com/media/en/technical-documentation/application-notes/AN-1337.pdf 

Best regards
igor

0 Kudos
Reply

1,575 Views
jaiminthakkar
Contributor II

Hi,

We tested camera output using imx-test (v4l2 test) and found noise in all scenarios except 5 megapixel (2592x1944) resolution output. We are unable to understand reason behind that. Camera test pattern is also fine.

We also checked signals using oscillosope and  found good termination.

Can you please help us more to know which type of noise it is and how to remove that?

Thanks,

Jaimin Thakkar

0 Kudos
Reply