Hello,
I am working on yocto project to create an image for my phyBOARD-Segin i.MX 6UL/ULL.
'm Working on a VM ubuntu 20.04 and following the user_guide:
https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf
Bitbake image took hours and went far (good sign) but I got a problem making target for a module i guess.
Here below a copy of my problem log:
<< make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-btwifi-sdio3_0.dtb'. Stop.
| make[1]: *** [/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/Makefile:1355: imx6ull-14x14-evk-btwifi-sdio3_0.dtb] Error 2
| make: *** [/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/Makefile:185: __sub-make] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command. >>
Is there a fix I can do or this is a compatibility problem ?
I saw similar problems with no answer
Any Ideas ?
Thanks in advance
Hi, Did you find any update on this or is the error is resolved?
Hi,
My steps are the same described in the user guide I mentioned above.
https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf
And the full log I got was:
<<<
WARNING: You have included the meta-virtualization layer, but 'virtualization' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-virtualization README for details on enabling virtualization support.
Loading cache: 100% |##########################################################################################| Time: 0:00:02
Loaded 5091 entries from dependency cache.
Parsing recipes: 100% |########################################################################################| Time: 0:00:02
Parsing of 3386 .bb files complete (3385 cached, 1 parsed). 5092 targets, 641 skipped, 6 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.52.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-fslc-linux-gnueabi"
MACHINE = "imx6ullevk"
DISTRO = "fslc-framebuffer"
DISTRO_VERSION = "3.4-snapshot-20220412"
TUNE_FEATURES = "arm vfp cortexa7 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:4d7162798ec19c726877e85509e4c7a99eb6576d"
meta-oe
meta-multimedia
meta-python = "HEAD:4647e3ea3708d30eeb0149f6d5626c9576bff520"
meta-freescale = "HEAD:ed3435620a2404c241fef3c4ef90d1f31d3b7a8a"
meta-freescale-3rdparty = "HEAD:155ffd6d7b694d8de76919c25681ecb98882646e"
meta-freescale-distro = "HEAD:d2e27cc4778663450495a67bfb036cba600cb27a"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:dd96a60afb72c0f89f384278e8fbbf4c8ea00a2c"
meta-nxp-demo-experience = "HEAD:4bbe714267b730df020438fe83ae2c7c91708045"
meta-chromium = "HEAD:e22bac72bc1f1bb5d2f44e64a53128b8be644272"
meta-clang = "HEAD:fc5389393adb005b519e488e9e6be4fc5791239c"
meta-gnome
meta-networking
meta-filesystems = "HEAD:4647e3ea3708d30eeb0149f6d5626c9576bff520"
meta-qt6 = "HEAD:1b9f4646dd69c5567d19ed77b8347506fe7faf2b"
meta-python2 = "HEAD:5243d509aebff378c1ae9d3dff6a29cfdc0dee1f"
meta-virtualization = "HEAD:ed52ba982179087ecc84f7dc3b0a16cfe25f2f8e"
Initialising tasks: 100% |#####################################################################################| Time: 0:00:01
Sstate summary: Wanted 0 Local 0 Network 0 Missed 0 Current 0 (0% match, 0% complete)
NOTE: No setscene tasks
NOTE: Executing Tasks
NOTE: Tasks Summary: Attempted 3 tasks of which 0 didn't need to be rerun and all succeeded.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 6 seconds
Summary: There was 1 WARNING message shown.
>>>
2.bitbake linux-fslc-imx step failed with the same status as my first log:
<<<
ERROR: linux-fslc-imx-5.10.74+gitAUTOINC+b0d74a58e2-r0 do_compile: oe_runmake failed
ERROR: linux-fslc-imx-5.10.74+gitAUTOINC+b0d74a58e2-r0 do_compile: ExecutionError('/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/temp/run.do_compile.1530435', 1, None, None)
ERROR: Logfile of failure stored in: /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/temp/log.do_compile.1530435
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: KBUILD_BUILD_TIMESTAMP: Mon Oct 18 17:39:28 UTC 2021
| NOTE: make -j 1 HOSTCC=gcc -isystem/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/osboxes/imx-yocto-bsp/build-first/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 HOSTCPP=gcc -E HOSTCXX=g++ -isystem/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/osboxes/imx-yocto-bsp/build-first/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 zImage CC=arm-fslc-linux-gnueabi-gcc -mno-thumb-interwork -marm -fuse-ld=bfd -fmacro-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0=/usr/src/debug/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0 -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0=/usr/src/debug/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0 -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot= -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source=/usr/src/kernel LD=arm-fslc-linux-gnueabi-ld.bfd LOADADDR=0x80008000
| GEN Makefile
| SYSHDR arch/arm/include/generated/uapi/asm/unistd-common.h
| SYSHDR arch/arm/include/generated/uapi/asm/unistd-oabi.h
| SYSHDR arch/arm/include/generated/uapi/asm/unistd-eabi.h
| HOSTCC scripts/dtc/dtc.o
| HOSTCC scripts/dtc/flattree.o
| HOSTCC scripts/dtc/fstree.o
| HOSTCC scripts/dtc/data.o
| HOSTCC scripts/dtc/livetree.o
| HOSTCC scripts/dtc/treesource.o
| HOSTCC scripts/dtc/srcpos.o
| HOSTCC scripts/dtc/checks.o
| HOSTCC scripts/dtc/util.o
| LEX scripts/dtc/dtc-lexer.lex.c
| YACC scripts/dtc/dtc-parser.tab.[ch]
| HOSTCC scripts/dtc/dtc-lexer.lex.o
| HOSTCC scripts/dtc/dtc-parser.tab.o
| HOSTLD scripts/dtc/dtc
| HOSTCC scripts/genksyms/genksyms.o
| YACC scripts/genksyms/parse.tab.[ch]
| HOSTCC scripts/genksyms/parse.tab.o
| LEX scripts/genksyms/lex.lex.c
| HOSTCC scripts/genksyms/lex.lex.o
| HOSTLD scripts/genksyms/genksyms
| HOSTCC scripts/kallsyms
| HOSTCC scripts/sorttable
| HOSTCC scripts/asn1_compiler
| HOSTCC scripts/extract-cert
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c: In function 'display_openssl_errors':
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:46:2: warning: 'ERR_get_error_line' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 46 | while ((e = ERR_get_error_line(&file, &line))) {
| | ^~~~~
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:23:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/err.h:411:15: note: declared here
| 411 | unsigned long ERR_get_error_line(const char **file, int *line);
| | ^~~~~~~~~~~~~~~~~~
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c: In function 'drain_openssl_errors':
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:59:2: warning: 'ERR_get_error_line' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 59 | while (ERR_get_error_line(&file, &line)) {}
| | ^~~~~
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:23:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/err.h:411:15: note: declared here
| 411 | unsigned long ERR_get_error_line(const char **file, int *line);
| | ^~~~~~~~~~~~~~~~~~
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c: In function 'main':
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:124:3: warning: 'ENGINE_load_builtin_engines' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 124 | ENGINE_load_builtin_engines();
| | ^~~~~~~~~~~~~~~~~~~~~~~~~~~
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:24:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/engine.h:358:28: note: declared here
| 358 | OSSL_DEPRECATEDIN_3_0 void ENGINE_load_builtin_engines(void);
| | ^~~~~~~~~~~~~~~~~~~~~~~~~~~
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:126:3: warning: 'ENGINE_by_id' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 126 | e = ENGINE_by_id("pkcs11");
| | ^
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:24:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/engine.h:336:31: note: declared here
| 336 | OSSL_DEPRECATEDIN_3_0 ENGINE *ENGINE_by_id(const char *id);
| | ^~~~~~~~~~~~
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:128:3: warning: 'ENGINE_init' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 128 | if (ENGINE_init(e))
| | ^~
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:24:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/engine.h:620:27: note: declared here
| 620 | OSSL_DEPRECATEDIN_3_0 int ENGINE_init(ENGINE *e);
| | ^~~~~~~~~~~
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:133:4: warning: 'ENGINE_ctrl_cmd_string' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 133 | ERR(!ENGINE_ctrl_cmd_string(e, "PIN", key_pass, 0), "Set PKCS#11 PIN");
| | ^~~
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:24:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/engine.h:479:5: note: declared here
| 479 | int ENGINE_ctrl_cmd_string(ENGINE *e, const char *cmd_name, const char *arg,
| | ^~~~~~~~~~~~~~~~~~~~~~
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:134:3: warning: 'ENGINE_ctrl_cmd' is deprecated: Since OpenSSL 3.0 [-Wdeprecated-declarations]
| 134 | ENGINE_ctrl_cmd(e, "LOAD_CERT_CTRL", 0, &parms, NULL, 1);
| | ^~~~~~~~~~~~~~~
| In file included from /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/extract-cert.c:24:
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include/openssl/engine.h:450:27: note: declared here
| 450 | OSSL_DEPRECATEDIN_3_0 int ENGINE_ctrl_cmd(ENGINE *e, const char *cmd_name,
| | ^~~~~~~~~~~~~~~
| WRAP arch/arm/include/generated/uapi/asm/kvm_para.h
| WRAP arch/arm/include/generated/uapi/asm/bitsperlong.h
| WRAP arch/arm/include/generated/uapi/asm/bpf_perf_event.h
| WRAP arch/arm/include/generated/uapi/asm/errno.h
| WRAP arch/arm/include/generated/uapi/asm/ioctl.h
| WRAP arch/arm/include/generated/uapi/asm/ipcbuf.h
| WRAP arch/arm/include/generated/uapi/asm/msgbuf.h
| WRAP arch/arm/include/generated/uapi/asm/param.h
| WRAP arch/arm/include/generated/uapi/asm/poll.h
| WRAP arch/arm/include/generated/uapi/asm/resource.h
| WRAP arch/arm/include/generated/uapi/asm/sembuf.h
| WRAP arch/arm/include/generated/uapi/asm/shmbuf.h
| WRAP arch/arm/include/generated/uapi/asm/siginfo.h
| WRAP arch/arm/include/generated/uapi/asm/socket.h
| WRAP arch/arm/include/generated/uapi/asm/sockios.h
| WRAP arch/arm/include/generated/uapi/asm/termbits.h
| WRAP arch/arm/include/generated/uapi/asm/termios.h
| WRAP arch/arm/include/generated/asm/early_ioremap.h
| WRAP arch/arm/include/generated/asm/extable.h
| WRAP arch/arm/include/generated/asm/flat.h
| WRAP arch/arm/include/generated/asm/parport.h
| WRAP arch/arm/include/generated/asm/seccomp.h
| WRAP arch/arm/include/generated/asm/compat.h
| WRAP arch/arm/include/generated/asm/current.h
| WRAP arch/arm/include/generated/asm/emergency-restart.h
| WRAP arch/arm/include/generated/asm/exec.h
| WRAP arch/arm/include/generated/asm/irq_regs.h
| WRAP arch/arm/include/generated/asm/kdebug.h
| WRAP arch/arm/include/generated/asm/local.h
| WRAP arch/arm/include/generated/asm/local64.h
| WRAP arch/arm/include/generated/asm/mm-arch-hooks.h
| WRAP arch/arm/include/generated/asm/mmiowb.h
| WRAP arch/arm/include/generated/asm/msi.h
| WRAP arch/arm/include/generated/asm/preempt.h
| WRAP arch/arm/include/generated/asm/rwonce.h
| WRAP arch/arm/include/generated/asm/serial.h
| WRAP arch/arm/include/generated/asm/simd.h
| WRAP arch/arm/include/generated/asm/trace_clock.h
| UPD include/config/kernel.release
| UPD include/generated/uapi/linux/version.h
| UPD include/generated/utsrelease.h
| SYSNR arch/arm/include/generated/asm/unistd-nr.h
| GEN arch/arm/include/generated/asm/mach-types.h
| SYSTBL arch/arm/include/generated/calls-oabi.S
| SYSTBL arch/arm/include/generated/calls-eabi.S
| CC scripts/mod/empty.o
| HOSTCC scripts/mod/mk_elfconfig
| MKELF scripts/mod/elfconfig.h
| HOSTCC scripts/mod/modpost.o
| CC scripts/mod/devicetable-offsets.s
| UPD scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTCC scripts/mod/sumversion.o
| HOSTLD scripts/mod/modpost
| CC kernel/bounds.s
| UPD include/generated/bounds.h
| UPD include/generated/timeconst.h
| CC arch/arm/kernel/asm-offsets.s
| UPD include/generated/asm-offsets.h
| CALL /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/checksyscalls.sh
| CALL /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/scripts/atomic/check-atomics.sh
| CC init/main.o
| CHK include/generated/compile.h
| UPD include/generated/compile.h
| CC drivers/input/touchscreen/goodix.o
...
...
| CC drivers/input/touchscreen/ili210x.o
| CC drivers/input/touchscreen/imx6ul_tsc.o
| CC drivers/input/touchscreen/max11801_ts.o
| CC drivers/input/touchscreen/mc13783_ts.o
| CC drivers/input/touchscreen/stmpe-ts.o
| CC drivers/input/touchscreen/tsc200x-core.o
| CC drivers/input/touchscreen/tsc2004.o
| CC drivers/input/touchscreen/tsc2007_core.o
| CC drivers/input/touchscreen/sx8654.o
| CC drivers/input/touchscreen/colibri-vf50-ts.o
| AR drivers/input/touchscreen/built-in.a
| CC drivers/input/misc/mma8450.o
| CC drivers/input/misc/mpl3115.o
| CC drivers/input/misc/fxls8471.o
| CC drivers/input/misc/fxls8471_i2c.o
| CC drivers/input/misc/isl29023.o
| CC drivers/input/misc/rpmsg_input.o
| AR drivers/input/misc/built-in.a
| CC drivers/input/input.o
| CC drivers/input/input-compat.o
| CC drivers/input/input-mt.o
| CC drivers/input/input-poller.o
| CC drivers/input/ff-core.o
| CC drivers/input/input-polldev.o
| CC drivers/input/matrix-keymap.o
| CC drivers/input/input-leds.o
| CC drivers/input/evdev.o
| AR drivers/input/built-in.a
| CC drivers/rtc/lib.o
| CC drivers/rtc/systohc.o
| CC drivers/rtc/class.o
| CC drivers/rtc/interface.o
| CC drivers/rtc/nvmem.o
| CC drivers/rtc/dev.o
| CC drivers/rtc/proc.o
| CC drivers/rtc/sysfs.o
| CC drivers/rtc/rtc-da9063.o
| CC drivers/rtc/rtc-ds1307.o
| CC drivers/rtc/rtc-imx-rpmsg.o
| CC drivers/rtc/rtc-isl1208.o
| CC drivers/rtc/rtc-m41t80.o
| CC drivers/rtc/rtc-mc13xxx.o
| CC drivers/rtc/rtc-mxc.o
| CC drivers/rtc/rtc-mxc_v2.o
| CC drivers/rtc/rtc-pcf8523.o
| CC drivers/rtc/rtc-pcf8563.o
| CC drivers/rtc/rtc-rc5t619.o
| CC drivers/rtc/rtc-snvs.o
| AR drivers/rtc/built-in.a
| CC drivers/i2c/algos/i2c-algo-bit.o
| AR drivers/i2c/algos/built-in.a
| CC drivers/i2c/busses/i2c-gpio.o
| CC drivers/i2c/busses/i2c-imx.o
| CC drivers/i2c/busses/i2c-imx-lpi2c.o
| AR drivers/i2c/busses/built-in.a
| CC drivers/i2c/muxes/i2c-mux-gpio.o
| AR drivers/i2c/muxes/built-in.a
| CC drivers/i2c/i2c-boardinfo.o
| CC drivers/i2c/i2c-core-base.o
| CC drivers/i2c/i2c-core-smbus.o
| CC drivers/i2c/i2c-core-of.o
| CC drivers/i2c/i2c-dev.o
| CC drivers/i2c/i2c-mux.o
| AR drivers/i2c/built-in.a
| AR drivers/i3c/built-in.a
| CC drivers/media/i2c/ir-kbd-i2c.o
| AR drivers/media/i2c/built-in.a
| AR drivers/media/tuners/built-in.a
| AR drivers/media/dvb-frontends/built-in.a
| CC drivers/media/mc/mc-device.o
| CC drivers/media/mc/mc-devnode.o
| CC drivers/media/mc/mc-entity.o
| CC drivers/media/mc/mc-request.o
| CC drivers/media/mc/mc-dev-allocator.o
| AR drivers/media/mc/built-in.a
| CC drivers/media/v4l2-core/v4l2-fwnode.o
| CC drivers/media/v4l2-core/v4l2-dev.o
| CC drivers/media/v4l2-core/v4l2-ioctl.o
| CC drivers/media/v4l2-core/v4l2-device.o
| CC drivers/media/v4l2-core/v4l2-fh.o
| CC drivers/media/v4l2-core/v4l2-event.o
| CC drivers/media/v4l2-core/v4l2-ctrls.o
| CC drivers/media/v4l2-core/v4l2-subdev.o
| CC drivers/media/v4l2-core/v4l2-clk.o
| CC drivers/media/v4l2-core/v4l2-async.o
| CC drivers/media/v4l2-core/v4l2-common.o
| CC drivers/media/v4l2-core/v4l2-mc.o
| CC drivers/media/v4l2-core/v4l2-spi.o
| CC drivers/media/v4l2-core/v4l2-i2c.o
| CC drivers/media/v4l2-core/v4l2-dv-timings.o
| CC drivers/media/v4l2-core/v4l2-mem2mem.o
| CC drivers/media/v4l2-core/videobuf-core.o
| CC drivers/media/v4l2-core/videobuf-dma-contig.o
| AR drivers/media/v4l2-core/built-in.a
| CC drivers/media/dvb-core/dvbdev.o
| CC drivers/media/dvb-core/dmxdev.o
| CC drivers/media/dvb-core/dvb_demux.o
| CC drivers/media/dvb-core/dvb_ca_en50221.o
| CC drivers/media/dvb-core/dvb_frontend.o
| CC drivers/media/dvb-core/dvb_net.o
| CC drivers/media/dvb-core/dvb_ringbuffer.o
| CC drivers/media/dvb-core/dvb_math.o
| AR drivers/media/dvb-core/built-in.a
| CC drivers/media/rc/keymaps/rc-adstech-dvb-t-pci.o
| CC drivers/media/rc/keymaps/rc-alink-dtu-m.o
| CC drivers/media/rc/keymaps/rc-anysee.o
| CC drivers/media/rc/keymaps/rc-apac-viewcomp.o
| CC drivers/media/rc/keymaps/rc-astrometa-t2hybrid.o
| CC drivers/media/rc/keymaps/rc-asus-pc39.o
| CC drivers/media/rc/keymaps/rc-asus-ps3-100.o
| CC drivers/media/rc/keymaps/rc-ati-tv-wonder-hd-600.o
| CC drivers/media/rc/keymaps/rc-ati-x10.o
| CC drivers/media/rc/keymaps/rc-avermedia-a16d.o
| CC drivers/media/rc/keymaps/rc-avermedia.o
| CC drivers/media/rc/keymaps/rc-avermedia-cardbus.o
| CC drivers/media/rc/keymaps/rc-avermedia-dvbt.o
| CC drivers/media/rc/keymaps/rc-avermedia-m135a.o
| CC drivers/media/rc/keymaps/rc-avermedia-m733a-rm-k6.o
| CC drivers/media/rc/keymaps/rc-avermedia-rm-ks.o
| CC drivers/media/rc/keymaps/rc-avertv-303.o
| CC drivers/media/rc/keymaps/rc-azurewave-ad-tu700.o
| CC drivers/media/rc/keymaps/rc-beelink-gs1.o
| CC drivers/media/rc/keymaps/rc-behold.o
| CC drivers/media/rc/keymaps/rc-behold-columbus.o
| CC drivers/media/rc/keymaps/rc-budget-ci-old.o
| CC drivers/media/rc/keymaps/rc-cinergy-1400.o
| CC drivers/media/rc/keymaps/rc-cinergy.o
| CC drivers/media/rc/keymaps/rc-d680-dmb.o
| CC drivers/media/rc/keymaps/rc-delock-61959.o
| CC drivers/media/rc/keymaps/rc-dib0700-nec.o
| CC drivers/media/rc/keymaps/rc-dib0700-rc5.o
| CC drivers/media/rc/keymaps/rc-digitalnow-tinytwin.o
| CC drivers/media/rc/keymaps/rc-digittrade.o
| CC drivers/media/rc/keymaps/rc-dm1105-nec.o
| CC drivers/media/rc/keymaps/rc-dntv-live-dvb-t.o
| CC drivers/media/rc/keymaps/rc-dntv-live-dvbt-pro.o
| CC drivers/media/rc/keymaps/rc-dtt200u.o
| CC drivers/media/rc/keymaps/rc-dvbsky.o
| CC drivers/media/rc/keymaps/rc-dvico-mce.o
| CC drivers/media/rc/keymaps/rc-dvico-portable.o
| CC drivers/media/rc/keymaps/rc-em-terratec.o
| CC drivers/media/rc/keymaps/rc-encore-enltv2.o
| CC drivers/media/rc/keymaps/rc-encore-enltv.o
| CC drivers/media/rc/keymaps/rc-encore-enltv-fm53.o
| CC drivers/media/rc/keymaps/rc-evga-indtube.o
| CC drivers/media/rc/keymaps/rc-eztv.o
| CC drivers/media/rc/keymaps/rc-flydvb.o
| CC drivers/media/rc/keymaps/rc-flyvideo.o
| CC drivers/media/rc/keymaps/rc-fusionhdtv-mce.o
| CC drivers/media/rc/keymaps/rc-gadmei-rm008z.o
| CC drivers/media/rc/keymaps/rc-geekbox.o
| CC drivers/media/rc/keymaps/rc-genius-tvgo-a11mce.o
| CC drivers/media/rc/keymaps/rc-gotview7135.o
| CC drivers/media/rc/keymaps/rc-hisi-poplar.o
| CC drivers/media/rc/keymaps/rc-hisi-tv-demo.o
| CC drivers/media/rc/keymaps/rc-imon-mce.o
| CC drivers/media/rc/keymaps/rc-imon-pad.o
| CC drivers/media/rc/keymaps/rc-imon-rsc.o
| CC drivers/media/rc/keymaps/rc-iodata-bctv7e.o
| CC drivers/media/rc/keymaps/rc-it913x-v1.o
| CC drivers/media/rc/keymaps/rc-it913x-v2.o
| CC drivers/media/rc/keymaps/rc-kaiomy.o
| CC drivers/media/rc/keymaps/rc-khadas.o
| CC drivers/media/rc/keymaps/rc-kworld-315u.o
| CC drivers/media/rc/keymaps/rc-kworld-pc150u.o
| CC drivers/media/rc/keymaps/rc-kworld-plus-tv-analog.o
| CC drivers/media/rc/keymaps/rc-leadtek-y04g0051.o
| CC drivers/media/rc/keymaps/rc-lme2510.o
| CC drivers/media/rc/keymaps/rc-manli.o
| CC drivers/media/rc/keymaps/rc-medion-x10.o
| CC drivers/media/rc/keymaps/rc-medion-x10-digitainer.o
| CC drivers/media/rc/keymaps/rc-medion-x10-or2x.o
| CC drivers/media/rc/keymaps/rc-msi-digivox-ii.o
| CC drivers/media/rc/keymaps/rc-msi-digivox-iii.o
| CC drivers/media/rc/keymaps/rc-msi-tvanywhere.o
| CC drivers/media/rc/keymaps/rc-msi-tvanywhere-plus.o
| CC drivers/media/rc/keymaps/rc-nebula.o
| CC drivers/media/rc/keymaps/rc-nec-terratec-cinergy-xs.o
| CC drivers/media/rc/keymaps/rc-norwood.o
| CC drivers/media/rc/keymaps/rc-npgtech.o
| CC drivers/media/rc/keymaps/rc-odroid.o
| CC drivers/media/rc/keymaps/rc-pctv-sedna.o
| CC drivers/media/rc/keymaps/rc-pinnacle-color.o
| CC drivers/media/rc/keymaps/rc-pinnacle-grey.o
| CC drivers/media/rc/keymaps/rc-pinnacle-pctv-hd.o
| CC drivers/media/rc/keymaps/rc-pixelview.o
| CC drivers/media/rc/keymaps/rc-pixelview-mk12.o
| CC drivers/media/rc/keymaps/rc-pixelview-002t.o
| CC drivers/media/rc/keymaps/rc-pixelview-new.o
| CC drivers/media/rc/keymaps/rc-powercolor-real-angel.o
| CC drivers/media/rc/keymaps/rc-proteus-2309.o
| CC drivers/media/rc/keymaps/rc-purpletv.o
| CC drivers/media/rc/keymaps/rc-pv951.o
| CC drivers/media/rc/keymaps/rc-hauppauge.o
| CC drivers/media/rc/keymaps/rc-rc6-mce.o
| CC drivers/media/rc/keymaps/rc-real-audio-220-32-keys.o
| CC drivers/media/rc/keymaps/rc-reddo.o
| CC drivers/media/rc/keymaps/rc-snapstream-firefly.o
| CC drivers/media/rc/keymaps/rc-streamzap.o
| CC drivers/media/rc/keymaps/rc-tango.o
| CC drivers/media/rc/keymaps/rc-tanix-tx3mini.o
| CC drivers/media/rc/keymaps/rc-tanix-tx5max.o
| CC drivers/media/rc/keymaps/rc-tbs-nec.o
| CC drivers/media/rc/keymaps/rc-technisat-ts35.o
| CC drivers/media/rc/keymaps/rc-technisat-usb2.o
| CC drivers/media/rc/keymaps/rc-terratec-cinergy-c-pci.o
| CC drivers/media/rc/keymaps/rc-terratec-cinergy-s2-hd.o
| CC drivers/media/rc/keymaps/rc-terratec-cinergy-xs.o
| CC drivers/media/rc/keymaps/rc-terratec-slim.o
| CC drivers/media/rc/keymaps/rc-terratec-slim-2.o
| CC drivers/media/rc/keymaps/rc-tevii-nec.o
| CC drivers/media/rc/keymaps/rc-tivo.o
| CC drivers/media/rc/keymaps/rc-total-media-in-hand.o
| CC drivers/media/rc/keymaps/rc-total-media-in-hand-02.o
| CC drivers/media/rc/keymaps/rc-trekstor.o
| CC drivers/media/rc/keymaps/rc-tt-1500.o
| CC drivers/media/rc/keymaps/rc-twinhan-dtv-cab-ci.o
| CC drivers/media/rc/keymaps/rc-twinhan1027.o
| CC drivers/media/rc/keymaps/rc-vega-s9x.o
| CC drivers/media/rc/keymaps/rc-videomate-m1f.o
| CC drivers/media/rc/keymaps/rc-videomate-s350.o
| CC drivers/media/rc/keymaps/rc-videomate-tv-pvr.o
| CC drivers/media/rc/keymaps/rc-videostrong-kii-pro.o
| CC drivers/media/rc/keymaps/rc-wetek-hub.o
| CC drivers/media/rc/keymaps/rc-wetek-play2.o
| CC drivers/media/rc/keymaps/rc-winfast.o
| CC drivers/media/rc/keymaps/rc-winfast-usbii-deluxe.o
| CC drivers/media/rc/keymaps/rc-su3000.o
| CC drivers/media/rc/keymaps/rc-xbox-dvd.o
| CC drivers/media/rc/keymaps/rc-x96max.o
| CC drivers/media/rc/keymaps/rc-zx-irdec.o
| AR drivers/media/rc/keymaps/built-in.a
| CC drivers/media/rc/rc-main.o
| CC drivers/media/rc/rc-ir-raw.o
| CC drivers/media/rc/gpio-ir-recv.o
| AR drivers/media/rc/built-in.a
| AR drivers/media/common/b2c2/built-in.a
| AR drivers/media/common/saa7146/built-in.a
| AR drivers/media/common/siano/built-in.a
| AR drivers/media/common/v4l2-tpg/built-in.a
| CC drivers/media/common/videobuf2/videobuf2-core.o
| CC drivers/media/common/videobuf2/videobuf2-v4l2.o
| CC drivers/media/common/videobuf2/videobuf2-memops.o
| CC drivers/media/common/videobuf2/videobuf2-vmalloc.o
| CC drivers/media/common/videobuf2/videobuf2-dma-contig.o
| AR drivers/media/common/videobuf2/built-in.a
| AR drivers/media/common/built-in.a
| AR drivers/media/platform/ti-vpe/built-in.a
| AR drivers/media/platform/stm32/built-in.a
| AR drivers/media/platform/davinci/built-in.a
| AR drivers/media/platform/omap/built-in.a
| CC drivers/media/platform/mxc/output/mxc_vout.o
| CC drivers/media/platform/mxc/output/mxc_pxp_v4l2.o
| AR drivers/media/platform/mxc/output/built-in.a
| AR drivers/media/platform/sunxi/sun4i-csi/built-in.a
| AR drivers/media/platform/sunxi/sun6i-csi/built-in.a
| AR drivers/media/platform/sunxi/sun8i-di/built-in.a
| AR drivers/media/platform/sunxi/sun8i-rotate/built-in.a
| AR drivers/media/platform/sunxi/built-in.a
| CC drivers/media/platform/imx-pxp.o
| CC drivers/media/platform/video-mux.o
| AR drivers/media/platform/built-in.a
| AR drivers/media/pci/ttpci/built-in.a
| AR drivers/media/pci/b2c2/built-in.a
| AR drivers/media/pci/pluto2/built-in.a
| AR drivers/media/pci/dm1105/built-in.a
| AR drivers/media/pci/pt1/built-in.a
| AR drivers/media/pci/pt3/built-in.a
| AR drivers/media/pci/mantis/built-in.a
| AR drivers/media/pci/ngene/built-in.a
| AR drivers/media/pci/ddbridge/built-in.a
| AR drivers/media/pci/saa7146/built-in.a
| AR drivers/media/pci/smipcie/built-in.a
| AR drivers/media/pci/netup_unidvb/built-in.a
| AR drivers/media/pci/intel/ipu3/built-in.a
| AR drivers/media/pci/intel/built-in.a
| AR drivers/media/pci/built-in.a
| AR drivers/media/usb/ttusb-dec/built-in.a
| AR drivers/media/usb/ttusb-budget/built-in.a
| AR drivers/media/usb/dvb-usb/built-in.a
| AR drivers/media/usb/dvb-usb-v2/built-in.a
| AR drivers/media/usb/siano/built-in.a
| AR drivers/media/usb/b2c2/built-in.a
| AR drivers/media/usb/zr364xx/built-in.a
| AR drivers/media/usb/stkwebcam/built-in.a
| AR drivers/media/usb/s2255/built-in.a
| AR drivers/media/usb/built-in.a
| AR drivers/media/mmc/siano/built-in.a
| AR drivers/media/mmc/built-in.a
| AR drivers/media/firewire/built-in.a
| AR drivers/media/spi/built-in.a
| AR drivers/media/test-drivers/built-in.a
| CC drivers/media/radio/radio-si476x.o
| AR drivers/media/radio/built-in.a
| AR drivers/media/built-in.a
| AR drivers/pps/clients/built-in.a
| AR drivers/pps/generators/built-in.a
| CC drivers/pps/pps.o
| CC drivers/pps/kapi.o
| CC drivers/pps/sysfs.o
| AR drivers/pps/built-in.a
| CC drivers/ptp/ptp_clock.o
| CC drivers/ptp/ptp_chardev.o
| CC drivers/ptp/ptp_sysfs.o
| AR drivers/ptp/built-in.a
| CC drivers/power/reset/syscon-reboot.o
| CC drivers/power/reset/syscon-poweroff.o
| AR drivers/power/reset/built-in.a
| CC drivers/power/supply/power_supply_core.o
| CC drivers/power/supply/power_supply_sysfs.o
| CC drivers/power/supply/power_supply_leds.o
| CC drivers/power/supply/power_supply_hwmon.o
| CC drivers/power/supply/sabresd_battery.o
| AR drivers/power/supply/built-in.a
| AR drivers/power/built-in.a
| CC drivers/hwmon/hwmon.o
| CC drivers/hwmon/gpio-fan.o
| CC drivers/hwmon/iio_hwmon.o
| CC drivers/hwmon/max17135-hwmon.o
| CC drivers/hwmon/mc13783-adc.o
| CC drivers/hwmon/mag3110.o
| CC drivers/hwmon/mxc_mma8451.o
| AR drivers/hwmon/built-in.a
| AR drivers/thermal/broadcom/built-in.a
| AR drivers/thermal/samsung/built-in.a
| AR drivers/thermal/intel/built-in.a
| AR drivers/thermal/st/built-in.a
| AR drivers/thermal/tegra/built-in.a
| CC drivers/thermal/thermal_core.o
| CC drivers/thermal/thermal_sysfs.o
| CC drivers/thermal/thermal_helpers.o
| CC drivers/thermal/thermal_hwmon.o
| CC drivers/thermal/thermal_of.o
| CC drivers/thermal/gov_step_wise.o
| CC drivers/thermal/cpufreq_cooling.o
| CC drivers/thermal/imx_thermal.o
| CC drivers/thermal/device_cooling.o
| AR drivers/thermal/built-in.a
| CC drivers/watchdog/watchdog_core.o
| CC drivers/watchdog/watchdog_dev.o
| CC drivers/watchdog/rn5t618_wdt.o
| CC drivers/watchdog/imx2_wdt.o
| CC drivers/watchdog/imx7ulp_wdt.o
| CC drivers/watchdog/da9062_wdt.o
| AR drivers/watchdog/built-in.a
| CC drivers/md/dm-builtin.o
| AR drivers/md/built-in.a
| CC drivers/bluetooth/hci_vhci.o
| CC drivers/bluetooth/hci_ldisc.o
| CC drivers/bluetooth/hci_serdev.o
| CC drivers/bluetooth/hci_h4.o
| CC drivers/bluetooth/hci_bcsp.o
| CC drivers/bluetooth/hci_ll.o
| CC drivers/bluetooth/hci_h5.o
| CC drivers/bluetooth/hci_mrvl.o
| CC drivers/bluetooth/btusb.o
| CC drivers/bluetooth/btintel.o
| CC drivers/bluetooth/btmrvl_main.o
| CC drivers/bluetooth/btmrvl_debugfs.o
| CC drivers/bluetooth/btmrvl_sdio.o
| CC drivers/bluetooth/btbcm.o
| CC drivers/bluetooth/btrtl.o
| AR drivers/bluetooth/built-in.a
| CC drivers/opp/core.o
| CC drivers/opp/cpu.o
| CC drivers/opp/of.o
| CC drivers/opp/debugfs.o
| AR drivers/opp/built-in.a
| CC drivers/cpufreq/cpufreq.o
| CC drivers/cpufreq/freq_table.o
| CC drivers/cpufreq/cpufreq_stats.o
| CC drivers/cpufreq/cpufreq_performance.o
| CC drivers/cpufreq/cpufreq_powersave.o
| CC drivers/cpufreq/cpufreq_userspace.o
| CC drivers/cpufreq/cpufreq_ondemand.o
| CC drivers/cpufreq/cpufreq_conservative.o
| CC drivers/cpufreq/cpufreq_governor.o
| CC drivers/cpufreq/cpufreq_governor_attr_set.o
| CC drivers/cpufreq/cpufreq-dt.o
| CC drivers/cpufreq/cpufreq-dt-platdev.o
| CC drivers/cpufreq/imx6q-cpufreq.o
| CC drivers/cpufreq/imx-cpufreq-dt.o
| AR drivers/cpufreq/built-in.a
| CC drivers/cpuidle/governors/menu.o
| AR drivers/cpuidle/governors/built-in.a
| CC drivers/cpuidle/cpuidle.o
| CC drivers/cpuidle/driver.o
| CC drivers/cpuidle/governor.o
| CC drivers/cpuidle/sysfs.o
| CC drivers/cpuidle/dt_idle_states.o
| CC drivers/cpuidle/cpuidle-arm.o
| CC drivers/cpuidle/cpuidle-psci.o
| CC drivers/cpuidle/cpuidle-psci-domain.o
| AR drivers/cpuidle/built-in.a
| CC drivers/mmc/core/core.o
| CC drivers/mmc/core/bus.o
| CC drivers/mmc/core/host.o
| CC drivers/mmc/core/mmc.o
| CC drivers/mmc/core/mmc_ops.o
| CC drivers/mmc/core/sd.o
| CC drivers/mmc/core/sd_ops.o
| CC drivers/mmc/core/sdio.o
| CC drivers/mmc/core/sdio_ops.o
| CC drivers/mmc/core/sdio_bus.o
| CC drivers/mmc/core/sdio_cis.o
| CC drivers/mmc/core/sdio_io.o
| CC drivers/mmc/core/sdio_irq.o
| CC drivers/mmc/core/slot-gpio.o
| CC drivers/mmc/core/regulator.o
| CC drivers/mmc/core/pwrseq.o
| CC drivers/mmc/core/debugfs.o
| CC drivers/mmc/core/pwrseq_simple.o
| CC drivers/mmc/core/pwrseq_emmc.o
| CC drivers/mmc/core/block.o
| CC drivers/mmc/core/queue.o
| AR drivers/mmc/core/built-in.a
| CC drivers/mmc/host/sdhci.o
| CC drivers/mmc/host/sdhci-pltfm.o
| CC drivers/mmc/host/sdhci-esdhc-imx.o
| CC drivers/mmc/host/cqhci.o
| AR drivers/mmc/host/built-in.a
| AR drivers/mmc/built-in.a
| CC drivers/leds/trigger/ledtrig-timer.o
| CC drivers/leds/trigger/ledtrig-oneshot.o
| CC drivers/leds/trigger/ledtrig-heartbeat.o
| CC drivers/leds/trigger/ledtrig-backlight.o
| CC drivers/leds/trigger/ledtrig-gpio.o
| CC drivers/leds/trigger/ledtrig-default-on.o
| AR drivers/leds/trigger/built-in.a
| CC drivers/leds/led-core.o
| CC drivers/leds/led-class.o
| CC drivers/leds/led-triggers.o
| CC drivers/leds/leds-gpio.o
| CC drivers/leds/leds-pwm.o
| AR drivers/leds/built-in.a
| AR drivers/firmware/arm_scmi/built-in.a
| AR drivers/firmware/broadcom/built-in.a
| AR drivers/firmware/meson/built-in.a
| CC drivers/firmware/imx/s400-api.o
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/drivers/firmware/imx/s400-api.c: In function 's4_muap_ioctl_img_auth_cmd_handler':
| /home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/drivers/firmware/imx/s400-api.c:446:24: warning: cast to pointer from integer of different size [-Wint-to-pointer-cast]
| 446 | memcpy((void *)img->dst, (const void *)(img->offset + phdr),
| | ^
| AR drivers/firmware/imx/built-in.a
| CC drivers/firmware/psci/psci.o
| AR drivers/firmware/psci/built-in.a
| CC drivers/firmware/smccc/smccc.o
| CC drivers/firmware/smccc/soc_id.o
| AR drivers/firmware/smccc/built-in.a
| AR drivers/firmware/tegra/built-in.a
| AR drivers/firmware/xilinx/built-in.a
| AR drivers/firmware/built-in.a
| AR drivers/crypto/hisilicon/built-in.a
| CC drivers/crypto/mxs-dcp.o
| CC drivers/crypto/sahara.o
| AR drivers/crypto/built-in.a
| CC drivers/clocksource/timer-of.o
| CC drivers/clocksource/timer-probe.o
| CC drivers/clocksource/mmio.o
| CC drivers/clocksource/arm_arch_timer.o
| CC drivers/clocksource/dummy_timer.o
| CC drivers/clocksource/timer-imx-gpt.o
| CC drivers/clocksource/timer-imx-tpm.o
| AR drivers/clocksource/built-in.a
| CC drivers/hid/usbhid/hid-core.o
| AR drivers/hid/usbhid/built-in.a
| CC drivers/hid/hid-core.o
| CC drivers/hid/hid-input.o
| CC drivers/hid/hid-quirks.o
| CC drivers/hid/hid-debug.o
| CC drivers/hid/hid-generic.o
| CC drivers/hid/hid-multitouch.o
| AR drivers/hid/built-in.a
| CC drivers/of/base.o
| CC drivers/of/device.o
| CC drivers/of/platform.o
| CC drivers/of/property.o
| CC drivers/of/kobj.o
| CC drivers/of/dynamic.o
| CC drivers/of/fdt.o
| CC drivers/of/fdt_address.o
| CC drivers/of/address.o
| CC drivers/of/irq.o
| CC drivers/of/of_net.o
| CC drivers/of/of_reserved_mem.o
| CC drivers/of/resolver.o
| CC drivers/of/overlay.o
| AR drivers/of/built-in.a
| AR drivers/staging/media/built-in.a
| AR drivers/staging/iio/accel/built-in.a
| AR drivers/staging/iio/adc/built-in.a
| AR drivers/staging/iio/addac/built-in.a
| AR drivers/staging/iio/cdc/built-in.a
| AR drivers/staging/iio/frequency/built-in.a
| AR drivers/staging/iio/impedance-analyzer/built-in.a
| AR drivers/staging/iio/meter/built-in.a
| AR drivers/staging/iio/resolver/built-in.a
| AR drivers/staging/iio/built-in.a
| AR drivers/staging/android/ion/built-in.a
| AR drivers/staging/android/built-in.a
| AR drivers/staging/hikey9xx/built-in.a
| AR drivers/staging/built-in.a
| AR drivers/platform/built-in.a
| CC drivers/mailbox/mailbox.o
| CC drivers/mailbox/imx-mailbox.o
| AR drivers/mailbox/built-in.a
| CC drivers/remoteproc/remoteproc_core.o
| CC drivers/remoteproc/remoteproc_coredump.o
| CC drivers/remoteproc/remoteproc_debugfs.o
| CC drivers/remoteproc/remoteproc_sysfs.o
| CC drivers/remoteproc/remoteproc_virtio.o
| CC drivers/remoteproc/remoteproc_elf_loader.o
| CC drivers/remoteproc/imx_rproc.o
| AR drivers/remoteproc/built-in.a
| CC drivers/rpmsg/rpmsg_core.o
| CC drivers/rpmsg/rpmsg_ns.o
| CC drivers/rpmsg/virtio_rpmsg_bus.o
| CC drivers/rpmsg/imx_rpmsg.o
| AR drivers/rpmsg/built-in.a
| CC drivers/extcon/extcon.o
| CC drivers/extcon/devres.o
| CC drivers/extcon/extcon-usb-gpio.o
| AR drivers/extcon/built-in.a
| AR drivers/iio/accel/built-in.a
| CC drivers/iio/adc/imx7d_adc.o
| CC drivers/iio/adc/rn5t618-adc.o
| CC drivers/iio/adc/vf610_adc.o
| AR drivers/iio/adc/built-in.a
| AR drivers/iio/afe/built-in.a
| AR drivers/iio/amplifiers/built-in.a
| CC drivers/iio/buffer/industrialio-triggered-buffer.o
| CC drivers/iio/buffer/kfifo_buf.o
| AR drivers/iio/buffer/built-in.a
| AR drivers/iio/chemical/built-in.a
| AR drivers/iio/common/cros_ec_sensors/built-in.a
| AR drivers/iio/common/hid-sensors/built-in.a
| AR drivers/iio/common/ms_sensors/built-in.a
| AR drivers/iio/common/scmi_sensors/built-in.a
| AR drivers/iio/common/ssp_sensors/built-in.a
| AR drivers/iio/common/st_sensors/built-in.a
| AR drivers/iio/common/built-in.a
| AR drivers/iio/dac/built-in.a
| AR drivers/iio/dummy/built-in.a
| AR drivers/iio/gyro/built-in.a
| AR drivers/iio/frequency/built-in.a
| AR drivers/iio/health/built-in.a
| AR drivers/iio/humidity/built-in.a
| AR drivers/iio/imu/bmi160/built-in.a
| AR drivers/iio/imu/inv_icm42600/built-in.a
| AR drivers/iio/imu/inv_mpu6050/built-in.a
| AR drivers/iio/imu/st_lsm6dsx/built-in.a
| AR drivers/iio/imu/built-in.a
| AR drivers/iio/light/built-in.a
| AR drivers/iio/magnetometer/built-in.a
| AR drivers/iio/multiplexer/built-in.a
| AR drivers/iio/orientation/built-in.a
| AR drivers/iio/position/built-in.a
| AR drivers/iio/potentiometer/built-in.a
| AR drivers/iio/potentiostat/built-in.a
| AR drivers/iio/pressure/built-in.a
| AR drivers/iio/proximity/built-in.a
| AR drivers/iio/resolver/built-in.a
| AR drivers/iio/temperature/built-in.a
| AR drivers/iio/trigger/built-in.a
| CC drivers/iio/industrialio-core.o
| CC drivers/iio/industrialio-event.o
| CC drivers/iio/inkern.o
| CC drivers/iio/industrialio-buffer.o
| CC drivers/iio/industrialio-trigger.o
| AR drivers/iio/built-in.a
| CC drivers/perf/arm_pmu.o
| CC drivers/perf/arm_pmu_platform.o
| AR drivers/perf/built-in.a
| AR drivers/hwtracing/intel_th/built-in.a
| CC drivers/nvmem/core.o
| CC drivers/nvmem/imx-ocotp.o
| CC drivers/nvmem/snvs_lpgpr.o
| CC drivers/nvmem/imx-ocotp-fsb-s400.o
| AR drivers/nvmem/built-in.a
| CC drivers/tee/optee/core.o
| CC drivers/tee/optee/call.o
| CC drivers/tee/optee/rpc.o
| CC drivers/tee/optee/supp.o
| CC drivers/tee/optee/shm_pool.o
| CC drivers/tee/optee/device.o
| AR drivers/tee/optee/built-in.a
| CC drivers/tee/tee_core.o
| CC drivers/tee/tee_shm.o
| CC drivers/tee/tee_shm_pool.o
| AR drivers/tee/built-in.a
| CC drivers/mux/core.o
| CC drivers/mux/mmio.o
| AR drivers/mux/built-in.a
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_math.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_debug.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_debugfs.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_allocator.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/allocator/default/gc_hal_kernel_allocator_user_memory.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/allocator/default/gc_hal_kernel_allocator_dma.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/allocator/default/gc_hal_kernel_allocator_gfp.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/allocator/default/gc_hal_kernel_allocator_reserved_mem.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_driver.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/platform/freescale/gc_hal_kernel_platform_imx.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/allocator/default/gc_hal_kernel_allocator_dmabuf.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_iommu.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_drm.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_command.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_db.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_event.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_heap.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_mmu.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_video_memory.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_power.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_security_v1.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_context.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_hardware.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_hardware_func.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_hardware_func_flop_reset.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_hardware_async_fe.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_hardware_mc_fe.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_hardware_waitlink_fe.o
| CC drivers/mxc/gpu-viv/hal/kernel/arch/gc_hal_kernel_recorder.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_vg.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_command_vg.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_interrupt_vg.o
| CC drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel_mmu_vg.o
| CC drivers/mxc/gpu-viv/hal/kernel/archvg/gc_hal_kernel_hardware_command_vg.o
| CC drivers/mxc/gpu-viv/hal/kernel/archvg/gc_hal_kernel_hardware_vg.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_sync.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.o
| CC drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_security_channel_emulator.o
| CC drivers/mxc/gpu-viv/hal/security_v1/gc_hal_ta.o
| CC drivers/mxc/gpu-viv/hal/security_v1/gc_hal_ta_hardware.o
| CC drivers/mxc/gpu-viv/hal/security_v1/gc_hal_ta_mmu.o
| CC drivers/mxc/gpu-viv/hal/security_v1/os/emulator/gc_hal_ta_emulator.o
| AR drivers/mxc/gpu-viv/built-in.a
| CC drivers/mxc/sim/imx_sim.o
| AR drivers/mxc/sim/built-in.a
| CC drivers/mxc/mlb/mxc_mlb.o
| AR drivers/mxc/mlb/built-in.a
| CC drivers/mxc/ipu3/ipu_common.o
| CC drivers/mxc/ipu3/ipu_ic.o
| CC drivers/mxc/ipu3/ipu_disp.o
| CC drivers/mxc/ipu3/ipu_capture.o
| CC drivers/mxc/ipu3/ipu_device.o
| CC drivers/mxc/ipu3/ipu_calc_stripes_sizes.o
| CC drivers/mxc/ipu3/vdoa.o
| CC drivers/mxc/ipu3/ipu_pixel_clk.o
| CC drivers/mxc/ipu3/prg.o
| CC drivers/mxc/ipu3/pre.o
| AR drivers/mxc/ipu3/built-in.a
| CC drivers/mxc/hdmi-cec/mxc_hdmi-cec.o
| AR drivers/mxc/hdmi-cec/built-in.a
| CC drivers/mxc/vpu/mxc_vpu.o
| AR drivers/mxc/vpu/built-in.a
| CC drivers/mxc/mipi/mxc_mipi_csi2.o
| AR drivers/mxc/mipi/built-in.a
| AR drivers/mxc/built-in.a
| AR drivers/built-in.a
| CC sound/core/sound.o
| CC sound/core/init.o
| CC sound/core/memory.o
| CC sound/core/control.o
| CC sound/core/misc.o
| CC sound/core/device.o
| CC sound/core/info.o
| CC sound/core/vmaster.o
| CC sound/core/ctljack.o
| CC sound/core/jack.o
| CC sound/core/timer.o
| CC sound/core/pcm.o
| CC sound/core/pcm_native.o
| CC sound/core/pcm_lib.o
| CC sound/core/pcm_misc.o
| CC sound/core/pcm_memory.o
| CC sound/core/memalloc.o
| CC sound/core/pcm_timer.o
| CC sound/core/pcm_drm_eld.o
| CC sound/core/pcm_iec958.o
| CC sound/core/pcm_dmaengine.o
| CC sound/core/rawmidi.o
| AR sound/core/built-in.a
| AR sound/i2c/other/built-in.a
| AR sound/i2c/built-in.a
| AR sound/drivers/opl3/built-in.a
| AR sound/drivers/opl4/built-in.a
| AR sound/drivers/mpu401/built-in.a
| AR sound/drivers/vx/built-in.a
| AR sound/drivers/pcsp/built-in.a
| AR sound/drivers/built-in.a
| AR sound/isa/ad1816a/built-in.a
| AR sound/isa/ad1848/built-in.a
| AR sound/isa/cs423x/built-in.a
| AR sound/isa/es1688/built-in.a
| AR sound/isa/galaxy/built-in.a
| AR sound/isa/gus/built-in.a
| AR sound/isa/msnd/built-in.a
| AR sound/isa/opti9xx/built-in.a
| AR sound/isa/sb/built-in.a
| AR sound/isa/wavefront/built-in.a
| AR sound/isa/wss/built-in.a
| AR sound/isa/built-in.a
| CC sound/pci/ac97/ac97_codec.o
| CC sound/pci/ac97/ac97_pcm.o
| CC sound/pci/ac97/ac97_proc.o
| AR sound/pci/ac97/built-in.a
| AR sound/pci/ali5451/built-in.a
| AR sound/pci/asihpi/built-in.a
| AR sound/pci/au88x0/built-in.a
| AR sound/pci/aw2/built-in.a
| AR sound/pci/ctxfi/built-in.a
| AR sound/pci/ca0106/built-in.a
| AR sound/pci/cs46xx/built-in.a
| AR sound/pci/cs5535audio/built-in.a
| AR sound/pci/lola/built-in.a
| AR sound/pci/lx6464es/built-in.a
| AR sound/pci/echoaudio/built-in.a
| AR sound/pci/emu10k1/built-in.a
| AR sound/pci/hda/built-in.a
| AR sound/pci/ice1712/built-in.a
| AR sound/pci/korg1212/built-in.a
| AR sound/pci/mixart/built-in.a
| AR sound/pci/nm256/built-in.a
| AR sound/pci/oxygen/built-in.a
| AR sound/pci/pcxhr/built-in.a
| AR sound/pci/riptide/built-in.a
| AR sound/pci/rme9652/built-in.a
| AR sound/pci/trident/built-in.a
| AR sound/pci/ymfpci/built-in.a
| AR sound/pci/vx222/built-in.a
| AR sound/pci/built-in.a
| AR sound/ppc/built-in.a
| AR sound/arm/built-in.a
| AR sound/sh/built-in.a
| AR sound/synth/built-in.a
| AR sound/usb/misc/built-in.a
| AR sound/usb/usx2y/built-in.a
| AR sound/usb/caiaq/built-in.a
| AR sound/usb/6fire/built-in.a
| AR sound/usb/hiface/built-in.a
| AR sound/usb/bcd2000/built-in.a
| AR sound/usb/built-in.a
| AR sound/firewire/built-in.a
| AR sound/sparc/built-in.a
| AR sound/spi/built-in.a
| AR sound/parisc/built-in.a
| AR sound/pcmcia/vx/built-in.a
| AR sound/pcmcia/pdaudiocf/built-in.a
| AR sound/pcmcia/built-in.a
| AR sound/mips/built-in.a
| CC sound/soc/codecs/ac97.o
| CC sound/soc/codecs/cs42xx8.o
| CC sound/soc/codecs/cs42xx8-i2c.o
| CC sound/soc/codecs/es8328.o
| CC sound/soc/codecs/es8328-i2c.o
| CC sound/soc/codecs/es8328-spi.o
| CC sound/soc/codecs/mc13783.o
| CC sound/soc/codecs/hdmi-codec.o
| CC sound/soc/codecs/sgtl5000.o
| CC sound/soc/codecs/si476x.o
| CC sound/soc/codecs/tlv320aic23.o
| CC sound/soc/codecs/tlv320aic23-i2c.o
| CC sound/soc/codecs/tlv320aic3x.o
| CC sound/soc/codecs/wm8960.o
| CC sound/soc/codecs/wm8962.o
| CC sound/soc/codecs/wm8994.o
| CC sound/soc/codecs/wm8958-dsp2.o
| CC sound/soc/codecs/wm_hubs.o
| CC sound/soc/codecs/rpmsg_wm8960.o
| CC sound/soc/codecs/rpmsg_wm8960_i2c.o
| AR sound/soc/codecs/built-in.a
| CC sound/soc/generic/simple-card-utils.o
| CC sound/soc/generic/simple-card.o
| AR sound/soc/generic/built-in.a
| AR sound/soc/adi/built-in.a
| AR sound/soc/amd/built-in.a
| AR sound/soc/atmel/built-in.a
| AR sound/soc/au1x/built-in.a
| AR sound/soc/bcm/built-in.a
| AR sound/soc/cirrus/built-in.a
| AR sound/soc/dwc/built-in.a
| CC sound/soc/fsl/fsl-asoc-card.o
| CC sound/soc/fsl/fsl_asrc.o
| CC sound/soc/fsl/fsl_asrc_dma.o
| CC sound/soc/fsl/fsl_sai.o
| CC sound/soc/fsl/fsl_sai_sysfs.o
| CC sound/soc/fsl/fsl_ssi.o
| CC sound/soc/fsl/fsl_ssi_dbg.o
| CC sound/soc/fsl/fsl_spdif.o
| CC sound/soc/fsl/fsl_esai.o
| CC sound/soc/fsl/fsl_esai_mix.o
| CC sound/soc/fsl/fsl_utils.o
| CC sound/soc/fsl/fsl_mqs.o
| CC sound/soc/fsl/fsl_hdmi.o
| CC sound/soc/fsl/fsl_rpmsg.o
| CC sound/soc/fsl/imx-ssi.o
| CC sound/soc/fsl/imx-audmux.o
| CC sound/soc/fsl/imx-pcm-dma.o
| CC sound/soc/fsl/imx-pcm-dma-v2.o
| CC sound/soc/fsl/imx-audio-rpmsg.o
| CC sound/soc/fsl/imx-pcm-rpmsg.o
| CC sound/soc/fsl/imx-hdmi-dma.o
| AS sound/soc/fsl/hdmi_pcm.o
| CC sound/soc/fsl/eukrea-tlv320.o
| CC sound/soc/fsl/imx-es8328.o
| CC sound/soc/fsl/imx-sgtl5000.o
| CC sound/soc/fsl/imx-wm8958.o
| CC sound/soc/fsl/imx-sii902x.o
| CC sound/soc/fsl/imx-spdif.o
| CC sound/soc/fsl/imx-mc13783.o
| CC sound/soc/fsl/imx-rpmsg.o
| CC sound/soc/fsl/imx-si476x.o
| CC sound/soc/fsl/imx-hdmi.o
| AR sound/soc/fsl/built-in.a
| AR sound/soc/hisilicon/built-in.a
| AR sound/soc/jz4740/built-in.a
| AR sound/soc/img/built-in.a
| AR sound/soc/intel/common/built-in.a
| AR sound/soc/intel/boards/built-in.a
| AR sound/soc/intel/built-in.a
| AR sound/soc/mediatek/built-in.a
| AR sound/soc/meson/built-in.a
| AR sound/soc/mxs/built-in.a
| AR sound/soc/kirkwood/built-in.a
| AR sound/soc/pxa/built-in.a
| AR sound/soc/qcom/built-in.a
| AR sound/soc/rockchip/built-in.a
| AR sound/soc/samsung/built-in.a
| AR sound/soc/sh/built-in.a
| AR sound/soc/sirf/built-in.a
| AR sound/soc/sof/built-in.a
| AR sound/soc/spear/built-in.a
| AR sound/soc/sprd/built-in.a
| AR sound/soc/sti/built-in.a
| AR sound/soc/stm/built-in.a
| AR sound/soc/sunxi/built-in.a
| AR sound/soc/tegra/built-in.a
| AR sound/soc/ti/built-in.a
| AR sound/soc/txx9/built-in.a
| AR sound/soc/uniphier/built-in.a
| AR sound/soc/ux500/built-in.a
| AR sound/soc/xilinx/built-in.a
| AR sound/soc/xtensa/built-in.a
| AR sound/soc/zte/built-in.a
| CC sound/soc/soc-core.o
| CC sound/soc/soc-dapm.o
| CC sound/soc/soc-jack.o
| CC sound/soc/soc-utils.o
| CC sound/soc/soc-dai.o
| CC sound/soc/soc-component.o
| CC sound/soc/soc-pcm.o
| CC sound/soc/soc-devres.o
| CC sound/soc/soc-ops.o
| CC sound/soc/soc-link.o
| CC sound/soc/soc-card.o
| CC sound/soc/soc-generic-dmaengine-pcm.o
| CC sound/soc/soc-ac97.o
| AR sound/soc/built-in.a
| AR sound/atmel/built-in.a
| AR sound/hda/built-in.a
| AR sound/x86/built-in.a
| AR sound/xen/built-in.a
| CC sound/sound_core.o
| CC sound/ac97_bus.o
| CC sound/last.o
| AR sound/built-in.a
| CC net/core/sock.o
| CC net/core/request_sock.o
| CC net/core/skbuff.o
| CC net/core/datagram.o
| CC net/core/stream.o
| CC net/core/scm.o
| CC net/core/gen_stats.o
| CC net/core/gen_estimator.o
| CC net/core/net_namespace.o
| CC net/core/secure_seq.o
| CC net/core/flow_dissector.o
| CC net/core/sysctl_net_core.o
| CC net/core/dev.o
| CC net/core/dev_addr_lists.o
| CC net/core/dst.o
| CC net/core/netevent.o
| CC net/core/neighbour.o
| CC net/core/rtnetlink.o
| CC net/core/utils.o
| CC net/core/link_watch.o
| CC net/core/filter.o
| CC net/core/sock_diag.o
| CC net/core/dev_ioctl.o
| CC net/core/tso.o
| CC net/core/sock_reuseport.o
| CC net/core/fib_notifier.o
| CC net/core/xdp.o
| CC net/core/flow_offload.o
| CC net/core/net-sysfs.o
| CC net/core/net-procfs.o
| CC net/core/ptp_classifier.o
| CC net/core/dst_cache.o
| CC net/core/gro_cells.o
| AR net/core/built-in.a
| CC net/llc/llc_core.o
| CC net/llc/llc_input.o
| CC net/llc/llc_output.o
| CC net/llc/llc_if.o
| CC net/llc/llc_c_ev.o
| CC net/llc/llc_c_ac.o
| CC net/llc/llc_conn.o
| CC net/llc/llc_c_st.o
| CC net/llc/llc_pdu.o
| CC net/llc/llc_sap.o
| CC net/llc/llc_s_ac.o
| CC net/llc/llc_s_ev.o
| CC net/llc/llc_s_st.o
| CC net/llc/af_llc.o
| CC net/llc/llc_station.o
| CC net/llc/llc_proc.o
| CC net/llc/sysctl_net_llc.o
| AR net/llc/built-in.a
| CC net/ethernet/eth.o
| AR net/ethernet/built-in.a
| CC net/802/p8022.o
| CC net/802/psnap.o
| AR net/802/built-in.a
| CC net/sched/sch_generic.o
| CC net/sched/sch_mq.o
| AR net/sched/built-in.a
| CC net/netlink/af_netlink.o
| CC net/netlink/genetlink.o
| CC net/netlink/policy.o
| AR net/netlink/built-in.a
| AR net/bpf/built-in.a
| CC net/ethtool/ioctl.o
| CC net/ethtool/common.o
| CC net/ethtool/netlink.o
| CC net/ethtool/bitset.o
| CC net/ethtool/strset.o
| CC net/ethtool/linkinfo.o
| CC net/ethtool/linkmodes.o
| CC net/ethtool/linkstate.o
| CC net/ethtool/debug.o
| CC net/ethtool/wol.o
| CC net/ethtool/features.o
| CC net/ethtool/privflags.o
| CC net/ethtool/rings.o
| CC net/ethtool/channels.o
| CC net/ethtool/coalesce.o
| CC net/ethtool/pause.o
| CC net/ethtool/eee.o
| CC net/ethtool/tsinfo.o
| CC net/ethtool/cabletest.o
| CC net/ethtool/tunnels.o
| AR net/ethtool/built-in.a
| CC net/netfilter/core.o
| CC net/netfilter/nf_log.o
| CC net/netfilter/nf_queue.o
| CC net/netfilter/nf_sockopt.o
| CC net/netfilter/utils.o
| AR net/netfilter/built-in.a
| AR net/ipv4/netfilter/built-in.a
| CC net/ipv4/route.o
| CC net/ipv4/inetpeer.o
| CC net/ipv4/protocol.o
| CC net/ipv4/ip_input.o
| CC net/ipv4/ip_fragment.o
| CC net/ipv4/ip_forward.o
| CC net/ipv4/ip_options.o
| CC net/ipv4/ip_output.o
| CC net/ipv4/ip_sockglue.o
| CC net/ipv4/inet_hashtables.o
| CC net/ipv4/inet_timewait_sock.o
| CC net/ipv4/inet_connection_sock.o
| CC net/ipv4/tcp.o
| CC net/ipv4/tcp_input.o
| CC net/ipv4/tcp_output.o
| CC net/ipv4/tcp_timer.o
| CC net/ipv4/tcp_ipv4.o
| CC net/ipv4/tcp_minisocks.o
| CC net/ipv4/tcp_cong.o
| CC net/ipv4/tcp_metrics.o
| CC net/ipv4/tcp_fastopen.o
| CC net/ipv4/tcp_rate.o
| CC net/ipv4/tcp_recovery.o
| CC net/ipv4/tcp_ulp.o
| CC net/ipv4/tcp_offload.o
| CC net/ipv4/datagram.o
| CC net/ipv4/raw.o
| CC net/ipv4/udp.o
| CC net/ipv4/udplite.o
| CC net/ipv4/udp_offload.o
| CC net/ipv4/arp.o
| CC net/ipv4/icmp.o
| CC net/ipv4/devinet.o
| CC net/ipv4/af_inet.o
| CC net/ipv4/igmp.o
| CC net/ipv4/fib_frontend.o
| CC net/ipv4/fib_semantics.o
| CC net/ipv4/fib_trie.o
| CC net/ipv4/fib_notifier.o
| CC net/ipv4/inet_fragment.o
| CC net/ipv4/ping.o
| CC net/ipv4/ip_tunnel_core.o
| CC net/ipv4/gre_offload.o
| CC net/ipv4/metrics.o
| CC net/ipv4/netlink.o
| CC net/ipv4/nexthop.o
| CC net/ipv4/udp_tunnel_stub.o
| CC net/ipv4/ip_tunnel.o
| CC net/ipv4/sysctl_net_ipv4.o
| CC net/ipv4/proc.o
| CC net/ipv4/tunnel4.o
| CC net/ipv4/ipconfig.o
| CC net/ipv4/netfilter.o
| CC net/ipv4/inet_diag.o
| CC net/ipv4/tcp_diag.o
| CC net/ipv4/tcp_cubic.o
| AR net/ipv4/built-in.a
| CC net/unix/af_unix.o
| CC net/unix/garbage.o
| CC net/unix/sysctl_net_unix.o
| CC net/unix/scm.o
| AR net/unix/built-in.a
| AR net/ipv6/netfilter/built-in.a
| CC net/ipv6/af_inet6.o
| CC net/ipv6/anycast.o
| CC net/ipv6/ip6_output.o
| CC net/ipv6/ip6_input.o
| CC net/ipv6/addrconf.o
| CC net/ipv6/addrlabel.o
| CC net/ipv6/route.o
| CC net/ipv6/ip6_fib.o
| CC net/ipv6/ipv6_sockglue.o
| CC net/ipv6/ndisc.o
| CC net/ipv6/udp.o
| CC net/ipv6/udplite.o
| CC net/ipv6/raw.o
| CC net/ipv6/icmp.o
| CC net/ipv6/mcast.o
| CC net/ipv6/reassembly.o
| CC net/ipv6/tcp_ipv6.o
| CC net/ipv6/ping.o
| CC net/ipv6/exthdrs.o
| CC net/ipv6/datagram.o
| CC net/ipv6/ip6_flowlabel.o
| CC net/ipv6/inet6_connection_sock.o
| CC net/ipv6/udp_offload.o
| CC net/ipv6/seg6.o
| CC net/ipv6/fib6_notifier.o
| CC net/ipv6/rpl.o
| CC net/ipv6/sysctl_net_ipv6.o
| CC net/ipv6/netfilter.o
| CC net/ipv6/proc.o
| CC net/ipv6/sit.o
| CC net/ipv6/addrconf_core.o
| CC net/ipv6/exthdrs_core.o
| CC net/ipv6/ip6_checksum.o
| CC net/ipv6/ip6_icmp.o
| CC net/ipv6/output_core.o
| CC net/ipv6/protocol.o
| CC net/ipv6/ip6_offload.o
| CC net/ipv6/tcpv6_offload.o
| CC net/ipv6/exthdrs_offload.o
| CC net/ipv6/inet6_hashtables.o
| CC net/ipv6/mcast_snoop.o
| AR net/ipv6/built-in.a
| CC net/packet/af_packet.o
| AR net/packet/built-in.a
| CC net/can/af_can.o
| CC net/can/proc.o
| CC net/can/raw.o
| CC net/can/bcm.o
| CC net/can/gw.o
| AR net/can/built-in.a
| CC net/bluetooth/rfcomm/core.o
| CC net/bluetooth/rfcomm/sock.o
| CC net/bluetooth/rfcomm/tty.o
| AR net/bluetooth/rfcomm/built-in.a
| CC net/bluetooth/bnep/core.o
| CC net/bluetooth/bnep/sock.o
| CC net/bluetooth/bnep/netdev.o
| AR net/bluetooth/bnep/built-in.a
| CC net/bluetooth/hidp/core.o
| CC net/bluetooth/hidp/sock.o
| AR net/bluetooth/hidp/built-in.a
| CC net/bluetooth/af_bluetooth.o
| CC net/bluetooth/hci_core.o
| CC net/bluetooth/hci_conn.o
| CC net/bluetooth/hci_event.o
| CC net/bluetooth/mgmt.o
| CC net/bluetooth/hci_sock.o
| CC net/bluetooth/hci_sysfs.o
| CC net/bluetooth/l2cap_core.o
| CC net/bluetooth/l2cap_sock.o
| CC net/bluetooth/smp.o
| CC net/bluetooth/lib.o
| CC net/bluetooth/ecdh_helper.o
| CC net/bluetooth/hci_request.o
| CC net/bluetooth/mgmt_util.o
| CC net/bluetooth/mgmt_config.o
| CC net/bluetooth/sco.o
| CC net/bluetooth/hci_debugfs.o
| AR net/bluetooth/built-in.a
| CC net/sunrpc/auth_gss/auth_gss.o
| CC net/sunrpc/auth_gss/gss_generic_token.o
| CC net/sunrpc/auth_gss/gss_mech_switch.o
| CC net/sunrpc/auth_gss/svcauth_gss.o
| CC net/sunrpc/auth_gss/gss_rpc_upcall.o
| CC net/sunrpc/auth_gss/gss_rpc_xdr.o
| CC net/sunrpc/auth_gss/trace.o
| AR net/sunrpc/auth_gss/built-in.a
| CC net/sunrpc/clnt.o
| CC net/sunrpc/xprt.o
| CC net/sunrpc/socklib.o
| CC net/sunrpc/xprtsock.o
| CC net/sunrpc/sched.o
| CC net/sunrpc/auth.o
| CC net/sunrpc/auth_null.o
| CC net/sunrpc/auth_unix.o
| CC net/sunrpc/svc.o
| CC net/sunrpc/svcsock.o
| CC net/sunrpc/svcauth.o
| CC net/sunrpc/svcauth_unix.o
| CC net/sunrpc/addr.o
| CC net/sunrpc/rpcb_clnt.o
| CC net/sunrpc/timer.o
| CC net/sunrpc/xdr.o
| CC net/sunrpc/sunrpc_syms.o
| CC net/sunrpc/cache.o
| CC net/sunrpc/rpc_pipe.o
| CC net/sunrpc/svc_xprt.o
| CC net/sunrpc/xprtmultipath.o
| CC net/sunrpc/backchannel_rqst.o
| CC net/sunrpc/stats.o
| CC net/sunrpc/sysctl.o
| AR net/sunrpc/built-in.a
| CC net/8021q/vlan_core.o
| AR net/8021q/built-in.a
| CC net/wireless/core.o
| CC net/wireless/sysfs.o
| CC net/wireless/radiotap.o
| CC net/wireless/util.o
| CC net/wireless/reg.o
| CC net/wireless/scan.o
| CC net/wireless/nl80211.o
| CC net/wireless/mlme.o
| CC net/wireless/ibss.o
| CC net/wireless/sme.o
| CC net/wireless/chan.o
| CC net/wireless/ethtool.o
| CC net/wireless/mesh.o
| CC net/wireless/ap.o
| CC net/wireless/trace.o
| CC net/wireless/ocb.o
| CC net/wireless/pmsr.o
| CC net/wireless/of.o
| CC net/wireless/wext-compat.o
| CC net/wireless/wext-sme.o
| GEN net/wireless/shipped-certs.c
| CC net/wireless/shipped-certs.o
| CC net/wireless/lib80211.o
| CC net/wireless/lib80211_crypt_wep.o
| CC net/wireless/lib80211_crypt_ccmp.o
| CC net/wireless/lib80211_crypt_tkip.o
| CC net/wireless/wext-core.o
| CC net/wireless/wext-proc.o
| CC net/wireless/wext-spy.o
| CC net/wireless/wext-priv.o
| AR net/wireless/built-in.a
| CC net/mac80211/main.o
| CC net/mac80211/status.o
| CC net/mac80211/driver-ops.o
| CC net/mac80211/sta_info.o
| CC net/mac80211/wep.o
| CC net/mac80211/aead_api.o
| CC net/mac80211/wpa.o
| CC net/mac80211/scan.o
| CC net/mac80211/offchannel.o
| CC net/mac80211/ht.o
| CC net/mac80211/agg-tx.o
| CC net/mac80211/agg-rx.o
| CC net/mac80211/vht.o
| CC net/mac80211/he.o
| CC net/mac80211/s1g.o
| CC net/mac80211/ibss.o
| CC net/mac80211/iface.o
| CC net/mac80211/rate.o
| CC net/mac80211/michael.o
| CC net/mac80211/tkip.o
| CC net/mac80211/aes_cmac.o
| CC net/mac80211/aes_gmac.o
| CC net/mac80211/fils_aead.o
| CC net/mac80211/cfg.o
| CC net/mac80211/ethtool.o
| CC net/mac80211/rx.o
| CC net/mac80211/spectmgmt.o
| CC net/mac80211/tx.o
| CC net/mac80211/key.o
| CC net/mac80211/util.o
| CC net/mac80211/wme.o
| CC net/mac80211/chan.o
| CC net/mac80211/trace.o
| CC net/mac80211/mlme.o
| CC net/mac80211/tdls.o
| CC net/mac80211/ocb.o
| CC net/mac80211/airtime.o
| CC net/mac80211/pm.o
| CC net/mac80211/rc80211_minstrel.o
| CC net/mac80211/rc80211_minstrel_ht.o
| AR net/mac80211/built-in.a
| CC net/dns_resolver/dns_key.o
| CC net/dns_resolver/dns_query.o
| AR net/dns_resolver/built-in.a
| CC net/devres.o
| CC net/socket.o
| CC net/sysctl_net.o
| AR net/built-in.a
| AR virt/lib/built-in.a
| AR virt/built-in.a
| AS arch/arm/lib/ashldi3.o
| AS arch/arm/lib/ashrdi3.o
| AS arch/arm/lib/backtrace.o
| AS arch/arm/lib/bswapsdi2.o
| AS arch/arm/lib/call_with_stack.o
| AS arch/arm/lib/changebit.o
| AS arch/arm/lib/clear_user.o
| AS arch/arm/lib/clearbit.o
| AS arch/arm/lib/copy_from_user.o
| AS arch/arm/lib/copy_page.o
| AS arch/arm/lib/copy_to_user.o
| AS arch/arm/lib/csumipv6.o
| AS arch/arm/lib/csumpartial.o
| AS arch/arm/lib/csumpartialcopy.o
| AS arch/arm/lib/csumpartialcopyuser.o
| AS arch/arm/lib/delay-loop.o
| CC arch/arm/lib/delay.o
| AS arch/arm/lib/div64.o
| AS arch/arm/lib/findbit.o
| AS arch/arm/lib/getuser.o
| AS arch/arm/lib/io-readsb.o
| AS arch/arm/lib/io-readsl.o
| AS arch/arm/lib/io-readsw-armv4.o
| AS arch/arm/lib/io-writesb.o
| AS arch/arm/lib/io-writesl.o
| AS arch/arm/lib/io-writesw-armv4.o
| AS arch/arm/lib/lib1funcs.o
| AS arch/arm/lib/lshrdi3.o
| AS arch/arm/lib/memchr.o
| AS arch/arm/lib/memcpy.o
| AS arch/arm/lib/memmove.o
| AS arch/arm/lib/memset.o
| AS arch/arm/lib/muldi3.o
| AS arch/arm/lib/putuser.o
| AS arch/arm/lib/setbit.o
| AS arch/arm/lib/strchr.o
| AS arch/arm/lib/strrchr.o
| AS arch/arm/lib/testchangebit.o
| AS arch/arm/lib/testclearbit.o
| AS arch/arm/lib/testsetbit.o
| AS arch/arm/lib/ucmpdi2.o
| AR arch/arm/lib/lib.a
| AR arch/arm/lib/built-in.a
| CC lib/math/div64.o
| CC lib/math/gcd.o
| CC lib/math/lcm.o
| CC lib/math/int_pow.o
| CC lib/math/int_sqrt.o
| CC lib/math/reciprocal_div.o
| CC lib/math/rational.o
| AR lib/math/built-in.a
| CC lib/crypto/chacha.o
| CC lib/crypto/aes.o
| CC lib/crypto/arc4.o
| CC lib/crypto/sha256.o
| AR lib/crypto/built-in.a
| CC lib/zlib_inflate/inffast.o
| CC lib/zlib_inflate/inflate.o
| CC lib/zlib_inflate/infutil.o
| CC lib/zlib_inflate/inftrees.o
| CC lib/zlib_inflate/inflate_syms.o
| AR lib/zlib_inflate/built-in.a
| CC lib/zlib_deflate/deflate.o
| CC lib/zlib_deflate/deftree.o
| CC lib/zlib_deflate/deflate_syms.o
| AR lib/zlib_deflate/built-in.a
| CC lib/lzo/lzo1x_compress.o
| CC lib/lzo/lzo1x_decompress_safe.o
| AR lib/lzo/built-in.a
| CC lib/lz4/lz4_decompress.o
| AR lib/lz4/built-in.a
| CC lib/zstd/fse_compress.o
| CC lib/zstd/huf_compress.o
| CC lib/zstd/compress.o
| CC lib/zstd/entropy_common.o
| CC lib/zstd/fse_decompress.o
| CC lib/zstd/zstd_common.o
| CC lib/zstd/huf_decompress.o
| CC lib/zstd/decompress.o
| AR lib/zstd/built-in.a
| CC lib/xz/xz_dec_syms.o
| CC lib/xz/xz_dec_stream.o
| CC lib/xz/xz_dec_lzma2.o
| CC lib/xz/xz_dec_bcj.o
| AR lib/xz/built-in.a
| CC lib/mpi/generic_mpih-lshift.o
| CC lib/mpi/generic_mpih-mul1.o
| CC lib/mpi/generic_mpih-mul2.o
| CC lib/mpi/generic_mpih-mul3.o
| CC lib/mpi/generic_mpih-rshift.o
| CC lib/mpi/generic_mpih-sub1.o
| CC lib/mpi/generic_mpih-add1.o
| CC lib/mpi/ec.o
| CC lib/mpi/mpicoder.o
| CC lib/mpi/mpi-add.o
| CC lib/mpi/mpi-bit.o
| CC lib/mpi/mpi-cmp.o
| CC lib/mpi/mpi-sub-ui.o
| CC lib/mpi/mpi-div.o
| CC lib/mpi/mpi-inv.o
| CC lib/mpi/mpi-mod.o
| CC lib/mpi/mpi-mul.o
| CC lib/mpi/mpih-cmp.o
| CC lib/mpi/mpih-div.o
| CC lib/mpi/mpih-mul.o
| CC lib/mpi/mpi-pow.o
| CC lib/mpi/mpiutil.o
| AR lib/mpi/built-in.a
| CC lib/fonts/fonts.o
| CC lib/fonts/font_8x8.o
| CC lib/fonts/font_8x16.o
| AR lib/fonts/built-in.a
| CC lib/argv_split.o
| CC lib/bug.o
| CC lib/clz_tab.o
| CC lib/cmdline.o
| CC lib/cpumask.o
| CC lib/ctype.o
| CC lib/dec_and_lock.o
| CC lib/decompress.o
| CC lib/decompress_bunzip2.o
| CC lib/decompress_inflate.o
| CC lib/decompress_unlz4.o
| CC lib/decompress_unlzma.o
| CC lib/decompress_unlzo.o
| CC lib/decompress_unxz.o
| CC lib/decompress_unzstd.o
| CC lib/dump_stack.o
| CC lib/earlycpio.o
| CC lib/extable.o
| CC lib/fdt.o
| CC lib/fdt_addresses.o
| CC lib/fdt_empty_tree.o
| CC lib/fdt_ro.o
| CC lib/fdt_rw.o
| CC lib/fdt_strerror.o
| CC lib/fdt_sw.o
| CC lib/fdt_wip.o
| CC lib/flex_proportions.o
| CC lib/idr.o
| CC lib/irq_regs.o
| CC lib/is_single_threaded.o
| CC lib/klist.o
| CC lib/kobject.o
| CC lib/kobject_uevent.o
| CC lib/logic_pio.o
| CC lib/memcat_p.o
| CC lib/nmi_backtrace.o
| CC lib/nodemask.o
| CC lib/plist.o
| CC lib/radix-tree.o
| CC lib/ratelimit.o
| CC lib/rbtree.o
| CC lib/seq_buf.o
| CC lib/sha1.o
| CC lib/show_mem.o
| CC lib/siphash.o
| CC lib/string.o
| CC lib/timerqueue.o
| CC lib/vsprintf.o
| CC lib/win_minmax.o
| CC lib/xarray.o
| AR lib/lib.a
| CC lib/lockref.o
| CC lib/bcd.o
| CC lib/sort.o
| CC lib/parser.o
| CC lib/debug_locks.o
| CC lib/random32.o
| CC lib/bust_spinlocks.o
| CC lib/kasprintf.o
| CC lib/bitmap.o
| CC lib/scatterlist.o
| CC lib/list_sort.o
| CC lib/uuid.o
| CC lib/iov_iter.o
| CC lib/clz_ctz.o
| CC lib/bsearch.o
| CC lib/find_bit.o
| CC lib/llist.o
| CC lib/memweight.o
| CC lib/kfifo.o
| CC lib/percpu-refcount.o
| CC lib/rhashtable.o
| CC lib/once.o
| CC lib/refcount.o
| CC lib/usercopy.o
| CC lib/errseq.o
| CC lib/bucket_locks.o
| CC lib/generic-radix-tree.o
| CC lib/string_helpers.o
| CC lib/hexdump.o
| CC lib/kstrtox.o
| CC lib/pci_iomap.o
| CC lib/iomap_copy.o
| CC lib/devres.o
| CC lib/hweight.o
| CC lib/assoc_array.o
| CC lib/bitrev.o
| CC lib/linear_ranges.o
| CC lib/crc16.o
| CC lib/crc-t10dif.o
| HOSTCC lib/gen_crc32table
| GEN lib/crc32table.h
| CC lib/crc32.o
| CC lib/xxhash.o
| CC lib/genalloc.o
| CC lib/percpu_counter.o
| CC lib/syscall.o
| CC lib/errname.o
| CC lib/nlattr.o
| CC lib/cpu_rmap.o
| CC lib/dynamic_queue_limits.o
| CC lib/glob.o
| CC lib/strncpy_from_user.o
| CC lib/strnlen_user.o
| CC lib/net_utils.o
| CC lib/sg_pool.o
| CC lib/stmp_device.o
| CC lib/asn1_decoder.o
| GEN lib/oid_registry_data.c
| CC lib/oid_registry.o
| CC lib/sbitmap.o
| AR lib/built-in.a
| GEN .version
| CHK include/generated/compile.h
| LD vmlinux.o
| MODPOST vmlinux.symvers
| MODINFO modules.builtin.modinfo
| GEN modules.builtin
| LD .tmp_vmlinux.kallsyms1
| KSYMS .tmp_vmlinux.kallsyms1.S
| AS .tmp_vmlinux.kallsyms1.S
| LD .tmp_vmlinux.kallsyms2
| KSYMS .tmp_vmlinux.kallsyms2.S
| AS .tmp_vmlinux.kallsyms2.S
| LD vmlinux
| SORTTAB vmlinux
| SYSMAP System.map
| OBJCOPY arch/arm/boot/Image
| Kernel: arch/arm/boot/Image is ready
| LDS arch/arm/boot/compressed/vmlinux.lds
| AS arch/arm/boot/compressed/head.o
| LZO arch/arm/boot/compressed/piggy_data
| AS arch/arm/boot/compressed/piggy.o
| CC arch/arm/boot/compressed/misc.o
| CC arch/arm/boot/compressed/decompress.o
| CC arch/arm/boot/compressed/string.o
| SHIPPED arch/arm/boot/compressed/hyp-stub.S
| AS arch/arm/boot/compressed/hyp-stub.o
| SHIPPED arch/arm/boot/compressed/lib1funcs.S
| AS arch/arm/boot/compressed/lib1funcs.o
| SHIPPED arch/arm/boot/compressed/ashldi3.S
| AS arch/arm/boot/compressed/ashldi3.o
| SHIPPED arch/arm/boot/compressed/bswapsdi2.S
| AS arch/arm/boot/compressed/bswapsdi2.o
| LD arch/arm/boot/compressed/vmlinux
| OBJCOPY arch/arm/boot/zImage
| Kernel: arch/arm/boot/zImage is ready
| NOTE: make -j 1 HOSTCC=gcc -isystem/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/osboxes/imx-yocto-bsp/build-first/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 HOSTCPP=gcc -E HOSTCXX=g++ -isystem/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/osboxes/imx-yocto-bsp/build-first/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 imx6ull-14x14-evk.dtb CC=arm-fslc-linux-gnueabi-gcc -mno-thumb-interwork -marm -fuse-ld=bfd -fmacro-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0=/usr/src/debug/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0 -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0=/usr/src/debug/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0 -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot= -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source=/usr/src/kernel LD=arm-fslc-linux-gnueabi-ld.bfd LOADADDR=0x80008000
| SYNC include/config/auto.conf.cmd
| GEN Makefile
| DTC arch/arm/boot/dts/imx6ull-14x14-evk.dtb
| NOTE: make -j 1 HOSTCC=gcc -isystem/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/osboxes/imx-yocto-bsp/build-first/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 HOSTCPP=gcc -E HOSTCXX=g++ -isystem/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -L/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/osboxes/imx-yocto-bsp/build-first/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 imx6ull-14x14-evk-btwifi-sdio3_0.dtb CC=arm-fslc-linux-gnueabi-gcc -mno-thumb-interwork -marm -fuse-ld=bfd -fmacro-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0=/usr/src/debug/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0 -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0=/usr/src/debug/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0 -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot= -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work/imx6ullevk-fslc-linux-gnueabi/linux-fslc-imx/5.10.74+gitAUTOINC+b0d74a58e2-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source=/usr/src/kernel LD=arm-fslc-linux-gnueabi-ld.bfd LOADADDR=0x80008000
| make[2]: *** No rule to make target 'arch/arm/boot/dts/imx6ull-14x14-evk-btwifi-sdio3_0.dtb'. Stop.
| make[1]: *** [/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/Makefile:1355: imx6ull-14x14-evk-btwifi-sdio3_0.dtb] Error 2
| make: *** [/home/osboxes/imx-yocto-bsp/build-first/tmp/work-shared/imx6ullevk/kernel-source/Makefile:185: __sub-make] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/osboxes/imx-yocto-bsp/sources/meta-freescale/recipes-kernel/linux/linux-fslc-imx_5.10.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 501 tasks of which 486 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 5 seconds
Summary: 1 task failed:
/home/osboxes/imx-yocto-bsp/sources/meta-freescale/recipes-kernel/linux/linux-fslc-imx_5.10.bb:do_compile
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
>>>>
BR
Can you share your steps?