Hi,
I'm having a strange problem booting my board from SD-Card
When mounting rootfs as read-only, it boots fine. But as long as I try to boot in read-write mode, the kernel panics.
I'm using a Seco Q7 board iMX6Q based, kernel 3.10.17ga-1.0.1
That's my kernel bootargs which works fine:
Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk0p1 rootdelay=1 ro mem=1024M arm_freq=792
And that's the problematic one:
Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk0p1 rootdelay=1 rw mem=1024M arm_freq=792
That's the message I get from console:
VFS: Cannot open root device "mmcblk0p1" or unknown-block(179,1): error -30
Please append a correct "root=" boot option; here are the available partitions:
b300 15212544 mmcblk0 driver: mmcblk
b301 1048576 mmcblk0p1 a89529c2-01
b302 14162944 mmcblk0p2 a89529c2-02
b308 3866624 mmcblk1 driver: mmcblk
b309 3865600 mmcblk1p1 af9f8377-01
b320 512 mmcblk1rpmb (driver?)
b318 2048 mmcblk1boot1 (driver?)
b310 2048 mmcblk1boot0 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,1)
I've also tried putting the sd-card in a USB adapter, loading the kernel from TFTP and the rootfs from the USB adapter, and it also works fine. So nothing wrong with the card and the FS.
Any thoughts?
Solved! Go to Solution.
There are no invalid arguments. As you can see, the only modification in bootargs is the change from ro to rw, and those seem to be pretty standard ones.
Anyway, I've upgraded uboot to the latest version (2015.04) and now it works fine.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Carlos
FSL BSP has kernel parameters as in attached document
Table 8. Kernel Boot Parameters, seems linux ignore bootargs
if encounters invalid argument. I think you can post this problem
to Seco Q7 forum or add source modifications so this parameter
become valid.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
There are no invalid arguments. As you can see, the only modification in bootargs is the change from ro to rw, and those seem to be pretty standard ones.
Anyway, I've upgraded uboot to the latest version (2015.04) and now it works fine.