New Linux 11.09 BSP Patch for the i.MX53 -blog archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New Linux 11.09 BSP Patch for the i.MX53 -blog archive

1,288 次查看
EnriqueOchoaVaz
Contributor V

The new i.MX53 Linux 11.09 patch is now available on the www.freescale.com page.

 

Name

Description

Web Link

IMX53_LINUX_1109_BSP_PATCH

Patch based on L2.6.35_11_09_ER_SOURCE, to provide: GPU driver update, Uboot update for plug-in mode support on Ripley QSB, VPU firmware update and other fixes

Link

IMX53_1109_LINUX_MMDOCS

Linux Multimedia Codecs Documentation. Includes CODECs Release Notes and User's Guide

Link

IMX53_11_09_LINUX_MMCODECS

Linux Multimedia Codecs Documentation and Sources 11.09 for i.MX53 for the Quick Start boards.

Link

AACP_CODECS_LINUX_11_09

AAC Plus Codec for Linux 11.09.

Link

   

Note:The codecs packages have been updated , the revision number and the date of the packages were updated to reflect the changes.

   

  •  Target HW boards
    • MCIMX53-START-R
    • MCIMX53-START
  • Issues solved
    • BSP part:
      • Uboot update for plug-in mode support on MCIMX53-START-R
      • Reset set to 4s
      • GPU microcode update with version 1020, The new GPU driver fix a random GPU hang issue that happens when a 3D application is running when the external memory bus is heavy loaded by other applications. 
      • DMA zone increase to 112M
      • I2C fix : reboot  I2C instable issue
      • Dialog fix
      • VPU firmware update
      • Bug fixes
    • MM part
      • Bug fixes
  • What are the main issues left
    • For known issues and limitations please consult the release notes.
标记 (1)
0 项奖励
回复
3 回复数

963 次查看
HenriBragge
Contributor I

How much do you encourage moving to 2.6.38? How well is different i.MX boards supported and tested, compared to 2.6.35.3?

0 项奖励
回复

963 次查看
KrishnaPavan
Contributor II

For Example ::

user@ubuntu:~/imx53/11.09.01/ltib$ cat ltib-fix-rpm-flag.patch
user@ubuntu:~/imx53/11.09.01/ltib$ patch -p 0 < ltib-fix-rpm-flag.patch

Open the patch file, you will find all the modifications, relative to patching of files.

0 项奖励
回复

963 次查看
Vinay_123
Contributor I

Dear  Enrique Ochoa Vazquez,

How are we going to update that patch in BSP. And how to verfiy whether patch is updated or not.?

Vinay Kumar

0 项奖励
回复