Hi Team ,
I have followed the https://www.nxp.com/docs/en/application-note/AN11697.pdf document and did the changes in yocto project kernel 4.14 . Driver is compiled successfully , .o file is generated . But I am not getting any debug message in my OS booting logs .
Driver is not getting registered .
Kindly suggest me for the same as soon as possible .
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
## dts file changes in imx8mm-evk.dts
pinctrl_i2c3: i2c3grp {
fsl,pins = <
MX8MM_IOMUXC_I2C3_SCL_I2C3_SCL 0x400001c3
MX8MM_IOMUXC_I2C3_SDA_I2C3_SDA 0x400001c3
MX8MM_IOMUXC_SAI1_TXC_GPIO4_IO11 0x41 /* Changes done for pn5xx */
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41 /* Changes done for pn5xx */
>;
};
------
------
&i2c3 {
clock-frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c3>;
status = "okay";
nfc:pn544@28 {
status = "okay";
compatible = "nxp,pn544";
reg = <0x28>;
clock-frequency = <400000>;
interrupt-gpios = <&gpio3 24 0>;
enable-gpios = <&gpio4 11 0>;
};
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Best regards ,
Pramod