NVCC_PLL pin i.MX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVCC_PLL pin i.MX6ULL

1,438件の閲覧回数
ban45
Contributor III

Hi

I connected 3.3V to the NVCC_PLL pin.
Will i.MX6ULL work?
Could you tell me the meaning of NVCC?

best regard.

0 件の賞賛
5 返答(返信)

1,431件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX 6ULL NVCC_PLL  is internal LDO output of 1.1 V - only capacitors (1×0.22uF+1×10uF)
should be connected with it. External voltage of 3.3V to the NVCC_PLL pin - definitely  is not
acceptable.

Regards,
Yuri.

0 件の賞賛

1,423件の閲覧回数
ban45
Contributor III

Hi

What if I don't connect a capacitor?

Will it happen that it does not oscillate without a capacitor?

best regard

0 件の賞賛

1,421件の閲覧回数
Yuri
NXP Employee
NXP Employee

LDO outputs require some capacitors to get stable voltage.

~Yuri.

0 件の賞賛

1,419件の閲覧回数
ban45
Contributor III

Hi

Thank you for your reply.
Does the installed capacitor act as a bypass capacitor?

best regard

0 件の賞賛

1,412件の閲覧回数
Yuri
NXP Employee
NXP Employee

yes.

0 件の賞賛