imx8qxp-mek开发板,yocto编译的4.14.98的内核和2018.03的BootLoader。
并使用example_kernel_emmc.uuu 修改为附件的烧录文件uuu_emmc.uuu。
内核与BootLoader在Ubuntu14.04下编译完毕后,cmd命令行使用uuu.exe uuu_emmc.uuu烧录(在Windows 10下操作 uuu.exe SDPS: boot -f u-boot.bin 现象相同)。提示:
I have replied your another same case, you can follow that one, any update, pls reply there
Hi Joanxie,
I have a same issue, Do you have a solution to fix that?
My error is :
[HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f imx-boot-imx8qxpmek-sd.bin-flash
Is there any different way to flash image in imx8qxp?