I successfully cross compiled with LTIB the linphone application from the fs.bluewind.it website.
I downloaded the kernel on the board, the problem is that the rootfs.jffs2 is to big to fit on the NOR flash...
So i tried to boot from nfs...
My daemon nfs is working correctly because i can mount it from a distant computer...
But I am not able to do it from the iMX27 board
Here is what i did :fis load kernel
exec -c "root=/dev/nfs nfsroot=192.168.49.30:/tftpboot console=ttymxc0 ip=192.168.49.179:192.168.49.30:192.168.49.254:255.255.255.0:imx27:
ff"
here is what i get :eth0: using half-duplex 10Base-T (RJ-45)
IP-Config: Complete:
device=eth0, addr=192.168.49.179, mask=255.255.255.0, gw=192.168.49.254,
host=imx27, domain=, nis-domain=(none),
bootserver=192.168.49.30, rootserver=192.168.49.30, rootpath=
Looking up port of RPC 100003/2 on 192.168.49.30
Looking up port of RPC 100005/1 on 192.168.49.30
VFS: Mounted root (nfs filesystem).
Freeing init memory: 192K
Setting the hostname to freescale
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Mounting filesystems
Starting syslogd and klogd
Running depmod
Setting up networking on loopback device:
Setting up networking on eth0:
Adding static route for default gateway to 172.27.255.254:
nfs: server 192.168.49.30 not responding, still trying
nfs: server 192.168.49.30 not responding, still trying
Thanks for your help,
aurelien