My mx6dl sabre board stop at 'Waiting for root device dev/mmcblk0p2... '

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

My mx6dl sabre board stop at 'Waiting for root device dev/mmcblk0p2... '

ソリューションへジャンプ
4,319件の閲覧回数
wenmingfeng
Contributor III

Hello, 

I have a mx6dl sabresd customer board, when I changed all the pins and make uboot working, It can boot and starting the kernel but stopped at "Waiting for root device dev/mmcblk0p2...", please help me.

Is it a filesystem issue or my board HW not working? the Board I used is customerize from imx6dl sabresd. and boot it from a SD card.

Size: 5692616, got: 5692616
5692616 bytes read in 10770 ms (515.6 KiB/s)
Initial value for argc=3
Final value for argc=3
Booting from mmc ...
Initial value for argc=6
Final value for argc=6
test(4): 'try' '=' 'yes': returns 1
Command failed, result=1test(4): 'try' '=' 'try': returns 0
reading imx6dl-sabresd.dtb
VFAT Support enabled
FAT12, fat_sect: 1, fatlength: 8
Rootdir begins at cluster: 0, sector: 17, offset: 2200
Data begins at: 33
Sector size: 512, cluster size: 8
FAT read(sect=17, cnt:2), clust_size=8, DIRENTSPERBLOCK=16
Rootvfatname: |imx6dl-sabresd.dtb|
RootName: imx6dl~1.dtb, start: 0x3, size: 0xa935
Filesize: 43317 bytes
43317 bytes
FAT12: entry: 0x0003 = 3, offset: 0x0003 = 3
FAT12: ret: 00000004, offset: 0003
FAT12: entry: 0x0004 = 4, offset: 0x0004 = 4
FAT12: ret: 00000005, offset: 0004
FAT12: entry: 0x0005 = 5, offset: 0x0005 = 5
FAT12: ret: 00000006, offset: 0005
FAT12: entry: 0x0006 = 6, offset: 0x0006 = 6
FAT12: ret: 00000007, offset: 0006
FAT12: entry: 0x0007 = 7, offset: 0x0007 = 7
FAT12: ret: 00000008, offset: 0007
FAT12: entry: 0x0008 = 8, offset: 0x0008 = 8
FAT12: ret: 00000009, offset: 0008
FAT12: entry: 0x0009 = 9, offset: 0x0009 = 9
FAT12: ret: 0000000a, offset: 0009
FAT12: entry: 0x000a = 10, offset: 0x000a = 10
FAT12: ret: 0000000b, offset: 000a
FAT12: entry: 0x000b = 11, offset: 0x000b = 11
FAT12: ret: 0000000c, offset: 000b
FAT12: entry: 0x000c = 12, offset: 0x000c = 12
FAT12: ret: 0000000d, offset: 000c
gc - clustnum: 3, startsect: 57
Size: 43317, got: 43317
43317 bytes read in 127 ms (333 KiB/s)
Initial value for argc=3
Final value for argc=3
## Current stack ends at 0x4ef3b800 * kernel: cmdline image address = 0x12000000
Kernel image @ 0x12000000 [ 0x000000 - 0x56dcc8 ]
## Skipping init Ramdisk
## No init Ramdisk
ramdisk start = 0x00000000, ramdisk end = 0x00000000
* fdt: cmdline image address = 0x18000000
## Checking for 'FDT'/'FDT Image' at 18000000
* fdt: raw FDT blob
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
of_flat_tree at 0x18000000 size 0x0000a935
Initial value for argc=3
Final value for argc=3
using: FDT
## initrd_high = 0xffffffff, copy_to_ram = 0
ramdisk load start = 0x00000000, ramdisk load end = 0x00000000
Using Device Tree in place at 18000000, end 1800d934
Initial value for argc=3
Final value for argc=3
No alias for ethernet0
switch to ldo_bypass mode!
## Transferring control to Linux (at address 12000000)...

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 3.14.52 (lucid@ubuntu) (gcc version 4.9.4 20151028 (prerelease) (Linaro GCC 4.9-2016.02) ) #1 SMP PREEMPT Tue Jan 17 07:36:38 PST 2017
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 DualLite SABRE Smart Device Board
cma: CMA: reserved 320 MiB at 3c000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @ab732000 s8320 r8192 d16256 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 700324K/1048576K available (7144K kernel code, 438K rwdata, 2444K rodata, 268K init, 417K bss, 348252K reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x8096526c (9589 kB)
.init : 0x80966000 - 0x809a9080 ( 269 kB)
.data : 0x809aa000 - 0x80a17a80 ( 439 kB)
.bss : 0x80a17a8c - 0x80a7ffb4 ( 418 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 512 kB
failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22
VPU 352M is enabled!
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x106d2998 - 0x106d29f0
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (12.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6DL, silicon rev 1.3
Use WDOG2 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1100 mV
vdd3p0: 2625 <--> 3400 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2400 mV
vddarm: 725 <--> 1450 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
usb_otg_vbus: 5000 mV
usb_h1_vbus: 5000 mV
wm8962-supply: no parameters
mipi_dsi_pwr_on: no parameters
sensor-supply: 3300 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usbphy_nop1.12 supply vcc not found, using dummy regulator
usbphy_nop2.13 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: Max17135 PMIC not found!
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 2007
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight.28 supply power not found, using dummy regulator
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
MIPI DSI driver module loaded
mxc_sdc_fb fb.25: registered mxc display driver ldb
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0x1a:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb.26: registered mxc display driver hdmi
mxc_hdmi 20e0000.hdmi_video: Read EDID again
imx_epdc_fb 20f4000.epdc: Unable to get display PMIC regulator.err = 0xfffffdfb
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.2
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1175 mV
SW1C: 300 <--> 1875 mV at 1175 mV
SW2: 800 <--> 3300 mV at 3000 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 1975 mV at 1800 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 800 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 3000 mV
VGEN6: 1800 <--> 3300 mV at 2800 mV
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
mxc_hdmi 20e0000.hdmi_video: create default modelist
console [ttymxc0] enabled
serial: Freescale lpuart driver
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
m25p80 spi0.0: found mr25h256, expected m25p32
m25p80 spi0.0: mr25h256 (32 Kbytes)
spi_imx 2008000.ecspi: probed
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
mxc_v4l2_output v4l2_out.31: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.31: V4L2 device registered as video17
mxc_v4l2_output v4l2_out.31: V4L2 device registered as video18
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
galcore: clk_get vg clock failed, disable vg!
Galcore version 5.0.11.33433
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_vpu 2040000.vpu: VPU initialized
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a160100 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 5a 9c fa 4a 4a 90 ed 7d
platform caam_sm: [0008] 48 8b e5 c0 88 ac 79 cf
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 02 97 91 2f 9a 88 8c 47
platform caam_sm: [0008] 23 c7 a0 5a 55 f9 7b 45
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 05 12 aa 81 e6 ab 76 15
platform caam_sm: [0008] 6a c7 0a fe 93 a5 3c 3d
platform caam_sm: [0016] 57 5f de 8c 56 6b 56 23
platform caam_sm: [0024] 80 ab 6e 7f 3e 1b 9e b6
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 1f 39 c7 41 70 b4 60 a5
platform caam_sm: [0008] 8e 01 4a 8f ed 39 a6 8d
platform caam_sm: [0016] 90 f9 51 76 ff 5d e8 fa
platform caam_sm: [0024] 5a 4e d7 79 9f cc 9f af
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 29 d6 15 aa 2f a9 10 33
platform caam_sm: [0008] 7b 6e 80 30 1e 99 fb 93
platform caam_sm: [0016] c4 74 4f 8c 66 39 cd 5c
platform caam_sm: [0024] 21 f0 d3 31 51 e0 c4 b0
platform caam_sm: [0032] f1 4f 21 9b a8 ea 61 f0
platform caam_sm: [0040] 5f ce 08 3e 80 44 c1 21
platform caam_sm: [0048] 0c a3 a8 cf 12 b3 28 51
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] e7 59 4b 72 4a a9 3f 87
platform caam_sm: [0008] 44 78 aa c3 5b d2 02 7e
platform caam_sm: [0016] 6d 39 f3 e1 46 72 dd 06
platform caam_sm: [0024] e3 e0 7d d7 1f b6 6d bc
platform caam_sm: [0032] 38 86 04 38 9f 56 4e ab
platform caam_sm: [0040] 3e 36 77 ce 79 de 35 80
platform caam_sm: [0048] 86 16 81 e8 7b fa ac da
platform caam_sm: [0056] 15 41 23 7d 14 c7 6b e8
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] cc 09 e2 a7 71 7a 15 36
platform caam_sm: [0008] 5a 46 94 3f 81 55 63 e3
platform caam_sm: [0016] 54 e2 af 70 17 4d 9f 8b
platform caam_sm: [0024] 91 c5 5e bf 04 2b 39 e0
platform caam_sm: [0032] 77 84 35 f2 00 2d 75 6b
platform caam_sm: [0040] ee 1c 7c 16 a2 4a d5 f1
platform caam_sm: [0048] 6b 7b 01 2e 0d da 35 15
platform caam_sm: [0056] f2 0c be ce e6 95 d2 99
platform caam_sm: [0064] 51 5a ed 62 11 47 74 b4
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 11 72 cb ad 89 2c d4 4d
platform caam_sm: [0008] e3 d6 6b 2f df 16 09 6d
platform caam_sm: [0016] 25 ec e9 0f bc 9d 95 60
platform caam_sm: [0024] 7d 4a ad c7 2a c6 35 ad
platform caam_sm: [0032] e0 1e c7 b6 39 a0 02 7b
platform caam_sm: [0040] 8a 17 de 1b 66 cb 83 03
platform caam_sm: [0048] 18 9f fc 19 91 ff 74 54
platform caam_sm: [0056] d3 62 77 aa ed 0e e4 d8
platform caam_sm: [0064] 2f 5d fd f9 6e 6d 87 a0
platform caam_sm: [0072] 20 01 18 43 ce b4 a2 b3
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 0b 3b fc b8 7b 0b 31 32
platform caam_sm: [0008] 96 77 79 a5 83 88 27 c9
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 02 97 91 2f 9a 88 8c 47
platform caam_sm: [0008] 23 c7 a0 5a 55 f9 7b 45
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 05 12 aa 81 e6 ab 76 15
platform caam_sm: [0008] 6a c7 0a fe 93 a5 3c 3d
platform caam_sm: [0016] 92 6a c6 b1 74 e6 9f 67
platform caam_sm: [0024] 0d 42 58 57 0f 63 2e 55
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 1f 39 c7 41 70 b4 60 a5
platform caam_sm: [0008] 8e 01 4a 8f ed 39 a6 8d
platform caam_sm: [0016] 90 f9 51 76 ff 5d e8 fa
platform caam_sm: [0024] 5a 4e d7 79 9f cc 9f af
snvs-secvio 20cc000.caam-snvs: can't get snvs clock
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
fsl-asrc 2034000.asrc: driver registered
imx-wm8962 sound.23: failed to find codec platform device
imx-wm8962: probe of sound.23 failed with error -22
imx-audio-hdmi sound-hdmi.24: hdmi-hifi <-> hdmi_audio.3 mapping ok
NET: Registered protocol family 26
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
failed to disable 1.2 GHz OPP
remove 396MHz OPP for VPU running at 352MHz!
increase SOC/PU voltage for VPU352MHz
VGEN2: disabling
SWBST: disabling
SW4: disabling
wm8962-supply: disabling
usb_otg_vbus: disabling
regulator-dummy: disabling
input: gpio-keys.22 as /devices/soc0/gpio-keys.22/input/input2
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)
ALSA device list:
#0: imx-hdmi-soc
Waiting for root device /dev/mmcblk0p2...

Thanks ahead.

Wenming

ラベル(2)
1 解決策
3,296件の閲覧回数
vinodmaverickr0
Contributor IV

Hi Wenming,

From the u-boot side I think there is no issue. It looks fine to me. But can you please share the pin muxing and device tree changes; you did in the kernel level.

In dtsi file card detect pin should be something like

MX6QDL_PAD_GPIO_1__GPIO1_IO01  0x1f059    /* CD */

Also please have a look in your device tree for the below details :

&usdhc1 {  // As you are using the mmc0 for SD card booting

cd-gpios = <&gpio1 1 GPIO_ACTIVE_LOW>;

bus-witdh=<4>;

}

Thanks,

Vinod

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,297件の閲覧回数
vinodmaverickr0
Contributor IV

Hi Wenming,

From the u-boot side I think there is no issue. It looks fine to me. But can you please share the pin muxing and device tree changes; you did in the kernel level.

In dtsi file card detect pin should be something like

MX6QDL_PAD_GPIO_1__GPIO1_IO01  0x1f059    /* CD */

Also please have a look in your device tree for the below details :

&usdhc1 {  // As you are using the mmc0 for SD card booting

cd-gpios = <&gpio1 1 GPIO_ACTIVE_LOW>;

bus-witdh=<4>;

}

Thanks,

Vinod

0 件の賞賛
返信
3,296件の閲覧回数
wenmingfeng
Contributor III

Thank Vinod,

After I upgrade the kernel to the latest one. rootfs works for my customer board.

3,296件の閲覧回数
wenmingfeng
Contributor III

Hi Vinod,

Thanks for your help, I am no lucky.

The dtsi changes I done in attached,  modified the usdhc2 to usdhc1 at line 752, and the CD pin and WP pin is used GPIO_1_IO01 and GPIO_1_IO09 which I changed in the pinctrl_hog. Any thing missed please help.

pastedImage_1.png

the uboot console mmc part: 

pastedImage_1.png

imx6qdl-sabresd {
pinctrl_hog: hoggrp {
fsl,pins = <
MX6QDL_PAD_NANDF_D0__GPIO2_IO00 0x80000000
MX6QDL_PAD_NANDF_D1__GPIO2_IO01 0x80000000
MX6QDL_PAD_GPIO_1__GPIO1_IO01 0x80000000
MX6QDL_PAD_GPIO_9__GPIO1_IO09 0x80000000
MX6QDL_PAD_GPIO_0__CCM_CLKO1 0x130b0

pinctrl_usdhc1: usdhc1grp {
fsl,pins = <
MX6QDL_PAD_SD1_CMD__SD1_CMD 0x17059
MX6QDL_PAD_SD1_CLK__SD1_CLK 0x10059
MX6QDL_PAD_SD1_DAT0__SD1_DATA0 0x17059
MX6QDL_PAD_SD1_DAT1__SD1_DATA1 0x17059
MX6QDL_PAD_SD1_DAT2__SD1_DATA2 0x17059
MX6QDL_PAD_SD1_DAT3__SD1_DATA3 0x17059
>;
};

&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc1>;
bus-width = <4>;
cd-gpios = <&gpio1 1 0>;
wp-gpios = <&gpio1 9 0>;
no-1-8-v;
keep-power-in-suspend;
enable-sdio-wakeup;
status = "okay";
};

after change the conflicts mutex usage, I got bellow error and kernel panic.

mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 sending stop command, original cmd response 0x900, card status 0x400900
mmcblk0: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
mmcblk0: retrying using single block read

mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 0
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 1, nr 7, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 1
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 2, nr 6, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 2
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 3, nr 5, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 3
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 4, nr 4, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 4
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 5, nr 3, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 5
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 6, nr 2, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 6
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 7, nr 1, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 7
Buffer I/O error on device mmcblk0, logical block 0
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 sending stop command, original cmd response 0x900, card status 0x400900
mmcblk0: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
mmcblk0: retrying using single block read
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 0
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 1, nr 7, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 1
random: nonblocking pool is initialized
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 2, nr 6, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 2
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 3, nr 5, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 3
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 4, nr 4, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 4
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 5, nr 3, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 5
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 6, nr 2, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 6
mmc0: Timeout waiting for hardware interrupt.
mmcblk0: error -110 transferring data, sector 7, nr 1, cmd response 0x900, card status 0x0
end_request: I/O error, dev mmcblk0, sector 7
Buffer I/O error on device mmcblk0, logical block 0
mmcblk0: unable to read partition table
wf@ name_to_dev_t name:/dev/mmcblk0p2
wf@ done name_to_dev_t name:mmcblk0p2 res:187695106
wf@ mount_block_root fs_name:ext3 name:/dev/root
wf@do_mount_root name:/dev/root fs:ext3 flag:0x8000 err:-6
wf@ mount_block_root:err=fffffffa
VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2): error -6
Please append a correct "root=" boot option; here are the available partitions:
1f00 32 mtdblock0 (driver?)
b300 15204352 mmcblk0 driver: mmcblk
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
CPU1: stopping
CPU: 1 PID: 0 Comm: swapper/1 Tainted: G W 3.14.52 #12
[<80014884>] (unwind_backtrace) from [<800117c8>] (show_stack+0x10/0x14)
[<800117c8>] (show_stack) from [<806b9698>] (dump_stack+0x7c/0xbc)
[<806b9698>] (dump_stack) from [<80013830>] (handle_IPI+0x144/0x158)
[<80013830>] (handle_IPI) from [<80008514>] (gic_handle_irq+0x58/0x5c)
[<80008514>] (gic_handle_irq) from [<80012280>] (__irq_svc+0x40/0x70)
Exception stack(0xa80dbf58 to 0xa80dbfa0)
bf40: a80dbfa0 3b9aca00
bf60: a33f0a35 0000002a a2e9f642 0000002a ab73b0d0 80985fd8 00000001 ab73b0d4
bf80: a80da000 00000000 00000017 a80dbfa0 a6aaaaab 804a5b00 00000113 ffffffff
[<80012280>] (__irq_svc) from [<804a5b00>] (cpuidle_enter_state+0x58/0xec)
[<804a5b00>] (cpuidle_enter_state) from [<804a5c98>] (cpuidle_idle_call+0x104/0x158)
[<804a5c98>] (cpuidle_idle_call) from [<8000f0b0>] (arch_cpu_idle+0x8/0x44)
[<8000f0b0>] (arch_cpu_idle) from [<800631d4>] (cpu_startup_entry+0x100/0x14c)
[<800631d4>] (cpu_startup_entry) from [<100085a4>] (0x100085a4)
------------[ cut here ]------------
WARNING: CPU: 0 PID: 1 at kernel/time/tick-broadcast.c:604 tick_handle_oneshot_broadcast+0x1ac/0x1c8()
Modules linked in:
CPU: 0 PID: 1 Comm: swapper/0 Tainted: G W 3.14.52 #12
[<80014884>] (unwind_backtrace) from [<800117c8>] (show_stack+0x10/0x14)
[<800117c8>] (show_stack) from [<806b9698>] (dump_stack+0x7c/0xbc)
[<806b9698>] (dump_stack) from [<80028ea4>] (warn_slowpath_common+0x6c/0x88)
[<80028ea4>] (warn_slowpath_common) from [<80028f5c>] (warn_slowpath_null+0x1c/0x24)
[<80028f5c>] (warn_slowpath_null) from [<800764c8>] (tick_handle_oneshot_broadcast+0x1ac/0x1c8)
[<800764c8>] (tick_handle_oneshot_broadcast) from [<8001d67c>] (mxc_timer_interrupt+0x2c/0x34)
[<8001d67c>] (mxc_timer_interrupt) from [<80063ad0>] (handle_irq_event_percpu+0x50/0x180)
[<80063ad0>] (handle_irq_event_percpu) from [<80063c3c>] (handle_irq_event+0x3c/0x5c)
[<80063c3c>] (handle_irq_event) from [<80066a74>] (handle_fasteoi_irq+0x84/0x14c)
[<80066a74>] (handle_fasteoi_irq) from [<8006325c>] (generic_handle_irq+0x2c/0x3c)
[<8006325c>] (generic_handle_irq) from [<8000ed80>] (handle_IRQ+0x40/0x90)
[<8000ed80>] (handle_IRQ) from [<800084e8>] (gic_handle_irq+0x2c/0x5c)
[<800084e8>] (gic_handle_irq) from [<80012280>] (__irq_svc+0x40/0x70)
Exception stack(0xa8099da0 to 0xa8099de8)
9da0: 00000000 00204140 809df400 00000000 00000002 00004458 000020d8 f4a00100
9dc0: a8098028 809def70 a8623000 8096804c 00000001 a8099de8 8002ce8c 8002ce9c
9de0: 20000113 ffffffff
[<80012280>] (__irq_svc) from [<8002ce9c>] (__do_softirq+0xc0/0x23c)
[<8002ce9c>] (__do_softirq) from [<8002d2d8>] (irq_exit+0xb8/0xf4)
[<8002d2d8>] (irq_exit) from [<8000ed84>] (handle_IRQ+0x44/0x90)
[<8000ed84>] (handle_IRQ) from [<800084e8>] (gic_handle_irq+0x2c/0x5c)
[<800084e8>] (gic_handle_irq) from [<80012280>] (__irq_svc+0x40/0x70)
Exception stack(0xa8099e70 to 0xa8099eb8)
9e60: 00000001 00000000 00000001 00000000
9e80: 809def70 8096804c a8623000 00000000 00000000 809def70 a8623000 8096804c
9ea0: 00000000 a8099eb8 8006146c 806b7648 60000113 ffffffff
[<80012280>] (__irq_svc) from [<806b7648>] (panic+0x160/0x1b8)
[<806b7648>] (panic) from [<809340a0>] (mount_block_root+0x1b0/0x240)
[<809340a0>] (mount_block_root) from [<80934330>] (mount_root+0x114/0x12c)
[<80934330>] (mount_root) from [<809344e8>] (prepare_namespace+0x1a0/0x1e4)
[<809344e8>] (prepare_namespace) from [<80933cfc>] (kernel_init_freeable+0x1c8/0x1d8)
[<80933cfc>] (kernel_init_freeable) from [<806b5b10>] (kernel_init+0xc/0xe8)
[<806b5b10>] (kernel_init) from [<8000e540>] (ret_from_fork+0x14/0x34)
---[ end trace 3406ff24bd973830 ]---

0 件の賞賛
返信
3,296件の閲覧回数
vinodmaverickr0
Contributor IV

Hi feng,

Please check your SD card detection pin and pin mux for the same (assuming your SD card partitions are correct).

Thanks,

Vinod

0 件の賞賛
返信
3,296件の閲覧回数
wenmingfeng
Contributor III

Hi Vinod,

Thanks for your response, the CD pin  we used is GPIO_1_IO01, and used as USDHC1_CD_GPIO.

#define USDHC1_CD_GPIO IMX_GPIO_NR(1, 1), I also checked the BOOTCFG2 0xe0,  and BOOTCFG1 0x42, for my start at SD card and with regular speed, 4bits bus, that is correctly. please help to point out steps to do or check pointers to get the root cause.

The SD card has two partitions following Installing Ubuntu Rootfs on NXP i.MX6 boards .  I also use buildroot to build the latest release  rel_imx_4.1.15_2.0.0_ga, then use the sudo dd if=sdcard.img of=/dev/sdx to get the SDcard.

static iomux_v3_cfg_t const usdhc1_pads[] = {
MX6_PAD_SD1_CLK__SD1_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_CMD__SD1_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT0__SD1_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT1__SD1_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT2__SD1_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD1_DAT3__SD1_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_GPIO_1__GPIO1_IO01 | MUX_PAD_CTRL(NO_PAD_CTRL), /* CD */
};

Thanks!

Wenming

0 件の賞賛
返信