Murata BT-WiFi V2 adaptor porting to iMX6Q-AI board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Murata BT-WiFi V2 adaptor porting to iMX6Q-AI board

ソリューションへジャンプ
3,516件の閲覧回数
rohitpatle
Contributor III

Dear Wigros Sun,

Thank you for your reply weidong.sun and work posted on the link. It very helpful to me.

Porting BCM4330/BCM43362 WIFI to Android4.2.2 

With with WiFi at my board is working absolutely fine. But while making it for BT i am facing some issue. The adb logcat of the activity is attached for your reference.

-----------------------start-of- log----------------------------------------------

01-01 00:04:22.233  2365  2382 E bt_hci  : startup_timer_expired
01-01 00:04:22.234  2365  2380 E bt_core_module: module_start_up failed to start up "hci_module"
01-01 00:04:22.238  2365  2389 I bt_btu  : btu_task pending for preload complete event
01-01 00:04:22.238  2365  2389 I bt_btu_task: Bluetooth chip preload is complete
01-01 00:04:22.238  2365  2389 I bt_btu  : btu_task received preload complete event
01-01 00:04:22.241  2365  2382 E bt_hci  : command_timed_out hci layer timeout waiting for response to a command. opcode: 0xc03
01-01 00:04:22.241  2365  2382 E bt_hci  : command_timed_out restarting the bluetooth process.
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_HCI
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_L2CAP
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_RFCOMM
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_AVDT
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_AVRC
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_A2D
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_BNEP
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_BTM
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_GAP
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_PAN
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_SDP
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_GATT
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_SMP
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_BTAPP
01-01 00:04:22.249  2365  2389 I         : BTE_InitTraceLevels -- TRC_BTIF
01-01 00:04:22.328  1091  1109 E BluetoothManagerService: MESSAGE_BLUETOOTH_SERVICE_DISCONNECTED: 1
01-01 00:04:22.328  1091  1109 D BluetoothManagerService: Broadcasting onBluetoothServiceDown() to 4 receivers.
01-01 00:04:22.332  1091  1102 I ActivityManager: Process com.android.bluetooth (pid 2365) has died
01-01 00:04:22.333  1091  1102 W ActivityManager: Scheduling restart of crashed service com.android.bluetooth/.btservice.AdapterService in 1000ms
01-01 00:04:22.334  1091  1102 W ActivityManager: Scheduling restart of crashed service com.android.bluetooth/.gatt.GattService in 11000ms
01-01 00:04:22.529  1091  1109 D BluetoothManagerService: MESSAGE_RESTART_BLUETOOTH_SERVICE: Restart IBluetooth service
01-01 00:04:22.573  1091  1109 I ActivityManager: Start proc 2391:com.android.bluetooth/1002 for service com.android.bluetooth/.btservice.AdapterService
01-01 00:04:22.659  2391  2391 I art     : Late-enabling JIT
01-01 00:04:22.690  2391  2391 I art     : JIT created with code_cache_capacity=2MB compile_threshold=1000
01-01 00:04:22.864  2391  2391 D AdapterServiceConfig: Adding HeadsetService
01-01 00:04:22.868  2391  2391 D AdapterServiceConfig: Adding A2dpService
01-01 00:04:22.873  2391  2391 D AdapterServiceConfig: Adding A2dpSinkService
01-01 00:04:22.878  2391  2391 D AdapterServiceConfig: Adding HidService
01-01 00:04:22.883  2391  2391 D AdapterServiceConfig: Adding HealthService
01-01 00:04:22.887  2391  2391 D AdapterServiceConfig: Adding PanService
01-01 00:04:22.891  2391  2391 D AdapterServiceConfig: Adding GattService
01-01 00:04:22.894  2391  2391 D AdapterServiceConfig: Adding BluetoothMapService
01-01 00:04:22.896  2391  2391 D AdapterServiceConfig: Adding AvrcpControllerService
01-01 00:04:22.940  1091  1109 D BluetoothManagerService: Added callback: android.bluetooth.IBluetoothManagerCallback$Stub$Proxy@51fc1d8:true
01-01 00:04:22.949  2391  2391 D BluetoothAdapterState: make() - Creating AdapterState
01-01 00:04:22.962  2391  2391 I bt_bluedroid: init
01-01 00:04:22.962  2391  2405 I BluetoothAdapterState: Entering OffState
01-01 00:04:22.965  2391  2406 I bt_bte_conf: bte_load_ble_conf attempt to load ble stack conf from /etc/bluetooth/ble_stack.conf
01-01 00:04:22.965  2391  2406 E bt_osi_config: config_new unable to open file '/etc/bluetooth/ble_stack.conf': No such file or directory
01-01 00:04:22.965  2391  2406 I bt_bte_conf: bte_load_ble_conf file >/etc/bluetooth/ble_stack.conf< not found
01-01 00:04:22.965  2391  2406 I bt_stack_config: init attempt to load stack conf from /etc/bluetooth/bt_stack.conf
01-01 00:04:22.966  2391  2391 I bt_bluedroid: get_profile_interface socket
01-01 00:04:22.975  2391  2409 D BluetoothAdapterProperties: Address is:22:22:A2:55:D1:2C
01-01 00:04:22.977  2391  2409 W art     : Method processed more than once: void com.android.bluetooth.btservice.AdapterProperties.adapterPropertyChangedCallback(int[], byte[][])
01-01 00:04:22.978  2391  2391 I bt_bluedroid: get_profile_interface sdp
01-01 00:04:22.981  2391  2409 D BluetoothAdapterProperties: Name is: SABREAUTO-MX6Q
01-01 00:04:22.985  2391  2403 I bt_bluedroid: config_hci_snoop_log
01-01 00:04:22.988  1091  1109 D BluetoothManagerService: Broadcasting onBluetoothServiceUp() to 5 receivers.
01-01 00:04:22.993  2391  2405 D BluetoothAdapterState: Current state: OFF, message: 0
01-01 00:04:22.993  2391  2405 D BluetoothAdapterProperties: Setting state to 14
01-01 00:04:22.993  2391  2405 I BluetoothAdapterState: Bluetooth adapter state changed: 10-> 14
01-01 00:04:23.003  2391  2405 D BluetoothBondStateMachine: make
01-01 00:04:23.008  2391  2410 I BluetoothBondStateMachine: StableState(): Entering Off State
01-01 00:04:23.031  2391  2405 I BluetoothAdapterState: Entering PendingCommandState
01-01 00:04:23.065  2391  2391 I BtGatt.JNI: classInitNative(L912): classInitNative: Success!
01-01 00:04:23.079  2391  2391 D BluetoothAdapterService: getAdapterService() - returning com.android.bluetooth.btservice.AdapterService@31282f0
01-01 00:04:23.082  2391  2391 D BtGatt.DebugUtils: handleDebugAction() action=null
01-01 00:04:23.083  2391  2391 D BtGatt.GattService: Received start request. Starting profile...
01-01 00:04:23.083  2391  2391 D BtGatt.GattService: start()
01-01 00:04:23.083  2391  2391 I bt_bluedroid: get_profile_interface gatt
01-01 00:04:23.086  2391  2391 D BluetoothAdapterService: getAdapterService() - returning com.android.bluetooth.btservice.AdapterService@31282f0
01-01 00:04:23.086  2391  2391 D BtGatt.AdvertiseManager: advertise manager created
01-01 00:04:23.107  2391  2391 V BluetoothAdapterState: isTurningOff()=false
01-01 00:04:23.107  2391  2391 V BluetoothAdapterState: isTurningOn()=false
01-01 00:04:23.107  2391  2391 V BluetoothAdapterState: isBleTurningOn()=true
01-01 00:04:23.107  2391  2391 V BluetoothAdapterState: isBleTurningOff()=false
01-01 00:04:23.109  2391  2405 D BluetoothAdapterState: Current state: PENDING_COMMAND, message: 4
01-01 00:04:23.109  2391  2405 I bt_bluedroid: enable
01-01 00:04:23.109  2391  2406 D bt_stack_manager: event_start_up_stack is bringing up the stack.
01-01 00:04:23.109  2391  2406 I bt_hci  : start_up
01-01 00:04:23.118  2391  2406 I bt_vendor: alloc value 0x9b2c87dd
01-01 00:04:23.118  2391  2406 I bt_vendor: init
01-01 00:04:23.118  2391  2406 I bt_vnd_conf: Attempt to load conf from /etc/bluetooth/bt_vendor.conf
01-01 00:04:23.118  2391  2406 D bt_vendor: op for 0
01-01 00:04:23.119  2391  2406 E bt_upio : init_rfkill : open(/sys/class/rfkill/rfkill2/type) failed: No such file or directory (2)
01-01 00:04:23.119  2391  2406 D bt_vendor: op for 0
01-01 00:04:23.119  2391  2406 E bt_upio : init_rfkill : open(/sys/class/rfkill/rfkill2/type) failed: No such file or directory (2)
01-01 00:04:23.120  2391  2406 D bt_hci  : start_up starting async portion
01-01 00:04:23.120  2391  2413 I bt_hci  : event_finish_startup
01-01 00:04:23.120  2391  2413 I bt_hci_h4: hal_open
01-01 00:04:23.120  2391  2413 D bt_vendor: op for 3
01-01 00:04:23.120  2391  2413 I bt_userial_vendor: userial vendor open: opening /dev/ttymxc2
01-01 00:04:23.123  2391  2413 I bt_userial_vendor: device fd = 53 open
01-01 00:04:23.124  2391  2413 D bt_vendor: op for 1
-----------------------End-of-log------------------------------------------------

. For your information my environment details are as follows:

1. Board          iMX6Q-AI

2. OS              Marshmallow 6.0.1

3. Kernel         linux 3.14.52

4. WiFi H/W    Murata WiFi-BT V2 adaptor

For more on this i am attaching the image of my hardware setup. Look forward for your support.

Thank you in advance.

Rohit

ラベル(1)
0 件の賞賛
返信
1 解決策
2,262件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Rohit,

     I don't have detailed documents on how to porting bluetooth for you. I checked android5.1.1 source code on sabresd_mx6dq board, in BoardConfig.mk, BCM4339 BT has beed supported, see following:

---------------------------------

# Broadcom BCM4339 BT
BOARD_HAVE_BLUETOOTH_BCM := true
BOARD_BLUETOOTH_BDROID_BUILDCFG_INCLUDE_DIR := device/fsl/sabresd_6dq/bluetooth

USE_ION_ALLOCATOR := false
USE_GPU_ALLOCATOR := true

---------------------------------

So it is no any problem for you to refer to BT source code for sabresd_mx6dq board, check Marshmallow 6.0.1 source code for sabresd_mx6dq board, please! then move corresponding source code to your board!

Best Regards,

Weidong

元の投稿で解決策を見る

2 返答(返信)
2,263件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Rohit,

     I don't have detailed documents on how to porting bluetooth for you. I checked android5.1.1 source code on sabresd_mx6dq board, in BoardConfig.mk, BCM4339 BT has beed supported, see following:

---------------------------------

# Broadcom BCM4339 BT
BOARD_HAVE_BLUETOOTH_BCM := true
BOARD_BLUETOOTH_BDROID_BUILDCFG_INCLUDE_DIR := device/fsl/sabresd_6dq/bluetooth

USE_ION_ALLOCATOR := false
USE_GPU_ALLOCATOR := true

---------------------------------

So it is no any problem for you to refer to BT source code for sabresd_mx6dq board, check Marshmallow 6.0.1 source code for sabresd_mx6dq board, please! then move corresponding source code to your board!

Best Regards,

Weidong

2,262件の閲覧回数
rohitpatle
Contributor III

Hello Wigros San,

Thank you for your reply.

As suggested i referred  the SD BT code and made the required changes for iMX6Q-AI board. One good thing is now WiFi-BT is working fine on my AI board with Marshmallow.

Currently I am able to transfer image, play media over Bluetooth on my board. But it is through the A2dpsink app (System app) given as part of Android BSP.

Now, further to this I want to achieve the functionality of HFP and A2dp for which want to develop a Android application, but while doing this I am facing below issues:

1. two class (import android.bluetooth.BluetoothA2dpSink and import android.bluetooth.BluetoothAvrcpController)files is not getting import in Android studio.

The source code of Android application i am referring is here .

Could you please guide me on this to realize the hansfree and A2dp functionality on my AI Board.

Thank you,

Rohit 

0 件の賞賛
返信