Hello everyone,
I am trying to activate Multilib Support under Yocto Hardknott.
My local.conf receives this modifications:
require conf/multilib.conf
MULTILIBS = "multilib:lib32"
DEFAULTTUNE_virtclass-multilib-lib32 = "armv7athf-neon"
IMAGE_INSTALL_append = " lib32-glibc lib32-libgcc lib32-libstdc++ lib32-openssl"
Unfortunately I end up with several issues. One is right at the beginning of compile process:
ERROR: Nothing PROVIDES 'virtual/arm-pokymllib32-linux-gnueabi-binutils'. Close matches:
virtual/lib32-arm-pokymllib32-linux-gnueabi-binutils
virtual/lib32-arm-pokymllib32-linux-gnueabi-gcc
virtual/lib32-arm-pokymllib32-linux-gnueabi-go-runtime
ERROR: Nothing PROVIDES 'virtual/arm-pokymllib32-linux-gnueabi-gcc'. Close matches:
virtual/lib32-arm-pokymllib32-linux-gnueabi-g++
virtual/lib32-arm-pokymllib32-linux-gnueabi-gcc
virtual/lib32-arm-pokymllib32-linux-gnueabi-go-runtime
With this error, sometimes the compilation process does not abort, and I can even get an Image. Is there anything wrong in this configuration?
What is the state of Multilib Support on Hardknott atm.?
Regards,
Max
Hello,
After investigating with team, the problem was caused by the package management. Multilib is not supported by the yocto package management so it went wrong while packing the lib32 into rootfs file.
I have succeded in building the yocto L5.15.71 with multilib by commenting the following item in the local.conf file.
#PACKAGE_CLASSES = "package_deb"
#EXTRA_IMAGE_FEATURES += "package-management"
This operation will make the package-management back to default red hat package-management.
Regards
Hello,
Which yocto are you based on? SInce multilib is supported in latest 5.15.71 BSP please download.
Regards