Missing software for AN13075

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing software for AN13075

Jump to solution
1,295 Views
Juozas
Contributor III

Hi everyone,

I'm trying to locate software mentioned in application note AN13075 but it seems I can't find it anywhere. I'm specifically interested in this – "Open the “Map_PXP_LCDIF_SingleTast” project." (on page 33).

My 1st question: where I can download mentioned application code?

Screenshot 2022-04-18 at 17.50.39.png

I tried looking in Documentation tab in iMXRT1170 page, also in other forum threads (some of those are from 2 years ago).

My 2nd question: any chance I could have that "Offline tool that converts SVG to Elementary structures" ?

image.png

 

Thank you.

0 Kudos
Reply
1 Solution
1,113 Views
KelvinQi
NXP Employee
NXP Employee

It's already released, you can check it out by clicking the link

View solution in original post

4 Replies
1,290 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Juozas,

Neither the software nor the offline tool have been released yet and are currently on the process of being updated and tested. Sorry for the inconvenience this may cause.

Below the title of the i.MX RT1170 main page, you will find a “Receive alerts” hyperlink which will notify you as soon as a new design resource (in this case, AN13075SW.zip) is released: https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...

In the meantime, I recommend looking into the vglite examples found in the SDK.

 

I hope this helps,

Edwin.

0 Kudos
Reply
1,157 Views
abdulhameed_moh
Contributor I

Hello,

Is the  AN13075SW.zip released? What is the current status?

0 Kudos
Reply
1,114 Views
KelvinQi
NXP Employee
NXP Employee

It's already released, you can check it out by clicking the link

1,110 Views
Juozas
Contributor III

Hi,

Any chance you could look into this question?

Duplicate information in AN13075SW

0 Kudos
Reply