Mipi Camera AutoFocus in SabreSD Lollipop 5.0 Release

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mipi Camera AutoFocus in SabreSD Lollipop 5.0 Release

624 次查看
himanshugusain
Contributor III

Hi Community

We are unable to see the auto-focus functionality in the Lollipop

5.0.2 release of Free-scale.

We don't see Camera2 app auto focusing while capturing images

Please let us know what all things we need to add/modify in order

to make this functionality working.

Camera we are using OV5640 Mipi

Regards

Himanshu

标签 (3)
标记 (2)
0 项奖励
2 回复数

414 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Himanshu

this feature was discussed on yocto meta-freescale mail list, so one can reuse it:

https://www.mail-archive.com/meta-freescale@yoctoproject.org/msg15825.html//www.mail-archive.com/meta-freescale@yoctoproject.org/msg15825.html

https://www.mail-archive.com/meta-freescale@yoctoproject.org/msg15861.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励

414 次查看
himanshugusain
Contributor III

Hello Igor

I have taken the firmware code from the above link

But i can see Autofocus firmware download when i launch apk

but when i take picture the firmware doesn't gets downloaded

It seems like we need to enable AF support in above layers

You have any information on that ?

Regards

Himanshu

0 项奖励