Memory requirment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory requirment

718 Views
adityaprajapati
Contributor I

I am using IMX6UL EVK board for development of my project.

i just want to get knowledge about few things such as memory allocation required for OS.

is it possible to load the OS in flash memory if yes, what amount of memory space will OS require.

my application can be easily run and completed in or around 150 MB so can you please guide me what will be total memory i will require for my project ???

thank you in advance 

With Regards 

Aditya

Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

632 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

may be useful to check SCM board configuration as it provides small images
(for example SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 spi-nor image)
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

632 Views
adityaprajapati
Contributor I

Respected sir,

Thank you so much for you kind concern

But I just wanted to ask that what is the memory that will be occupied by the BSP Linux if I use BSP without GUI??

How much total memory would be required for the whole system to run efficiently

With Regards

Aditya

0 Kudos
Reply