Dear Sir or Madam,
Hello.
Refer to "18.3 CCM Clock Tree" in IMX6DQRM_Rev.2.
There is below description.
"The default frequency values (in MHz) for the PLLs and PFDs is the maximum allowed frequency. The PLL and PFD control registers should not be programmed to exceed these values."
Next, refer to "Table 18-4. System Clock Frequency Values".
ARM_CLK_ROOT Default Frequency was 792MHz.
freescale has i.MX6DQ product for automotive with 1 GHz grade.
What description is right?
Please give me the correct CCM tree.
(If the RM was typo, please fix these description)
Best Regards,
Keita
已解决! 转到解答。
Hi Keita
correct is :
"Table 18-4. System Clock Frequency Values".
ARM_CLK_ROOT Default Frequency was 792MHz.
RM has not typo, probably not clear wording, since there is one
document Reference Manual for all I.MX6DQ speed grades.
That is RM is document describing silicon, while speed grades
are selected silicon samples during PVTC testing on factory.
So "18.3 CCM Clock Tree" in IMX6DQRM_Rev.2 description:
"The default frequency values (in MHz) for the PLLs and PFDs is the maximum allowed frequency.
applies to all speed grades - value "792MHz" defined by lowest speed grade:
IMX6DQIEC Industrial max.800MHz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
correct is :
"Table 18-4. System Clock Frequency Values".
ARM_CLK_ROOT Default Frequency was 792MHz.
RM has not typo, probably not clear wording, since there is one
document Reference Manual for all I.MX6DQ speed grades.
That is RM is document describing silicon, while speed grades
are selected silicon samples during PVTC testing on factory.
So "18.3 CCM Clock Tree" in IMX6DQRM_Rev.2 description:
"The default frequency values (in MHz) for the PLLs and PFDs is the maximum allowed frequency.
applies to all speed grades - value "792MHz" defined by lowest speed grade:
IMX6DQIEC Industrial max.800MHz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Hello.
Thank you for your prompt reply!
I understood for ARM clock.
I checked another PLLs value and found typo.
PLL4 and PLL5 looked 650MHz from 10.3.2.3 PLLs in MCIMX6DQRM(Rev.2).
But, there were description of PLL4 and PLL5 = 630MHz in "Figure 18-2. Clock Tree".
Is this typo?
And, is there another typo in Figure 18-2?
Best Regards,
Keita