Hi,
We are currently working with an official nxp bsp (rel_imx_4.1.15_2.1.0_ga) on our custom imx6ull
board. We are trying to move to mainstream kernel. For now the work is done on 4.19.X release.
I am able to make work my audio codec, wifi, bluetooth, etc.. correctly. I have one last issue... The power
off feature.
By just running poweroff command in the shell on my board, the log seems good :
# poweroff
imx2-wdt 20bc000.wdog: Device shutdown: Expect reboot!
reboot: System halted
But the led are always on and I am not able to boot anymore.
The custom board uses a pfuze3000 pmic. Eveything is working perfectly on the officiel nxp release
of course but not on the mainstream kernel. It is like the pmic is not doing his work correctly.
There are thousands of patch on nxp bsp. Any clue about a patch to make work the poweroff
feature on the mainstream kernel with a pmic on imx6 board?
I tried to align the pfuze100_regulator sources, all the device tree sources, and it is always
not working properly
Thanks,
Arthur.
解決済! 解決策の投稿を見る。
Hi,
snvs_poweroff is disabled by default
I think because there are several poweroff drivers (at least there is still gpio-poweroff), but only one can be used. Therefore, you just need to enable it in your DTS
&snvs_poweroff { status = "okay"; };
Alexander
Hi,
I think this is implemented in the Linux kernel since version 4.20
Alexander
Thank you for your answer. I tried to add this to my kernel and this is not working.
I have the log a the end "Unable to poweroff system"
Probably because the pmic power off sequence is not running correctly after this code :
imx6_set_lpm(STOP_POWER_OFF);imx6q_suspend_finish(0);
I tried to test directly the 4.20 kernel on my board. Same failure on the power off.
I was able to find this very useful commit in my kernel log in on the nxp bsp:
https://lkml.org/lkml/2018/9/12/105
In fact my board uses PMIC_ON_REQ and not the PMIC_STBY_REQ signal. So I must no used
the fsl,pmic-stby-poweroff system in the device tree but the syscon-poweroff instead.
On a working kernel the code to handle the poweroff is in drivers/power/reset/syscon-poweroff. The probe
and the syscon_poweroff function seems to be not trigger on mainstream kernel. There is probably
something missing in the imx6ull.dtsi or imx6ul.dtsi.
Thank you to pointing me the good direction :smileyhappy:
Hi,
snvs_poweroff is disabled by default
I think because there are several poweroff drivers (at least there is still gpio-poweroff), but only one can be used. Therefore, you just need to enable it in your DTS
&snvs_poweroff { status = "okay"; };
Alexander
Yes that's it... There is no "disabled" in the original device tree in nxp official bsp.
Juste a "disabled" line to remove in the imx6ul.dtsi or a status okay to add to my
custom board device tree to trigger the driver and now everything is working like a charm...
Hello Arthur,
The mainstream kernel is not supported so we do not have much information that may be of help to get it running on the i.MX6ULL.
There are some threads on the communities of a similar behavior although in NXP’s BSPs and not in mainstream kernel. Maybe they may provide some hints:
https://community.nxp.com/thread/359508
https://community.nxp.com/thread/385097
There is a new 4.14.78_1.0.0 BSP Release, perhaps you could look at how the PMIC is handled there although you would need to look among the number of patches included.
Another alternative would be contacting NXP Professional Services to ask for help implementing this feature.
My apologies for the inconvenience.
Regards,