Maaxboard sn65dsi83 mipi dsi to lvds Converter Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maaxboard sn65dsi83 mipi dsi to lvds Converter Issue

1,298 Views
ahmetkoc
Contributor III

Hello all,

     I have a 10.25 "1280 * 480 resolution screen. I want to run this screen with maaxboard, but I was not successful.

I connect the screen with sn65dsi83 which is a mipi dsi to lvds converter, I tried the kernel configurations with dcss and lcdif, I could only print the test pattern in the test mode on  screen when i use sn65dsi83 with maaxboard via i2c communication. I could not get any image in the normal mode .

 

I'm trying to stand up with maaxboard-dcss-mipi.dtb;

     When I use this dtb file, the system gets up properly, I see that the sn65dsi83 installation has been done properly, but I can't get any image. You can see the output of dmesg in the "maaxboard-dcss-mipi-dmesg.txt" file.

 

I'm trying to stand up with maaxboard-lcdif-mipi.dts;

     When I use this dtb file, the system loading is interrupted and the root file cannot jump to the system.

You can see the output of dmesg in the "maaxboard-lcdif-mipi-dmesg.txt" file.

 

Device                : Maaxboard imx8mq / https://www.avnet.com/wps/portal/us/products/new-product-introductions/npi/avnet-maaxboard/

Yocto version      : https://github.com/Avnet/meta-maaxboard/tree/zeus

sn65dsi83 driver : https://github.com/digi-embedded/linux/tree/v5.4/dey-3.0%2Fmaint/drivers/gpu/drm/bridge/sn65dsi83

Screen                : 10.25 '' 1280x480

 

I have a hard time understanding where I am having problems. I would be glad if you could help. Thanks

 

Files

1) maaxboard-dcss-mipi-dmesg.txt

2) maaxboard-lcdif-mipi-dmesg.txt

3) maaxboard-dcss-mipi.dts

4) maaxboard-lcdif-mipi.dts

5) maaxboard-dsi-common.dtsi

TestPattern.jpeg

 
Labels (2)
0 Kudos
1 Reply

1,129 Views
Tooght
Contributor III

as far as I know, yocto zeus version does not support maaxboard (only maaxboard nano are supported). I check their repository and their note is still there. Firstly you should make sure that is not a problem.

0 Kudos