MX8MQ - Trouble getting HB-050WISB0GA0-B HDMI display working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8MQ - Trouble getting HB-050WISB0GA0-B HDMI display working

475 Views
bshortridge
Contributor I

I'm having issues with connecting the DART-MX8M board running Yocto to a HDMI screen. It works fine if I connect it to a HDMI monitor, but when I try to connect it to the display we want to use (HB-050WISB0GA0-B), it doesn't work, I see the following reported over the USB Debug cable:

[ 5149.145476] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 5149.151498] [drm] Cannot find any crtc or sizes
[ 5149.177868] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 5149.210668] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0              
[ 5149.216635] [drm] Cannot find any crtc or sizes                             
[ 5149.221192] [drm] HDMI Cable Plug In

To set the HDMI output (works with HDMI monitor, just not this display) I used:
# cd /boot
# ln -fs imx8mq-var-dart-dt8mcustomboard-wifi-hdmi.dtb imx8mq-var-dart-dt8mcustomboard.dtb

The display itself works fine if I connect it to my laptop.

I saw this thread: https://community.nxp.com/t5/i-MX-Processors/HDMI-DRM-custom-resolution-and-clock-frequency/m-p/1029... which claims that I need to input timing parameters into the spreadsheet and then modify the kernel, but I've got no idea what many of the parameters are, and I can't find them on the datasheet:

Pixel encoding: RGB
Color depth: 8
Reference clock frequency [MHz]: ?
Expected pixel clock frequency [MHz]: 25.00?
Generated clock tolerance [%]: ?

Pll input divider: ?
Pll feedback divider: ?
Pixel clock divider: ?
Character clock divider: ?

I can get an edid file by:
cat /sys/devices/platform/soc@0/soc@0:bus@32c00000/32e00000.display-controller/drm/card0/card0-HDMI-A-1/edid > ~/edid.bin

If I then parse that file with parse-edid < edid.bin, it reports this:

Checksum Correct
 
Section "Monitor"
        Identifier "HDMI Panel W"
        ModelName "HDMI Panel W"
        VendorName "DWI"
        # Monitor Manufactured week 9 of 2020
        # EDID version 1.4
        # Digital Display
        DisplaySize 890 500
        Gamma 2.20
        Option "DPMS" "false"
        Horizsync 14-70
        VertRefresh 50-70
        # Maximum pixel clock is 50MHz
 
        #Extension block found. Parsing...
        Modeline        "Mode 2" 25.200 640 656 752 800 480 490 492 525 -hsync -vsync
        Modeline        "Mode 0" +hsync -vsync 
        Modeline        "Mode 1" +hsync -vsync 
        Option "PreferredMode" "Mode 2"
EndSection
 
Please help.
 
Thanks
0 Kudos
0 Replies