MX8_DSI_OLED1 won't show anything

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX8_DSI_OLED1 won't show anything

1,204件の閲覧回数
anton_platonov
Contributor I
Hi, I bought NXP iMX8M-mini evaluation board with MX8_DSI_OLED1 and the display shows nothing when I connect it to the board. If I use IMX-MIPI-HDMI converter and connect it to external HDMI display, it works fine.
I tested Test points: TP4, TP5, TP6 (all good ground):
  • TP7 => 4.87v
  • TP8 => 3.31v
  • TP9 => 1.81v
  • TP10 => 0v
  • TP11 => 0v
  • TP12 => 0v
  • OLED_EN => 0v
 
It looks like the display is not being enabled, so the EL_VDD, EL_VSS, and VSP voltages are not being output from the TPS65651 chip.
How do I troubleshoot MX8_DSI_OLED1 display?
タグ(2)
0 件の賞賛
3 返答(返信)

824件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,


Please note that for the MIPI panel to be tested with our demo image you'll need to select the correct device tree:

Android

dtbo-imx8mm-mipi-panel.img

 

Linux

Image-fsl-imx8mm-evk-rm67191.dtb                 * LPDDR4 EVK

Image-fsl-imx8mm-ddr4-evk-rm67191.dtb         * DDR4 EVK

 

Hope this helps,

Regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

824件の閲覧回数
anton_platonov
Contributor I

Aldo Gutierrez wrote:


Please note that for the MIPI panel to be tested with our demo image you'll need to select the correct device tree:

Android

dtbo-imx8mm-mipi-panel.img

 

Thank you for this suggestion, but how do I do that?

I am trying to run default Android OS that was on microSD with the kit and I tried the following commands (found them in OLED1 manual):

U-Boot > setenv fdt_file dtbo-imx8mm-mipi-panel.img

U-Boot > run bootcmd

 

But it won't change anything.

0 件の賞賛

824件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

You'll need to reflash one of our android releases, you may find them here:

https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tools:IMX-SW

 

Please follow the guide Android_Quick_Start_Guide.pdf, I'll attach here the android_p9.0.0_2.0.0-ga one here, you'll find an step by step on how to flash the demo image in section 3.3 Flashing board images.

 

Hope this helps,

Regards,

Aldo.

0 件の賞賛