OTA recovery process failure for iMX8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA recovery process failure for iMX8mm

1,317 Views
s_inamura
Contributor I

Hello ,

NXP community.

I'm trying to confirm OTA update by recovery process for iMX8mm  with Android 9 OS.

however the recovery process is not complete because of the error after reboot for recovery console.

LCD panel with this board displays comments as "/cache/recovery/block.map failed" when it occurred

(please see attached jpeg file).

I took adb logcat log and usb serial port log which I have attached  to this site.

I don't know why  iMX8mm stopped recovery console by the error and how to solve this problem.

regards,

Seiji Inamura 

0 Kudos
Reply
2 Replies

1,181 Views
s_inamura
Contributor I

Additional information.

evaluation board : DART-MX8M-MINI

firmware version : p9.0.0_1.0.0

used android build ota Package: android_build/vendor/nxp-opensource/fsl_imx_demo/FSLOta

operations :

I stepped following operations  on Android GUI.

<Settings> --> <System> --> <Advanced> --> <Additional system updates> 

regards,

Seiji Inamura.

0 Kudos
Reply

1,181 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the board that you are using is from a third party and they have their own Android BSP. What I strongly suggest is to go with Variscite and ask directly to them. 

Variscite Support Center - Variscite 

Best regards,

Diego.

0 Kudos
Reply