MX8_DSI_OLED1 won't show anything

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8_DSI_OLED1 won't show anything

1,194 Views
anton_platonov
Contributor I
Hi, I bought NXP iMX8M-mini evaluation board with MX8_DSI_OLED1 and the display shows nothing when I connect it to the board. If I use IMX-MIPI-HDMI converter and connect it to external HDMI display, it works fine.
I tested Test points: TP4, TP5, TP6 (all good ground):
  • TP7 => 4.87v
  • TP8 => 3.31v
  • TP9 => 1.81v
  • TP10 => 0v
  • TP11 => 0v
  • TP12 => 0v
  • OLED_EN => 0v
 
It looks like the display is not being enabled, so the EL_VDD, EL_VSS, and VSP voltages are not being output from the TPS65651 chip.
How do I troubleshoot MX8_DSI_OLED1 display?
0 Kudos
3 Replies

814 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,


Please note that for the MIPI panel to be tested with our demo image you'll need to select the correct device tree:

Android

dtbo-imx8mm-mipi-panel.img

 

Linux

Image-fsl-imx8mm-evk-rm67191.dtb                 * LPDDR4 EVK

Image-fsl-imx8mm-ddr4-evk-rm67191.dtb         * DDR4 EVK

 

Hope this helps,

Regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

814 Views
anton_platonov
Contributor I

Aldo Gutierrez wrote:


Please note that for the MIPI panel to be tested with our demo image you'll need to select the correct device tree:

Android

dtbo-imx8mm-mipi-panel.img

 

Thank you for this suggestion, but how do I do that?

I am trying to run default Android OS that was on microSD with the kit and I tried the following commands (found them in OLED1 manual):

U-Boot > setenv fdt_file dtbo-imx8mm-mipi-panel.img

U-Boot > run bootcmd

 

But it won't change anything.

0 Kudos

814 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

You'll need to reflash one of our android releases, you may find them here:

https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tools:IMX-SW

 

Please follow the guide Android_Quick_Start_Guide.pdf, I'll attach here the android_p9.0.0_2.0.0-ga one here, you'll find an step by step on how to flash the demo image in section 3.3 Flashing board images.

 

Hope this helps,

Regards,

Aldo.

0 Kudos