I have been working with the iMX8 QuadXPlus MEK with two of the NXP MX8 DSI OLED1 screens attached, and I can't get the touch to work. I followed the instructions in the i.MX Yocto Project User's Guide, and I am able to build an image where the display is working, but touch is not. I am working with 4.14.78_1.0.0_ga and using fsl-imx8qxp-mek-dsi-rm67191 for the device tree. In trying to figure the issue out I found a similar question:
https://community.nxp.com/message/1035302
but the answer there did not fix the issue. I have the kernel configuration options the same as that post, but the there is no synaptics section of the dts. From what I can tell, this touch screen uses I2C, and none of the I2C devices in the device tree seem to be touch screen related.
Is there a device tree for this board which does support the MX8 DSI OLED1 with touch?
If not, what all do I need to do to add touch support to fsl-imx8qxp-mek-dsi-rm67191?
Hi Emmett,
I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE. Just as reference, you could take a look to the following Community threads:
https://community.nxp.com/thread/497477
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------