As I mentioned in some threads, we are trying on MX6Q+LPDDR2 combined design. but make no sense why boot failure in mfg bootimage.
We use Mx6DQSDL LPDDR2 Script Aid V0.04.xlsx to generate flashheader DCD part (attached file 6q_lpddr2_32.inc). The Samsung eMCP
DS attched,too.
Our DDR config:
Single Channel 32bit
2CS, each cs is 128Mx32 (totally 1GB)
With default DSE 40ohm (SI configuration in Mx6DQSDL LPDDR2 Script Aid V0.04.xlsx ), 400MHz DDR stress test failure, but it's okay change them
to 34ohm. But with this stress pass DCD, my uboot_mfg can't boot properly (no output in default console).
Please help us!
Original Attachment has been moved to: 6q_lpddr2_32.inc.zip
Original Attachment has been moved to: mx6q_tdh_lpddr2_400_v004.inc.zip
已解决! 转到解答。
With help of FSL FAE, now it can boot up properly. Root cause :
We can't gate/ungate 528 pfd2 (FSL's explanation).
int arch_cpu_init(void){
/* Due to hardware limitation, on MX6Q we need to gate/ungate all PFDs | ||
* to make sure PFD is working right, otherwise, PFDs may | ||
* not output clock after reset, MX6DL and MX6SL have added 396M pfd | ||
* workaround in ROM code, as bus clock need it | ||
*/ | ||
writel(BM_ANADIG_PFD_480_PFD3_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD2_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_480_SET); | ||
writel(BM_ANADIG_PFD_528_PFD3_CLKGATE | |
#if defined(CONFIG_MX6Q) && !defined(CONFIG_LPDDR2)
BM_ANADIG_PFD_528_PFD2_CLKGATE | |
#endif
BM_ANADIG_PFD_528_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_528_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_528_SET); |
writel(BM_ANADIG_PFD_480_PFD3_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD2_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_480_CLR); | ||
writel(BM_ANADIG_PFD_528_PFD3_CLKGATE | |
#if defined(CONFIG_MX6Q) && !defined(CONFIG_LPDDR2)
BM_ANADIG_PFD_528_PFD2_CLKGATE | |
#endif
BM_ANADIG_PFD_528_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_528_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_528_CLR); |
...
}
Hi Raymond
suggest to build just Uboot (not MFG) and try to boot it,
flash_header.S should be modified with new DCD settings.
Regarding MFG Tool, its firmware (initramfs.cpio.gz.uboot)
should be rebuilt with new DCD, please check
i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf
sect.3.9 "Building Manufacturing Firmware".
Actually you can download just modified Uboot with MFG Tool,
modifiy ucl2.xml (also one can create new Profile, check with MFG2 Tool documentation).
u-boot-mx6q-sabresd_nopad.bin is Uboot image without offset (0x400).
Note, for USB loading one needs the same images, but without offset.
Changed "SabreSD-SD" profile:
<LIST name="SabreSD-SD" desc="USB SDP">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot-mx6q-sabresd_nopad.bin" >Loading image</CMD>
<CMD state="BootStrap" type="jump" > Jumping to image. </CMD>
<CMD state="Updater" type="push" body="$ echo Load Complete!">Done</CMD>
</LIST>
On Windows platform for creating Uboot image without offset, "dd"
utility may be used (http://www.chrysocome.net/dd):
dd.exe if=u-boot-mx6q-sabresd.bin of=u-boot-mx6q-sabresd_nopad.bin bs=1024 skip=1
Best regards
chip
Dear Chip
I tried to enable 1 gpio to light on a LED, seems failure . I think this means cpu did not
run there.
BTW, I found a DCD data to enable DDR 400MHz:
setmem /32 0x020c4018 = 0x00060324
Is it right?
BR
RaymondWang
I Add the gpio code in uboot since DCD can't access gpio module directly.
I test my uboot with sabresd DDR3 config, it does work.
Only one CCM register is set in DCD,
setmem /32 0x020c4018 = 0x00060324
I don't think it relevant to GPIO required clocks.
I doubt DCD ccm register setting not enough to let LPDDR2 working at 400MHz. Our board
can't pass 528MHz DDR stress test.
Hi Raymond
I would suggest to use Linux or even SDK
at bring-up phase. They are simpler, better documented,
easier for debugging.
Best regards
chip
I rebuild sdk_unit_test_ALL.bin with replacing smart_device dcd.c to my LPDDR2.
And add it to mfg tool
<LIST name="DWLD_IN_SDP" desc="Download and execute a binary!">
<CMD state="BootStrap" type="find" body="Recovery" timeout="180"/>
<CMD state="BootStrap" type="boot" body="Recovery" file="sdk_unit_test_ALL.bin">Loading
SDK image</CMD>
<CMD state="BootStrap" type="jump">Jumping to SDK image.</CMD>
</LIST>
The mfgtool hangs with display state in "Loading SDK image" about 75% over 5mins.
I enclosed my new dcd.c.
Hi Raymond
I would suggest to start
with attached examples. One uses iRAM,
second DDR3 - you can modify it for LPDDR2.
Optionally you can build SDK examples and run in iRAM using link below
iRAM (OCRAM) i.MX6 SDK Application
Best regards
chip
I don't think so since it's generated by FSL designing aiding tool. Meanwhile FSL local FAE also tried his DCD.
FSL local FAE told me today that he will take our board to Freescale ShangHai RD center to find out root cause.
With help of FSL FAE, now it can boot up properly. Root cause :
We can't gate/ungate 528 pfd2 (FSL's explanation).
int arch_cpu_init(void){
/* Due to hardware limitation, on MX6Q we need to gate/ungate all PFDs | ||
* to make sure PFD is working right, otherwise, PFDs may | ||
* not output clock after reset, MX6DL and MX6SL have added 396M pfd | ||
* workaround in ROM code, as bus clock need it | ||
*/ | ||
writel(BM_ANADIG_PFD_480_PFD3_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD2_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_480_SET); | ||
writel(BM_ANADIG_PFD_528_PFD3_CLKGATE | |
#if defined(CONFIG_MX6Q) && !defined(CONFIG_LPDDR2)
BM_ANADIG_PFD_528_PFD2_CLKGATE | |
#endif
BM_ANADIG_PFD_528_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_528_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_528_SET); |
writel(BM_ANADIG_PFD_480_PFD3_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD2_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_480_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_480_CLR); | ||
writel(BM_ANADIG_PFD_528_PFD3_CLKGATE | |
#if defined(CONFIG_MX6Q) && !defined(CONFIG_LPDDR2)
BM_ANADIG_PFD_528_PFD2_CLKGATE | |
#endif
BM_ANADIG_PFD_528_PFD1_CLKGATE | | ||
BM_ANADIG_PFD_528_PFD0_CLKGATE, | ||
ANATOP_BASE_ADDR + HW_ANADIG_PFD_528_CLR); |
...
}
You can clone the bootloader tree https://github.com/xhteam/bootable-bootloader-uboot-imx/