Hi NXP,
I would like to download the MQX 4.1 included i.mx6sx bsp for SABRE-SDB Board.
How to get MQX 4.1 included i.mx6sx bsp?
Thanks,
Jackey
Hi Jackey
available versions are described on
MQX™ v5 Software Solutions|NXP
MQX 4.1 is not available, probably due to licensing.
Best regards
igor
Hi Igor,
Thanks for your supprot.
Before the license agreement, I want to test MQX RTOS included i.mx6sx BSP on SABRE-SD Board.
Can i get the MQX RTOS included i.mx6sx BSP(ssi, sai, esai, adc, spi, gpio, i2c, uart, wdog, ect) ?
My goal of BSP is using audio system.
Thanks,
Jackey
Beware MXQ 4.1 on imx6sx has no builtin support for audio (ie no ssi, sai or esai). You need to write your own drivers.
Hi Jas Math,
Thanks for your support.
Ok, I understood your commet.
I would like to download MQX 4.1 included imx6sx for testing as below link:
https://community.nxp.com/docs/DOC-104422
Can you help where I can get MQX 4.1 included imx6sx?
Thanks,
Jackey
Its no longer available from the NXP website because the old download link is no longer active. BTW you can use FreeRTOS to implement the same task.
Hi Jackey
suggest to mail to vendor of this product info@embedded-access.com
for availability older versions.
Best regards
igor
Hi Igor,
I would like to test as below:
https://community.nxp.com/docs/DOC-104422
FIRMWARE MQX
Download the last MQX source code from Freescale's website at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX#. I have used the 4.1.0 version in the tests. Do not forget to download the Linux version (*.gz).
Create a directory and decompress the source code:
$ cd $IMX6SOLOX $ mkdir -p mqx && cd mqx $ tar xfv ~/Downloads/Freescale\ MQX\ RTOS\ 4.1.0\ for\ i.MX\ 6SoloX\ Linux\ Base.gz $ ls build config doc mcc mqx tools
Thanks,
Jackey
MQX was replaced with FreeRTOS (FreeRTOS_MX6SX_1.0.1_LINUX) so that is the recommended option.