MPF0100F0ANES pmic not replying on i2c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPF0100F0ANES pmic not replying on i2c

808 次查看
angelo_d
Senior Contributor I

Hi all,

did a small linux tool for i2c, and (unless i have no bugs, that shouldn't be since all other devices in the bus are detected correctly) looks like the PMIC is not replying. It should reply at a 0x08 address, or near it.

We should need to control some voltage so if possible i would understand what is wrong here.

Reagrds

Angelo

标签 (1)
0 项奖励
回复
3 回复数

698 次查看
angelo_d
Senior Contributor I

Hi igor,

thanks,

i have several devices in the bus, working properly. Only PMIC is not responding, so i would exclude any imx6q pinmux issue.

VIN is 3V3, VDDIO is 3v3.

Is it possible some of this chip are programmed on OTP without i2c enabled ?

Regards

Angelo

0 项奖励
回复

698 次查看
igorpadykov
NXP Employee
NXP Employee

Hi angelo

i2c can not be disabled. Is this one chip or several,

had you checked signals with oscilloscope?

Best regards

igor

0 项奖励
回复

698 次查看
igorpadykov
NXP Employee
NXP Employee

Hi angelo

one can check i2c iomux settings and if SION bit is set in

IOMUXC_SW_MUX_CTL register. As for PMIC, to communicate with I2C,

VIN must be valid and VDDIO, to which SDA and SCL are pulled up, must be

powered by a 1.7 to 3.6 V supply.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复