Hi
I am going to use MMPF0100F0ANES in our design which has the Package Outline Drawing Number 98ASA00589D.
http://cache.freescale.com/files/shared/doc/package_info/98ASA00589D.pdf
Do you have any PCB Guideline document recommend for this package 98ASA00589D as the following for package 98ASA00379D (page 4,5)?
Can 98ASA00589D package use the same PCB with 98ASA00379D ?
http://cache.freescale.com/files/shared/doc/package_info/98ASA00379D.pdf
I've referenced AN1902 (Assembly Guidelines for QFN (Quad Flat No-lead) and DFN (Dual Flat No-lead) Packages) but it is better if you have a guideline PCB for 98ASA00589D?
Best Regards,
Nhat
Hi Thanh
suggest to look at sect.7.2 PF0100 Layout Guidelines MMPF0100
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
Thank you very much for your reply.
I have referenced section 7.2 Layout Guidelines as your suggest.
I am sorry that my question is not clearly.
I want to find the Land Pattern Design guideline for part MMPF0100F0ANES, which is not mention in section 7.2
In the datasheet of MMPF0100Z, section 8, suffix ES part (WF-Type package ) can refer to two package documents 98ASA00379D, 98ASA00589D.
Do you have the Land Pattern Design guideline for 98ASA00589D?
Can 98ASA00589D package use the same Land Pattern Design with 98ASA00379D?
Best Regards,
Nhat
Hi Thanh
I think one can look at i.MX6_SABRE_SDP_DESIGNFILES : Design files, including hardware
schematics, Gerbers, and OrCAD files,
it uses MMPF0100
Best regards
igor
Hi,
I would like to follow up with this PCB land pattern for Package Outline Drawing Number 98ASA00589D.
Would the land pattern used below work for the 98ASA00589D package?
http://cache.freescale.com/files/shared/doc/package_info/98ASA00379D.pdf
Thanks,
Gus
Hi Thanh
not, since these packages are different
http://cache.freescale.com/files/shared/doc/package_info/98ASA00379D.pdf
http://cache.freescale.com/files/shared/doc/package_info/98ASA00589D.pdf
Best regards
igor