I have a custom device based on the MX6Q processor that works fine with Kernel version 3.14.52. I am trying to upgrade to Kernel version 4.1.15 but the boot process will not complete due to MMC issues. Don't know if I am missing a new device tree parameter or a patch file?
The boot process stops at this line: Waiting for root device /dev/mmcblk0p2...
Here is the section of the boot cycle that is MMC specific:
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
The 3.14.52 Kernel has additional MMC messages that I do not see for the newer version. These are here:
mmc0: new high speed SDHC card at address 1234
mmcblk0: mmc0:1234 SA08G 7.21 GiB
mmcblk0: p1 p2
Any insight would be appreciated!
解決済! 解決策の投稿を見る。
Hi Paul,
Please make sure you pass the GPIO_ACTIVE_LOW polarity in your cd-gpios line, like this:
cd-gpios = <&gpio2 0 GPIO_ACTIVE_LOW>;
Hello,
Have You tried NXP L4.1.15 demo ?
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Paul,
Please make sure you pass the GPIO_ACTIVE_LOW polarity in your cd-gpios line, like this:
cd-gpios = <&gpio2 0 GPIO_ACTIVE_LOW>;
Thanks for the response. Here is what I have in my device tree. I have the CD pin defined as active high.
#define GP_SD1_CS <&gpio1 1 GPIO_ACTIVE_HIGH>
&usdhc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc1>;
bus-width = <4>;
cd-gpios = GP_SD1_CS;
keep-power-in-suspend;
status = "okay";
};
&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2>;
bus-width = <4>;
keep-power-in-suspend;
status = "okay";
};
I changed the CD to GPIO_ACTIVE_LOW and the build worked! Thanks.
Why did GPIO_ACTIVE_HIGH work for version 3.14.52 and now it doesn't work for the newer version??
I did notice the following log message that does not appear in the 3.14.52 boot:
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
The explanation for using active low for the card detect gpio is provided in this commit:
commit 50eda1546d87542d21eb5a69caf4f046a4bb416e
Author: Dong Aisheng <aisheng.dong@freescale.com>
Date: Wed Jul 22 20:53:02 2015 +0800
dts: imx6: fix sd card gpio polarity specified in device tree
commit 89c1a8cf63f8c69dfddb6e377c04df8b25ab1c88 upstream.
cd-gpios polarity should be changed to GPIO_ACTIVE_LOW and wp-gpios
should be changed to GPIO_ACTIVE_HIGH.
Otherwise, the SD may not work properly due to wrong polarity inversion
specified in DT after switch to common parsing function mmc_of_parse().
Signed-off-by: Dong Aisheng <aisheng.dong@freescale.com>
Acked-by: Shawn Guo <shawnguo@kernel.org>
Signed-off-by: Ulf Hansson <ulf.hansson@linaro.org>
Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>=