We are currently using a iMX6 Sabre board for development, and are looking to see if the Linux distros supported via. Yocto include MIPI support. We have a custom product we are looking to integrate with over MIPI, and are trying to estimate the effort to get data into Linux. Is this generic, or does a specific driver/layer need to be created to support this?
Thanks,
Rich
Richard,
If only regrading to driver level, here's related kernel source code on MX6 MIPI support, incluing display and camera:
MIPI camera:
include/linux/mipi_csi2.h
drivers/mxc/mipi/mxc_mipi_csi2.c
drivers/mxc/mipi/mxc_mipi_csi2.h
drivers/media/platform/mxc/capture/ov5640_mipi.c
MIPI display:
drivers/video/mxc/mipi_dsi.h
drivers/video/mxc/mipi_dsi.c
Richard,
Had your question got answered? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
The right question would be if kernel 3.10.17-1.0.0 is going to support any MIPI camera.
As I know the kernel already published (3.10.17-1.0.0) does support one MIPI camera. As I understand, the application does not recognize if camera is mipi or csi or usb, because this differentiation is handled by kernel.
Richard
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing