Hello,
I'm currently trying to connect a MA130 Sony Camera (I suspect it's a imx135 camera module) to an iMX6Q via MIPI.
I based my driver on the ov5640_mipi. The MIPI side seems to works fine but the IPU/CSI don't.
I would like to have some thoughts on my configuration. The camera outputs 1080p30 video, YUV422, 81MHz pixel clock, MIPI on 2 lanes. I'm connected to the Virtual channel 0 (I think, I don't have the confirmation) on IPU1 CSI0
This is how I calculated the MIPI clock (for MIPI_CSI2_PHY_TST_CTRL1), using chapter 3.4 of this document:
- 1920*1080*30*1cycle/pixel*blanking = 81MHz -> blanking = 1.24 (coherent)
- MIPI data Rate: 81MHz*16bits = 1296Mb/s
- MIPI Clock: 1296/2/2 = 324MHz (like the datasheet)
- MIPI_CSI2_PHY_TST_CTRL1= 324*2=648MHz register = 0x10
When I start the driver, I got these registers:
MIPI_CSI_PHY_STATE 0x200
MIPI_CSI_ERR1 0x0
MIPI_CSI_ERR2 0x0
Everything seems fine for the MIPI side.
About the IPU
IPU ID = 0, CSI ID = 0
IPU_CONF = 0x10000661
-> CSI_SEL to CSI0, CSI0_DATA_SOURCE, CSI0 enabled
CSI_SENS_CONF = 0x00008A00 (// I tested 0x00008A20 with no success : Gated vs bt656)
CSI_SENS_FRM_SIZE = 0x0437077F //1920*1080
CSI_ACT_FRM_SIZE = 0x0437077F //1920*1080
CSI_OUT_FRM_CTRL = 0x00000000
CSI_TST_CTRL = 0x00000000
CSI_CCIR_CODE_1 = 0x00040030
CSI_CCIR_CODE_2 = 0x00000000
CSI_CCIR_CODE_3 = 0x00FF0000
I configured the pixelformat like the OV5640 : V4L2_PIX_FMT_UYVY,
iftype=V4L2_IF_TYPE_BT656
mode=V4L2_IF_TYPE_BT656_MODE_NOBT_8BIT
When I start a gstreamer pipeline I still get the same error:
v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
Did you see any misconfiguration?
Best regards,
Pierre-Olivier
解決済! 解決策の投稿を見る。
Hi Pierre-Olivier
for two lanes correct MIPI_CSI_PHY_STATE is 0x330,
the value is jump between 0x330 and 0x300). May be useful to check
Debug steps for customer MIPI sensor.docx
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pierre-Olivier
for two lanes correct MIPI_CSI_PHY_STATE is 0x330,
the value is jump between 0x330 and 0x300). May be useful to check
Debug steps for customer MIPI sensor.docx
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for the tip, I have found a thread about that : https://community.nxp.com/thread/356082
Now the register MIPI_CSI_PHY_STATE=0x300 or 0x330, but the ERR1 register is 0x3 now. Did I misconfigured the clock?
Edit :The TEST_CTRL1 register was not correctly set. I have an image now, but it flickers and it's mainly yellow. Any Thoughts?
Edit2: Misconfiguration in ipu_capture, I have the imge, but there is a strang behavior: at first start everything is ok, then if a restart the pipeline, I got IPU_INT_STAT_10=0x00000001 and the image is rolling.
I suspect the IPU_CSI_CLK_MODE_NONGATED_CLK, any thoughts?
Best regards
Pierre-Olivier