MFGTOOL V2 support on IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFGTOOL V2 support on IMX6

994 Views
tomsaluzzo
Contributor III

Using the MCIMX6Q7CZK08AD.

Is there any way to verify if the latest MFGTOOL V2 will work with this pop processor? We keep running into issues where it’s not able to write to the DDR2.

Labels (1)
0 Kudos
1 Reply

665 Views
b36401
NXP Employee
NXP Employee

Actually MfgTool2 is official Manufacturing Toolkit for i.MX6Q. Here are download links for Linux 3.10.17 and 4.1.15 respectively:
http://nxp.com/webapp/Download?colCode=IMX_6_MFG_L3.10.17_1.0.0_TOOL
http://nxp.com/webapp/Download?colCode=IMX6_L4.1.15_1.0.0_MFG_TOOL

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos