MFG-Tool download error with imx6solo sabresd board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFG-Tool download error with imx6solo sabresd board.

762件の閲覧回数
hanseunglee
Contributor III


Hi, every body.

------------------------------------------

i.mx6solo sabresd board

Kernel. 3.14.52

ubuntu 14.04

-----------------------------------------

 

When I download linux image file with use MFG-TOOLS, I have some error.

mfg-tools version also 3.14.52 .

--------------------------------------------------------------------------------------------------------------------------

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Dec 05 2015 - 02:02:52)

 

 

CPU:   Freescale i.MX6SOLO rev1.2 at 792 MHz

CPU:   Temperature 46 C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

 

 

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

switch to partitions #0, OK

mmc2(part 0) is current device

Net:   FEC [PRIME]

Error: FEC address not set.

 

 

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Kernel image @ 0x12000000 [ 0x000000 - 0x521260 ]

## Loading init Ramdisk from Legacy Image at 12c00000 ...

   Image Name:   fsl-image-mfgtool-initramfs-imx6

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    7508220 Bytes = 7.2 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800d9b2

switch to ldo_bypass mode!

 

 

Starting kernel ...

 

--------------------------------------------------------------------------------------------------------------------------------------------

 

Do not proceed download.

What problem am i have?

How to solve this problem?

Original Attachment has been moved to: MfgTool.log.zip

Original Attachment has been moved to: mfgtools-err.log.zip

ラベル(1)
0 件の賞賛
返信
1 返信

514件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hanseung

sabresd board has i.MX6DL processor, for custom board with i.MX6S processor

it is necessary to run ddr test

https://community.freescale.com/docs/DOC-105652

find new calibration coefficients and rebuild mfg tools, please refer

to attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信