MCIMX6Q6AVT10AC DDR3 only 1 512MB-bank stress test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6Q6AVT10AC DDR3 only 1 512MB-bank stress test

764件の閲覧回数
cgonzalez
Contributor I

Hi all,

We are currently developing a tablet-based system in which we have 4x 512MB DDR3 memory banks.

We have had an issue regarding DDR3 layout and we cannot use all of these 4 banks due to un-matched signal lenghts, but we need to test other features of the system.

How can configure iMX6 to use only 1 bank?

Can we perform a DDR3 stress test only taking 1 of these banks?

Can we anyway discard 3 banks of DDR3 to copy our OS only into 1 bank?

Thank you very much !

ラベル(1)
0 件の賞賛
返信
1 返信

564件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Carlos

seems it is possible with selection 16 bit bus width (this will select first ddr

connected to lower 16 bits of MMDC bus, DSIZ field register MMDCx_MDCTL)

please check presentation FTF-SDS-F0170 on link how use script for ddr tester

DDR Stress Test - Question - why is it slow? 

The same configuration will work for uboot/linux.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信