MCIMX6Q5EYM10AE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q5EYM10AE

328 Views
RamakrishnaC
Contributor II

Hi Team,

What happens if Boot device (e.g. NOR flash) is not programmed with program image for boot mode set to "Internal Boot" and serial downloader interface is also not available? Can IMX6 still be accessed through JTAG interface to run DDR test  and can JTAG interface be used to program the Boot device (NOR flash) through it?

Please help me..

0 Kudos
Reply
5 Replies

293 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

You can base on this post.

 

Best regards.

0 Kudos
Reply

274 Views
RamakrishnaC
Contributor II

Hi,

Thank you.

In my design we are using only NOR flash as booting device and boot mode is set to boot from NOR flash and if NOR flash is empty then will imx6 will stall in boot ROM and allow us to connect to target through JTAG?

Please share the details

Tags (1)
0 Kudos
Reply

269 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

In this case, it will set secondary image persistent bit and perform SW reset. If device is in serial download, it can't support JTAG detection. Since SDP is not enable will go to SW reset.

Best regards.

0 Kudos
Reply

267 Views
RamakrishnaC
Contributor II

Hi,

Thank you.

"If device is in serial download, it can't support JTAG detection" What we do? Is there any alternte please suggest.

 

 

0 Kudos
Reply

262 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Did you disable SDP after flashing? or is it just a hypothetical situation?

Best regards.

0 Kudos
Reply