MCIMX6Q-SDP fals boot rarely.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q-SDP fals boot rarely.

1,150 Views
satoshishimoda
Senior Contributor I

Hi community,

I have some question about i.MX6 SABRE platform.

Rarely, MCIMX6Q-SDP cannot boot correctly with a error (virtual address error) similar to the attached file.

=====

[Board]

MCIMX6Q-SDP

[BSP]

jb4.2.2_1.0.0-ga

[Procedure]

1. Boot Android 4.2 BSP.

2. After boot, execute a command "reboot -p" to power off.

3. After power off, push power button to reboot.

4. Repeat 2, 3 procedure.

=====

[Q]

Do you have a solution to resolve this issue?

Best Regards,

Satoshi Shimoda

Labels (3)
0 Kudos
Reply
4 Replies

1,051 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

Which error have you met when you boot ? And about the android image you built yourself or demo image from freescale?

Have a nice day~~

Best Regards

Dan

0 Kudos
Reply

1,051 Views
satoshishimoda
Senior Contributor I

Hi Dan,

Sorry, I forgot attaching file.

This issue was occurred with freescale pre-built image.

Best Regards,

Satoshi Shimoda

0 Kudos
Reply

1,051 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

The demo image is default boot from eMMC. If you want to boot from SD card, you need to modify somethings. If using the default image without any changes , errors come. So here I recommend you to burn the images to eMMC and boot from it.

You can have a try.

Best Regards

Dan

0 Kudos
Reply

1,051 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

Where have you burned the image to ? SD card or eMMC?

Best Regards

Dan

0 Kudos
Reply