MCIMX6Q-SDP fals boot rarely.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCIMX6Q-SDP fals boot rarely.

1,085 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have some question about i.MX6 SABRE platform.

Rarely, MCIMX6Q-SDP cannot boot correctly with a error (virtual address error) similar to the attached file.

=====

[Board]

MCIMX6Q-SDP

[BSP]

jb4.2.2_1.0.0-ga

[Procedure]

1. Boot Android 4.2 BSP.

2. After boot, execute a command "reboot -p" to power off.

3. After power off, push power button to reboot.

4. Repeat 2, 3 procedure.

=====

[Q]

Do you have a solution to resolve this issue?

Best Regards,

Satoshi Shimoda

标签 (3)
0 项奖励
回复
4 回复数

986 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

Which error have you met when you boot ? And about the android image you built yourself or demo image from freescale?

Have a nice day~~

Best Regards

Dan

0 项奖励
回复

986 次查看
satoshishimoda
Senior Contributor I

Hi Dan,

Sorry, I forgot attaching file.

This issue was occurred with freescale pre-built image.

Best Regards,

Satoshi Shimoda

0 项奖励
回复

986 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

The demo image is default boot from eMMC. If you want to boot from SD card, you need to modify somethings. If using the default image without any changes , errors come. So here I recommend you to burn the images to eMMC and boot from it.

You can have a try.

Best Regards

Dan

0 项奖励
回复

986 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi,

Where have you burned the image to ? SD card or eMMC?

Best Regards

Dan

0 项奖励
回复