Hello,
I am designing with an IMX8QM and see that it is recommended to use both MC33PF8100EPES and MC33PF8100EQES. This is correct?
Would it be recommended to directly connect both PMIC 'RESET_MCU' directly to the IMX8 POR_B?
Thank you!
Hi Brandon
>it is recommended to use both MC33PF8100EPES and MC33PF8100EQES. This is correct?
yes as described in Table 2. Ordering information PF8100_PF8200, 12-channel power management integrated circuit for high performance applications - Da...
>Would it be recommended to directly connect both PMIC 'RESET_MCU' directly to the IMX8 POR_B?
yes, one can look at MCIMX8QM-CPU MEK – Schematics
Best regards
igor