Hello,
I am using the latest release 4.9.98_2.0.0 on iMX 8M Quad EVK.
I want to set the CPU frequency lower than 1.0GHz.
I tried to change the dts file with i.MX_Linux Reference_Manual.pdf, but there are 4 operational points already.
~/imx-yocto-bsp/build-xwayland/tmp/work-shared/imx8mqevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mq-evk.dts
&A53_0 {
operating-points = <
/* kHz uV */
1500000 1000000
1300000 1000000
1000000 900000
800000 900000
>;
dc-supply = <®_gpio_dvfs>;
};
I confirmed that the EVK board is using this dts.
root@imx8mqevk:/proc/device-tree# strings compatible
fsl,imx8mq-evk
fsl,imx8mq
The operating point is displayed as follows.
root@imx8mqevk:/proc/device-tree/cpus/cpu@0# hexdump -C operating-points
00000000 00 16 e3 60 00 0f 42 40 00 13 d6 20 00 0f 42 40 |...`..B@... ..B@|
00000010 00 0f 42 40 00 0d bb a0 00 0c 35 00 00 0d bb a0 |[email protected].....|
0x16e360 -> 1500000(1.5GHz)
0x13d620 -> 1300000(1.3GHz)
0xf4240 -> 1000000(1.0GHz)
0xdbba0 -> 900000(900MHz)
0xc3500 -> 800000(800MHz)
However, only two operating points in the governor are displayed.
root@imx8mqevk:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_frequencies
1000000 1500000
Also, the minimum clock cannot be set lower than 1.0GHz.
Where should I change to add an operating point?
Best regards,
Yoshinari.