Load signed u-boot on secure board through JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Load signed u-boot on secure board through JTAG

694件の閲覧回数
mohamed-ali_fod
Contributor I

Hi,

I want to load signed u-boot using JTAG on imx6 processor. The same below steps work fine after DDR initialization but, the u-boot run and I can get console only on non secure board, but it doesn't run on secure board (SECURE_CONFIG bit enabled). For information I already check that the signed u-boot works fine on another secured board.
 
loadbin ./u-boot-spinor-signed.imx.bin 0x177ff400
SetPC 0x17800000
g
 
Downloading file [./u-boot-spinor-2020.04-r1.imx.bin]...
O.K.
 
VerifyBin ./u-boot-spinor-signed.imx.bin 0x177ff400
Loading binary file ./u-boot-spinor-signed.imx.bin
Reading 689472 bytes data from target memory @ 0x177FF400.
Verify successful.
 
As mentioned above the load works well on secure and non secure board but the loaded u-boot works only on non secure board.
 
Could you please help? Are the 0x17800000 or 0x177FF400 addresses still valid in case of secure board?
 
Best regards,
Mohamed Ali
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

652件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @mohamed-ali_fod,

I hope you are doing well.

->You need some u-boot executable that's been built to work on the board.

-> Please check the below documents for your reference.
 

http://imx6dev.blogspot.ru/2014/07/inexpensive-jtag-on-imx6-solo-u-boot.html


Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信

649件の閲覧回数
mohamed-ali_fod
Contributor I

Hi Dhruvit,

Of course I have functional u-boot that works for this board , it works if the u-boot is flashed in the flash memory. Also the same u-boot works fine for non secured board through jtag as I mentioned in my previous email (u-boot-spinor-signed.imx.bin). But my question why this u-boot doesn't work through jtag in secured board (secure_config fuse enabled), what could be the difference vs non secure board.

I hope the question is clear.

Thank you in advance,

Mohamed Ali

 

0 件の賞賛
返信

602件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @mohamed-ali_fod,

I hope you are doing well.

->Can you let me know if secure JTAG is enabled or not?
->Please verify whether the CSF file had the correct UID.

->Please refer to 5.2.13.1  Unlock Examples in Code-Signing Tool User’s Guide
https://www.nxp.com/webapp/Download?colCode=IMX_CST_TOOL_NEW

 
Thanks & Regards,
Dhruvit Vasavada
0 件の賞賛
返信

596件の閲覧回数
mohamed-ali_fod
Contributor I

Hi @Dhruvit

The secure JTAG is not enabled I enabled only secure_config fuse.

Is it mandatory to add UID in CSF to load signed u-boot through jtag?

Please note that my signed u-boot is working well on my board if the board boot from memory flash, my problem is to boot the board using signed u-boot loaded through jtag.

Best regards,

Mohamed Ali

0 件の賞賛
返信

554件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @mohamed-ali_fod,

I hope you are doing well.

One needs to enable Secure JTAG mode on a closed device.

It limits the JTAG access by using a challenge/response-based authentication mechanism.

Please refer to Secure Debug in i.MX 6/7/8M Family of Applications Processors for more information.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信