I am using Ubuntu 16.04LTS to build android images for the sabresd_6dq board that I have. I can successfully flash the emmc using the mfg tool in Windows 10.
I have tried the attached script and also using the mfg tool.
When I try to use the mfg tools on Ubuntu by running:
./linux-runvbs.sh mfgtool2-android-mx6dl-sabresd-emmc.vbs
I get the following error:
mfgtool2-android-mx6dl-sabresd-emmc.vbs
Executing: ./mfgtoolcli -l eMMC-Android -s board=sabresd -s folder=sabresd -s soc=6dl -s mmc=3 -s data_type=
Your Options:
board: sabresd
folder: sabresd
soc: 6dl
mmc: 3
data_type:
Ready to flash.
init op Failed code# 21
The device is connected with the boot switch (SW6) set to 00001100. How do I flash the emmc of a sabre SD on Ubuntu?
The problem is "There is no -c Linux in mfgtool2-android-mx6dl-sabreauto-sdcard-f2fs.vbs.sh" It cause mfgtoolcli to open ucl2.xml under Profiles/placeholder/OS Firmware/ folder which is wrong.
After fixing it, I got another error code now
ModuleID[2] LevelID[1]: Error: Invalid device name: MX6SLL
ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 24
How wonderful! Does NXP test it on Ubuntu when they publish it????
I got around error code 24 by commenting out the MX6SLL, MX6ULL, and MX7ULP lines at the beginning of ucl2.xml.
<CFG> <STATE name="BootStrap" dev="MX6SL" vid="15A2" pid="0063"/> <!-- <STATE name="BootStrap" dev="MX6SLL" vid="1FC9" pid="0128"/> --> <STATE name="BootStrap" dev="MX6D" vid="15A2" pid="0061"/> <STATE name="BootStrap" dev="MX6Q" vid="15A2" pid="0054"/> <STATE name="BootStrap" dev="MX6SX" vid="15A2" pid="0071"/> <STATE name="BootStrap" dev="MX6UL" vid="15A2" pid="007D"/> <STATE name="BootStrap" dev="MX7D" vid="15A2" pid="0076"/> <!-- <STATE name="BootStrap" dev="MX6ULL" vid="15A2" pid="0080"/> --> <!-- <STATE name="BootStrap" dev="MX7ULP" vid="1FC9" pid="0126"/> --> <STATE name="Updater" dev="MSC" vid="066F" pid="37FF"/> </CFG>