Hi!
we need to change MTU size more than 1500 default on imx6ull/ul linux imx
ifconfig eth0 mtu 2000
we get
ifconfig : SIOCSIFMTU invalid argument
Please explain how to change MTU size in linux imx?
How can we can add Jumbo packet support on imx6?
Thanks
Vladimir
Hello,
Generally, from software point of view, frame length can be configured up to
16K size. According to section 22.6.4.5 (Frame length/type verification: frame length
check) of the i.MX 6UL Reference Manual:
“When the receive frame length exceeds MAX_FL bytes, the BABR interrupt is generated
and the RxBD[LG] bit is set.
The frame is not truncated unless the frame length exceeds the value programmed in
ENETn_FTRL[TRUNC_FL].”
Bit fields MAX_FL of Receive Control Register (ENETx_RCR) and TRUNC_FL of
Frame Truncation Length (ENETx_FTRL) are 14-bit values.
The problem is that ENET hardware does not support Jumbo frames directly.
In particular, FIFO is not sized for jumbo frames. This means data lost can take place
with high probability.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
Hello,
It would be possible in store and forward disable mode (defined by bit STRFWD in
Transmit FIFO Watermark Register [ENETx_TFWR]. But section 22.6.8.4 (Received
frame discard) of the 6UL RM states, that the receive FIFO must be operated in store
and forward mode.
Nevertheless, customers can try the store and forward disable mode.
Regards,
Yuri.
Hello!
Do i need to change the ENETx_RCR ENETx_FTRL ENETx_TFWR registers only to allow Jumbo packets
Do i need to patch Freescale FEC driver?
if you know any patch like this please find out!
Regards
Vladimir
Hello,
Yes, it is needed to disable store and forward mode, configure FIFO watermarks
and provide enough buffers for data (to load the jumbo frames). It will require
to modify NXP ENET / FEC driver. We do not have patches for the Jumbo, sorry.
Regards,
Yuri.
Hello
I have done the patch I can receive a frame of 2002 bytes with the disabled store and forward.
i have changed registries ENETx_RCR ENETx_FTRL ENETx_TFWR
plus FEC_ENET_RX_FRSIZE
FEC_ENET_TX_FRSIZE
What did i miss?
2000 bytes is FIFO maximum on imx6ul?
i haven't found config of Maximum Receive Buffer Size Register ENETx_MRBR its located in ref. manual 22.5.23
but i don't see it in the code
Regards
Vladimir
The original IEEE 802.3 Ethernet standard defines the Ethernet frame structure with MTU (i.e. frame payload size in bytes) in range of 46 to 1500. The higher values of MTU can be achieved using so-called Jumbo frames. However, this type of frames is not defined by the IEEE 802.3 standard and depends on the particular network equipment vendor. So, the ENET controllers of the i.MX series processors do not support the Jumbo frames and their highest MTU value is 1500 according to the IEEE 802.3 standard.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
We are streaming raw images to the board through ethernet and for us it is very important to be able to run jumbo packets to lower the overhead. In the i.MX8 reference manual (IMX8MDQLQRM.pdf) chapter 11.5.4.1 the 9000 octets packets are mentioned in multiple tables and there is a note stating:
"Although the IEEE specification defines a maximum frame length, the MAC core provides the flexibility to program any value for the frame maximum length."
So my question is if the limitation not valid for i.MX8 and only i.MX6 and earlier? Jumbo packets is crucial for our selection of platform. Secondly I wonder if the solution above is enough for running jumbo pakets.
Thank you!