After updating with gpu-viv-bin-mx6q-3.0.35-4.0.0.gz our Qt5 application no longer links correctly.
errors are:
libGLESv2.so: undefined reference to `gcoOS_MemCopy'
libGLESv2.so: undefined reference to `gcoOS_StrLen'
libGLESv2.so: undefined reference to `gcoOS_ZeroMemory'
I found that prototypes of these (and some other) calls were removed from the updated include file HAL/gc_hal_base.h so these
changes must be deliberate.
So my questions are:
Is the file libGLESv2.so.2.0.0 not correctly updated?
or
Is there another library that needs to be linked to provide these functions?
regards,
Henk
解決済! 解決策の投稿を見る。
PrabhuSundararaj Aug 26, 2013 7:04 AM (in response to Karina Valencia Aguilar)
Those functions are no more public and defined a static functions. Can you please try to rebuild the QT5 framwork and the application with the new binaries.
You seem to lack a '-lGAL' gcc option.
PrabhuSundararaj Aug 26, 2013 7:04 AM (in response to Karina Valencia Aguilar)
Those functions are no more public and defined a static functions. Can you please try to rebuild the QT5 framwork and the application with the new binaries.
i've got the same problem, could you point me to where i can download
gpu-viv-bin-mx6q-3.0.35-4.0.0.gz please ?
i found one here: http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0/
but i'd rather get it directly from freescale for security purposes.
Go to: https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
click the i.MX6 SoloLit Evaluation Kit dropdown box under the software and updates paragraph
select Linux source
Through the licence agreement this will bring you to:
Within that tar file you will find further tar files, among which the gpu-viv-bin
I solved my original problem, one of the files was not correctly updated.
regards,
Henk.