Hi everyone,
I have integrated touch for my custom board, and i need integrate leds for button touch. I have created dev file button-backlight in /sys/class/leds/ and add code as below to imx/lights/fsl_lights.c in HAL:
char const*const KEYBOARD_FILE
= "/sys/class/leds/button-backlight/brightness";
...
static int
set_light_buttons(struct light_device_t *dev,
struct light_state_t const *state)
{
int err = 0;
int on = is_lit(state);
pthread_mutex_lock(&g_lock);
err = write_int(KEYBOARD_FILE, on ? 255 : 0);
pthread_mutex_unlock(&g_lock);
return err;
}
...
if (0 == strcmp(LIGHT_ID_BACKLIGHT, name))
set_light = set_light_backlight;
else if (0 == strcmp(LIGHT_ID_KEYBOARD, name))
set_light = set_light_keyboard;
else if (0 == strcmp(LIGHT_ID_BUTTONS, name))
set_light = set_light_buttons;
else if (0 == strcmp(LIGHT_ID_BATTERY, name))
set_light = set_light_battery;
else if (0 == strcmp(LIGHT_ID_NOTIFICATIONS, name))
set_light = set_light_notification;
else if (0 == strcmp(LIGHT_ID_ATTENTION, name))
set_light = set_light_attention;
else
return -EINVAL;
But it do not work, i think platform of FSL is using LIGHT_ID_BATTERY and LIGHT_ID_BACKLIGHT, and I do not know where to configure for LIGHT_ID_BUTTONS. If anyone has solution for this issue, let me know, thank you very much!
Dear Dinh,
Let me give you some resume about how the inputs are working in Android, I think you should use the events to call the led ligth from there. Please see the attach
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------