Hi
I was wondering if I could somewhere get a hold of the latest Vivante prebuilt hardfloat binaries ?
I have a custom iMX6q board and wanted to see if there were any newer binaries available then L3.0.35_4.1.0, see here: https://community.freescale.com/docs/DOC-95560
I have used this version with Qt5.2 and Qt5.3 some time ago but now I when I use it against Qt5.4 it crashes. My application is using the eglfs platform (No X or Wayland) and it crashes after trying to open /dev/fb0.
I decided to give a new version a try if it were available.
My goal is to run a Qt5.4 browser application that utilizes the 2D acceleration.
regards
Einar
解決済! 解決策の投稿を見る。
I found what I was looking for here: http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/
Timesys is keeping a repo of prebuilt binaries and header files that follow the kernel versions issued by Freescale, the latest one being 3.10.17.
I downloaded the libraries and header files, recompiled Qt5 and things started to work-ish !!
I had a kernel panic which lead me to change the split ptlock in include/linux/mm_types.h as suggested in the patch here: https://lists.yoctoproject.org/pipermail/meta-freescale/2014-March/007816.html.
After that the graphics work fine and the accelerated examples provided both by Qt and Vivante are working fine, i.e. utilizing the GPU.
Hope this helps somebody.
regards
Einar
I found what I was looking for here: http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/
Timesys is keeping a repo of prebuilt binaries and header files that follow the kernel versions issued by Freescale, the latest one being 3.10.17.
I downloaded the libraries and header files, recompiled Qt5 and things started to work-ish !!
I had a kernel panic which lead me to change the split ptlock in include/linux/mm_types.h as suggested in the patch here: https://lists.yoctoproject.org/pipermail/meta-freescale/2014-March/007816.html.
After that the graphics work fine and the accelerated examples provided both by Qt and Vivante are working fine, i.e. utilizing the GPU.
Hope this helps somebody.
regards
Einar
Hello, Einar
Can you share your image?
BR, Dmitry
Hi Dmitry and sorry for my terribly late answer.
Do you still need an image ?
regards
Einar
Hi Einar
I think one can look at
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.31_1.1.0_beta
and post to meta-fsl-arm mailing list, so that someone familiar with latest drivers could
try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------