Hi li
for 800x480 lvds settings one can look at nitrogen board
Universal Boot Loader general discussion ()
[PATCH 17/32] nitrogen6x: display: add wvga-lvds panel
Theory&Example :
AN3974 Different Display Configurations on i.MX35 Linux PDK
how to support WSVGA output in imx6sdq
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
our board is mx6q,and android version is 4.4.3_r1. kernel 3.10.53 u-boot 2014.04
below is the u-boot seting.
static struct display_info_t const displays[] = {{
.bus = -1,
.addr = 0,
.pixfmt = IPU_PIX_FMT_RGB666,
.detect = NULL,
.enable = NULL,
.mode = {
.name = "Hannstar-XGA",
.refresh = 60,
.xres = 800,//1024,
.yres = 480,//768,
.pixclock = 19531,//15385,
.left_margin = 160,//220,
.right_margin = 160,//40,
.upper_margin = 18,//21,
.lower_margin = 18,//7,
.hsync_len = 60,
.vsync_len = 10,
.sync = FB_SYNC_EXT,
.vmode = FB_VMODE_NONINTERLACED
} }
below is the kernel device tree seting
lvds-channel@0 { | ||
crtc = "ipu2-di0"; | ||
status = "okay"; | ||
fsl,data-mapping = "spwg"; | ||
fsl,data-width = <18>; |
display-timings { | ||||
native-mode = <&timing0>; | ||||
timing0: hsd100pxn1 { | ||||
clock-frequency = <65000000>; | ||||
hactive = <800>; | ||||
vactive = <480>; | ||||
hback-porch = <160>; | ||||
hfront-porch = <160>; | ||||
vback-porch = <18>; | ||||
vfront-porch = <18>; | ||||
hsync-len = <60>; | ||||
vsync-len = <10>; | ||||
}; | ||||
}; | ||||
}; |
Dear sir.
in that link.Universal Boot Loader general discussion ()
what is the base version?
I can't found the match line in u-boot 2014.04